CNC - Haas Automation, Inc. - Preowned Machines
|
|
|
| |
|
All Haas Automation certified pre-owned machines go through an
extensive testing program before being certified for sale. As
a recognized leader in the manufacture of American-made CNC
machining centers, Haas has established this step-by-step,
150-point rebuild process to bring the Haas Automation
pre-owned or demo machine back into the workforce as a
fully-capable, ready-to-cut machine. The perfect solution for
companies and shops looking for a quick machine addition to
meet increased work demands, or as an affordable upgrade to
their existing machining center lineup.
Offered in the new certified machine program is a full
assortment of pre-owned Haas CNC products, including vertical
and horizontal machining centers, CNC lathes and Haas rotary
tables and indexers.
But first, let’s look at what the Haas Certified Pre-Owned
Machine Program provides you, the shop owner . . .
1. Initial Evaluation
All pre-owned machines received at Haas Automation are
evaluated upon receipt to establish the machine’s condition
and suitability for rebuilding. The evaluation looks at
factors such as age, condition, and model. Only those machines
that are deemed suitable for rebuilding are placed in the
rebuild schedule.
2. Rebuild Schedule
Haas Automation employs a dedicated CNC machining center
rebuild area, staffed with experienced technicians trained in
the rebuild process. When the selected machine arrives in the
rebuild area, it undergoes yet another extensive evaluation
under power to determine the complete scope of work required
to make it functionally and cosmetically conform to current
Haas Automation engineering standards.
3. Rebuild Process
When the rebuild process is begun at Haas Automation, it is
done in a systematic and controlled fashion. Utilizing Haas’
ERP (Enterprise Resource Planning) system, the correct
materials — required to rebuild the machine — are withdrawn
from inventory and staged in the dedicated rebuild area.
4. Machine Testing
When the rebuild process is complete, the machining center
undergoes the same inspection program used on our new
production machines. These processes verify that the machine
performs accurately and correctly, and that the entire machine
functions as it should. The inspection process includes
verification of:
• Machine model, type and options
• Machine operation
• Machine settings and parameters
• Machine accuracy, repeatability and geometry
• Machine documentation
Please reference Haas Automation’s 150+ Point Inspection
Process.
When you buy Haas pre-owned machines directly from Haas
Automation, you know they have passed a 150-point inspection
and are certified by Haas. Pre-owned machines bought from an
HFO or Customer are not subject to this certification process.
If you are viewing or planning to buy a pre-owned machine from
an HFO, or Customer, you will need to ask about their specific
rebuild regimen. Haas Automation will not assume
responsibility for any machine that is not clearly identified
as a Haas-certified pre-owned machine.
Attention Visitors: Please be aware that numerous sites are
using the Haas name to sell used Haas CNC equipment. These
websites are not authorized to use the Haas name and the
equipment they sell is not necessarily the same as what you
see here.
Top
|
|
|
|
|
|
 |