PERFORMANCEDRIVEN HORIZONTAL MACHINING CENTERS Rigid foundation Motion control Spindle & spindle drive Tool changers Chip removal & coolant systems EC Series 40taper HMCs EC Series 50taper HMCs HS Series 50taper HMCs The Haas control Operator convenience Machine dimensions Machine specifications 45 67 811 1213 1415 1625 2627 2829 3035 36 37 3839 T he new generation of Haas horizontal machining centers started with a simple idea and a clean design slate. The engineering mission was to design and build a productionfocused HMC that was robust and dependable, easy to use and affordable to buy and service. These are the trademarks of a Haas machine tool. The EC Series HMCs are completely new from the ground up, and designed to meet the needs of today's industries right out of the box. Like the industryleading Haas VMC line and the highly successful SL Series turning center line, Haas EC Series HMCs are based on shopproven designs that provide the best costtoperformance ratio available. Inside this brochure you'll find all of the latest technological advancements, new machine sizes and capabilities that Haas Automation has developed through constant research and ongoing product advancement. 2 MODELS: EC300 EC400 EC400PP EC500 EC1600 EC2000 EC3000 HS3 & 3R HS4 & 4R HS6 & 6R HS7 & 7R Rigid Foundation Innovative Designs and HighAccuracy Processing Yield a 50% increase in machine rigidity over previous models. Rigid, HeavyDuty TBase Design Haas EC Series horizontals are based on a classic and proven design. The rigid Tbase foundation allows the pallet carrier to move in the Z axis, while the spindle head moves only in the X and Y axes. Specifications subject to change without notice. Not responsible for typographical errors. 4 1 Setup, 5 Sides Surfaced, Drilled and Tapped EC Series base castings are machined on stateoftheart, 5side CNC machines. Each casting is completely machined, drilled, tapped and inspected in a single setup, which provides higher accuracies and smoother production. Our ability to precisely machine all critical features of each casting eliminates alignment errors in final assembly. Highaccuracy inprocess inspection guarantees that every casting meets our stringent quality standards. Cast iron provides up to 10 times the damping capacity of steel. That's why Haas uses cast iron for all major components. Our castings are internally reinforced with heavy ribs to resist flex and damp vibration. All Haas castings are thoroughly inspected before and after machining to ensure they are free of flaws. All structural components are optimized using finite element analysis (FEA) to produce the most rigid designs. AntiFlex, Reinforced Base & Column Castings Our specially designed base and column castings feature heavy ribs that absorb vibration and transfer it away from the cutting area. The column castings yield superior rigidity and provide the most antiflex properties of any design. 5 Motion Control Electronic Thermal Compensation System When ballscrews rotate they generate heat, which can cause them to expand. With high duty cycles, ballscrew growth can lead to cutting errors. Our electronic thermal compensation (ETC) algorithm accurately models this heating effect and compensates for screw position. 100% Ballbar Tested Haas uses a stateoftheart ballbar test to ensure the linear accuracy and geometry of every machine. The ballbar tracks machine movement to ±0.5 micron, with a resolution of 0.1 micron. The bar is attached to the spindle and a fixed point on the table. Then the machine is put through a series of circular moves to certify synchronous movement, and verify axis straightness and squareness. Data from the ballbar generates a chart illustrating machine accuracy. Any deviations in squareness or accuracy show up as distorted circles that are very easy to spot. A copy of this chart ships with each Haas HMC as assurance that the machine is accurate and properly aligned. DoubleAnchored Ballscrews Haas uses only premiumquality ballscrews and guides from the world's top manufacturers. Although more expensive, their premium quality is the only way to achieve the high accuracy and long life that our customers demand. The ballscrews are anchored at both ends and inspected for 100% parallelism to the axis guides. Preloaded ball nuts eliminate backlash. 6 Recirculating Ball Guideways Haas uses recirculating ball guideways for each axis of every HMC. These guideways are preloaded for zero clearance, and provide full loadcarrying capacity in all directions. They consume less power, do not require adjustment and are proven to outperform sliding box ways for accuracy and speed. Each guideway is lubricated automatically to guarantee long life. Brushless Servomotors Box Way Recirculating Ball Guideway Required Clearance Zero Clearance Haas uses stateoftheart brushless servomotors that offer more torque in a smaller frame than almost any other motors available. These highperformance servos provide more power for heavy cuts, and higher acceleration/deceleration rates to reduce cycle times. Highresolution encoders and closedloop digital feedback ensure ultraprecise positioning. Recirculating Ball Guideways Outperform Box Ways Recirculating ball guideways are preloaded to provide zero clearance between the moving surfaces. This increases rigidity and stiffness, while providing higher accuracy and reliability. Box ways require clearance between the moving surfaces in order to operate. Recirculating ball guides have a very low coefficient of friction, which allows faster movements without sacrificing repeatability or positioning accuracy. Box ways have a high coefficient of friction, which results in stickslip effects that can lead to machine errors. Automatic Lubrication The Haas automatic lubrication system meters and distributes oil to guideways and ballscrews as the machine operates. This ensures that all critical components are lubricated with the correct amount of oil at all times, saving time and reducing maintenance costs. Haas DirectCoupled Servomotors Our servomotors are coupled directly to the ballscrews with steel disc couplings to eliminate windup, even under severe loading. This greatly improves positioning accuracy, and provides more accurate threading and contouring. And they don't wear out or lose accuracy over time. 7 Main Spindle Features Powerful Vector Spindle Drives The Haasdesigned and built vector spindle drive uses closedloop, digital servo technology to provide precise speed control and peak performance under heavy cutting loads. The system greatly increases lowspeed torque and accelerations, resulting in the fastest, most powerful spindle ever. These drives allow you to push the spindle to 150 percent of the motor's continuous power rating for 15 minutes, and to 200 percent for 5 minutes. That's more performance headroom than other spindle drives on the market. Spindle Configurations Model EC300 · EC400 · EC400PP · EC500 · EC1600 EC2000 EC3000 HS3 HS3R HS4 HS4R HS6 HS6R HS7 HS7R 40 TAPER 50 TAPER STD 2SPEED GEARBOX 5,000 RPM STD 6,000 / OPT 10,000 RPM STD 8,000 / OPT 12,000 RPM · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · Gearbox standard w/50taper spindle. All machines available in CT or BT. 8 HighCapacity Cartridge Spindle The advanced design of our spindles provides high axialthrust capability, yet generates minimal heat. The front and rear bores of the housing and the OD of the spindle are finished in one operation. This guarantees perfect alignment between the bores and ODs, thus reducing bearing heat. Preloaded angular contact bearings are used throughout, with the two forward bearings separated by a large spacer to enhance radial stability enabling heavy cuts in steel. To ensure long life, the spindle is pressurized with air to prevent coolant contamination, and an air/oil mixture is injected automatically at preset intervals to ensure precise lubrication and long bearing life. OnTheFly WYEDELTA Switching Haas HMCs feature the Haas DualDrive system, which consists of a dualwinding motor Wye and Delta and an electronic switch to change between the windings. Selecting the best winding for lowrpm cutting and the best winding for highrpm cutting yields higher torque over a much wider rpm range. Onthefly switching maximizes acceleration/deceleration rates for more chip making and less waiting. Spindle Unit Replacement PEAK POWER RPM Typical power curve Enhanced power range with onthefly WyeDelta The cartridge design of the Haas spindle simplifies service by allowing quick changeout of the entire spindle. Some items shown in this brochure are optional. Please contact your local distributor for assistance. 9 Main Spindle Features 40Taper Inline DirectDrive Spindle and Motor Unit The most advanced Haas spindle design is our innovative inline directdrive spindle that is coupled directly to the motor. This provides supersmooth operation for excellent surface finishes, and reduces operating heat for greater thermal stability. Driving our inline spindle is a highoutput motor designed and built completely inhouse by Haas. This allows us to control quality and delivery, while producing a rigid, wellbalanced motor that has a wide power band and smooth output. Our 8,000rpm, 20 hp inline directdrive spindle is standard on Haas 40 taper HMCs, and a 12,000rpm, 30 hp spindle is optional. Rigid Tapping Using an encoder attached directly to the Haas highperformance spindle, Zaxis motion is synchronized with the spindle's rotation. Synchronized tapping eliminates the need for expensive, floating tap holders, and prevents leadthread distortion and startthread pullout. To reduce cycle times, the tap can reverse out of a rigidtapped hole faster than it went in. 90 80 70 60 50 40 30 20 10 Spindle Torque Cutting performance, material removal rates and surface finish are the products of torque, speed and power. The chart at left shows a Haas 12,000rpm 30 hp inline spindle for 40taper HMCs. The chart at right shows a geardriven, 10,000rpm spindle for 50taper models. 9,500 12,000 Shift Point = 2,950 rpm Specifications subject to change without notice. Not responsible for typographical errors. 10 50Taper Features 50Taper GearDriven Haas Spindle The Haas gearedhead spindle provides increased lowend torque for powerful cutting, while retaining the ability to run at high speed for smooth surface finishes. The 30 hp, 50taper spindle is standard on larger Haas horizontals, and provides 450 ftlb of cutting torque for heavy material removal. A 10,000rpm option is available. HighPrecision Gearbox Haas has invested more than $4 million in the finest gearmaking and inspection equipment in the world. Haas gears are CNC machined and hobbed out of 8620 steel, heat treated to 60 Rc, and precision CNC ground to AGMA Class 13 quality. A drysump oiling system circulates oil to all vital areas of the gearbox. 50 Taper Offers More A Gage diameter (A) A B Taper length (B) B Tool clamp force* Max tool weight Max tool diameter *Nominal 40 Taper 1.750" 44.45 mm 2.687" 68.25 mm 1,800 lb 8 007 N 12 lb 5.4 kg 6" 152.4 mm 50 Taper 2.750" 69.85 mm 4.000" 101.60 mm 4,000 lb 17 793 N 30 lb 13.6 kg 10" 254 mm 11 Tool Changing Remote ToolLoad Station To simplify tool maintenance and inspection, Haas palletchanging HMCs with highcapacity tool changers include a remote toolload station. This convenient side window and control panel allow the operator to access tools easily without having to load/unload them via the machine's spindle. This increases productivity by allowing the operator to perform tool maintenance while the machine is cutting. Tool Changer Specifications Maximum tool sizes for automatic tool changers Tool Changer Type Standard configuration # Tools Machine Models EC300 EC400 EC500 EC400 Pallet Pool EC1600/2000/3000 HS3/4/6/7 Tool to Tool Chip to Chip A Max Dia. when adj. pocket full/empty 3" / 6" 3" / 6" 3" / 6" 3" / 6" 4" / 10" 4.9" / 9.8" B Tool Length 10" 12" 12" 12" 20" 20" Max Tool Weight 12 lb 12 lb 12 lb 12 lb 30 lb 80 lb A A 40taper sidemount 40taper sidemount 40taper sidemount 40taper sidemount 50taper sidemount 24+1 24+1 40+1 70+1 30+1 38+1 2.8 sec 2.1 sec 1.6 sec 1.6 sec 10.3 sec 4.9 sec 4.5 sec 3.7 sec 2.8 sec 2.8 sec 12.6 sec 15.8 sec B 50 Taper 40 Taper B 50taper sidemount Optional configuration 40taper sidemount 40taper sidemount 50taper sidemount 50taper sidemount 50taper sidemount 50taper sidemount 40+1 70+1 50+1 60+1 90+1 120+1 EC300 & EC400 EC400 & EC500 EC1600/2000/3000 HS3/4/6/7 HS3/4/6/7 HS3/4/6/7 1.6 sec 1.6 sec 10.3 sec 4.9 sec 4.9 sec 4.9 sec 2.8 sec 2.8 sec 12.6 sec 15.8 sec 15.8 sec 15.8 sec 3" / 6" 3" / 6" 4" / 10" 4.9" / 9.8" 4.9" / 9.8" 4.9" / 9.8" 12" 12" 20" 20" 20" 20" 12 lb 12 lb 30 lb 80 lb 80 lb 80 lb From concept to reality The Haasdesigned and built sidemount tool changer symbolizes our focus on inhouse design, development and manufacturing. It's the best way to ensure total control. We use this approach to refine our processes, control costs and ensure a consistent high level of quality in everything we build. 12 SMTC Tool Change Times as short as 1.6 (tool to tool) SECONDS Inside the Haas SideMount Tool Changer The synchronized cycloidal motion of our sidemount tool changers is controlled by precision cams that are manufactured inhouse on custombuilt, 5axis Haas machines. This rugged, dependable design uses a special Haas wormgear drive and an electronically controlled start/stop system for long life and maintenancefree operation. Every Haas SMTC is manufactured completely inhouse to guarantee fast, smooth, reliable operation. 13 Chip Removal Triple Chip Augers (Below) Highproduction machining generates a large volume of chips that must be removed from the machine quickly to maximize cutting time and optimize returns. EC400 and EC500 HMCs utilize a tripleauger chipconveyor system to remove chips from the machine efficiently. Steeplysloped way covers force chips into a pair of side augers that move them out of the work area. A third auger at the front of the machine transports the chips to a discharge chute compressing them and wringing out the coolant in the process. For added reliability, the system reverses automatically if a jam occurs. A quadauger system is part of the enclosure option for the EC1600, 2000 and 3000. BeltType Conveyor (Above) On EC400 and EC500 Haas HMCs, the main auger can be replaced with a belttype chip conveyor that discharges chips at a standard barrel height. A belttype conveyor is standard on the EC300, and an intank conveyor is available for the EC1600, 2000 and 3000 with enclosure option. 14 Coolant Systems Programmable Coolant Nozzle Our programmable coolant nozzle is controlled automatically by the part program to direct coolant precisely at the cutting area, eliminating constant adjustments by the operator. Coolant nozzle positions are specified during set up, just like tool offsets, and called up automatically for each tool as the program runs. The nozzle can also be adjusted manually from the keypad while a program is running. Flow Rate Dynamics The chart above illustrates the 8.0 relationship between flow and 7.0 pressure. For both the 300psi and 6.0 1,000psi throughspindle coolant 5.0 options, the highest pressure 4.0 occurs at the lowest flow rate. The 3.0 actual pressure delivered to the 2.0 cutting edge depends on the size 300 psi 1.0 TSC output 1,000 psi TSC output of the coolant passages in the tool. 0 Smaller coolant passages restrict 300 1,000 the flow, causing the pressure to increase (up to the maximum provided by the system). Larger coolant passages in the tool allow more fluid to pass through, resulting in lower pressure at the cutting edge. 300psi or 1,000psi ThroughSpindle Coolant Throughspindle coolant supplies coolant through the tool, directly to the cutting edge. This increases tool life, allows higher cutting speeds, and clears chips during deephole drilling and blindpocket milling. Two systems are available. One provides up to 300 psi to the cutting edge, and the other provides up to 1,000 psi. The 1,000 psi system includes the auxiliary coolant filter (shown at right). The actual pressure of both systems will vary with the size of the coolant passages in the tool. See details at right. EasyAccess, RollOut Coolant Tanks Volume (GPM) Our coolant tanks have wheels for easy removal and to facilitate cleaning. A separate chip basket and liftout screen prevent chips from reaching the pump, and all electrical and hose connections at the tank can be removed by hand. Some items shown in this brochure are optional. Please contact your local distributor for assistance. 15 Coolant Level Sensor A sensor in the coolant tank allows you to monitor coolant level directly on the control screen, preventing damaged tools and saving time. Auxiliary Coolant Filter This 25micron, #2 bagtype filter system removes contamination and minute particles from the coolant before they can be recirculated through the coolant pump. EC300 HMC Axis travels (xyz) Pallet size Maximum pallet load Pallet change time Tool taper/type 20" x 18" x 14" 11.81" 550 lb 4.7 sec CT 40 taper 508 x 457 x 356 mm 300 mm 250 kg BT 40 optional Standard Features · 20 hp Vector Dual Drive · 8,000rpm 40 Taper Spindle · Inline DirectDrive System · Full 4th Axis · Dual Pallet Changer (300 mm pallets) · 1,000 ipm Rapids · 24Pocket SideMount Tool Changer · BeltType Chip Conveyor · Rigid Tapping Options (partial list) · 12,000rpm Spindle · 30 hp Vector Dual Drive · 40Pocket SideMount Tool Changer · ThroughSpindle Coolant · Programmable Coolant Nozzle Ø 15.00" Ø 381 mm 100 mm (3.937") 125 mm (4.921") 75 mm (2.953") 25 mm (0.984") Standard Pallet: 36 x 1/2"13 UNC2B Metric Pallet: 36 x M12 x 1.75 150 mm 125 mm (5.906") 100 mm (4.921") (3.937") 22.50" 572 mm 75 mm (2.953") 80 mm (3.150") 25 mm (0.984") 300 mm (11.811") 150 mm (5.906") Maximum fixture/workpiece size for pallet changes 80 mm (3.150") 300 mm (11.811") 16 Compact and Cost Effective 300 mm pallets not a lot of floor space Do you need a highproductivity HMC with 300 mm pallets? Look no further than the EC300. With its compact footprint, long list of standard features, and a wide selection of options that includes a 12,000rpm spindle and 1,000 psi throughspindle coolant, the EC300 is an affordable way for any shop to increase productivity. Some items shown in this brochure are optional. Please contact your local distributor for assistance. 17 EC400 HMC Axis travels (xyz) Pallet size Maximum pallet load Pallet change time Tool taper/type 20" x 20" x 20" 15.75" 1,000 lb 8 sec CT 40 508 x 508 x 508 mm 400 mm 454 kg BT 40 optional Standard Features · 20 hp Vector Dual Drive · 8,000rpm 40Taper Spindle · Inline DirectDrive System · 1Degree Tombstone Indexing · Dual Pallet Changer (400 mm pallets) · 1,000 ipm Rapids · 24Pocket SideMount Tool Changer · Triple ChipAuger System · Rigid Tapping Options (partial list) · 12,000rpm Spindle · 30 hp Vector Dual Drive · Full 4th Axis · 40 or 70Pocket SideMount Tool Changer · ThroughSpindle Coolant · Programmable Coolant Nozzle Ø 19.69" Ø 500 mm M12 x 1.75 x 1.13 Dp 400 mm (15.75") 5/8"11 x 1.13 Dp 30.00" 762 mm Metric Inch 80 mm (3.15") 400 mm (15.75") 50.0 mm 50.0 mm 80 mm (3.15") Maximum fixture/workpiece size for pallet changes Specifications subject to change without notice. Not responsible for typographical errors. 18 HighProductivity Solutions 400 mm Workhorse A 400 mm pallet HMC is the workhorse of many production shops, and the EC400 packs more value into its footprint than any other 400 mm HMC on the market. With its standard tripleauger chipconveyor system, available 70pocket automatic tool changer and optional 1,000 psi throughspindle coolant, the EC400's performance cannot be matched. Some items shown in this brochure are optional. Please contact your local distributor for assistance 19 Horizontal PalletSystem Design Simple, Dependable PalletIndexing System The palletindexing system for EC Series machines employs a simple, robust and shopproven design that has been perfected by more than 20 years of experience building rotary tables. At the heart of the system is a precision wormgear set that is manufactured to AGMA Class 13 quality using the same highaccuracy techniques used to build Haas rotary tables. This proven design ensures precise positioning and years of troublefree operation. Model Pallet Size Capacity Indexer Capacity Full 4th Clamping Force* Change Time EC300 11.81" 300 mm 550 lb 249 kg 550 lb 249 kg 9,000 lb 40 034 N 4.7 sec EC400 15.75" 400 mm 1,000 lb 454 kg 660 lb 300 kg 14,000 lb 62 275 N 8 sec EC500 19.69" 500 mm 1,000 lb 454 kg 660 lb 300 kg 14,000 lb 62 275 N 9 sec *At 85 psi (5.6 bar) air pressure. HeavyDuty Pallet Clamping To hold the pallet securely to the receiver during machining, we utilize a simple but innovative design that combines mechanical and pneumatic forces to provide 7 tons of clamping force.* The pallet is accurately positioned on the receiver by six locating keys set at the widest possible point on the pallet's base. A plate then clamps the pallet directly over the locating keys using a combination of heavyduty Belleville springs and air pressure. Since pneumatic force is used only to boost clamping force and to release the clamp, a loss of air pressure will not cause the pallet to release. *EC300 has 4 tons of clamping force and uses pneumatic clamping only Special Features Optional HydraulicClamping Provision Decrease part loading/unloading times and ensure consistent part clamping by using hydraulic workholding on EC400 and EC500 HMCs. Our hydraulic clamping provision supplies hydraulic lines and routing for a signal cable from the back of the machine to a pair of distribution manifolds mounted to the pallet changer door. Hydraulic unit, connections to the tombstones and workholding not included. 21 EC400 Pallet Pool Why the Haas System is Different The Haas EC400 Pallet Pool HMC is an easytounderstand and employ productivity solution that avoids the drawbacks of complicated and expensive FMS installations. The system installs easily in your shop in less than a day, and programs just like every other Haas. Standard equipment includes a 70pocket sidemount tool changer, 300 psi throughspindle coolant and a belttype chip conveyor. The userfriendly Haas interface simplifies pallet scheduling and tool management, and it is very intuitive to use. Extremely affordable, easy to use and backed by the best aftersales service in the industry you won't find a better productivity solution than the EC400 Pallet Pool. 173" 4394 mm Door Open Simple Pallet Scheduling The six pallets in the pallet pool are scheduled via the versatile palletscheduler screen. The operator can assign programs to each pallet, schedule jobs and set priorities. Pallets are moved to and from the load station and storage rack by highlighting the pallet number on the screen and pressing a single key. We've made the pallet pool simple to use and easy to program just what you'd expect from Haas. 22 LightsOut Operation 217" 5512 mm 23 EC500 HMC Axis travels (xyz) Pallet size Maximum pallet load Pallet change time Tool taper/type 32" x 20" x 28" 19.68" 1,000 lb 9.0 sec CT 40 813 x 508 x 711 mm 500 mm 454 kg BT 40 optional Standard Features · 20 hp Vector Dual Drive · 8,000rpm 40Taper Spindle · Inline DirectDrive System · 1Degree Indexing · Dual Pallet Changer (500 mm pallets) · 1,000 ipm Rapids · 40Pocket SideMount Tool Changer · Triple Chip Auger System · Rigid Tapping Options (partial list) · 12,000rpm Spindle · 30 hp Vector Dual Drive · Full 4th Axis · 70Pocket SideMount Tool Changer · ThroughSpindle Coolant · Programmable Coolant Nozzle Ø 29.50" Ø 750 mm 30.00" 762 mm Maximum fixture/workpiece size for pallet changes 24 HighProductivity Solutions Bigger Parts, Bigger Pallets The EC500 features a 32" x 20" x 28" work envelope, a dual pallet changer with 500 mm pallets and a builtin, highprecision pallet indexer. The machine comes standard with an 8,000rpm, 40taper spindle, a 40pocket sidemount tool changer, 1,000 ipm rapids and a highvolume coolant system. Also standard is a highprecision, facegear pallet indexer that provides 1degree indexing. The machine's enclosure allows a maximum part swing of 29.5" on the indexer. M12 x 1.75 x 1.13" Dp 500 mm (19.69") 5/8"11 x 1.13" Dp Metric 500 mm (19.69") 400 mm (15.75") Inch 50 mm 100 mm (3.94") 50 mm 100 mm (3.94") 25 EC1600 HMC Axis travels (xyz) Table size Maximum table load Large 64" x 40" x 32" 1626 x 1016 x 813 mm 64" x 32" 1626 x 813 mm 10,000 lb 4536 kg Big, Powerful, Economical The EC1600 base model is configured as an openframe HMC with unimpeded access to the table which handles workpieces weighing up to 10,000 lb. For added versatility, the EC1600 may be configured with an optional 5degree facegear indexer or full 4thaxis rotary platter built into the table. All 50taper EC models also are available with an optional full enclosure that includes a highvolume coolant system and triple chip augers. Even with the full enclosure, you'll still have plenty of access through a 61" (1549 mm) operator door opening. Basic configuration Available Sizes EC1600 64" x 40" x 32" 1626 x 1016 x 813 mm EC1600ZT 64" x 40" x 40" 1626 x 1016 x 1016 mm EC1600YZT 64" x 50" x 40" 1626 x 1270 x 1016 mm EC2000 84" x 40" x 32" 2134 x 1016 x 813 mm EC3000 120" x 40" x 32" 3048 x 1016 x 813 mm Hydraulic Clamping for 4thAxis Platter To hold the 4thaxis platter in position under heavy cutting loads, the EC1600 utilizes an ingenious hydraulicbrake design. Hydraulic fluid is pumped at 1,000 psi into a sealed cavity between two disks. The fluid forces the outer disc against the inner wall of the gear. Assembled with minimum clearance to the gear wall, a push out of only a few thousandths of an inch yields 4,000 ftlb of brake torque. And with no moving parts, the system provides longterm, troublefree operation. Also used on HS Series HMCs with builtin 4th axis. Optional Full 4th Axis * Platter Diameter Drive System 30" 762 mm Servo Rotational Torque 2,000 ftlb 2712 Nm Brake Torque 4,000 ftlb 5423 Nm 10,000 lb 4536 kg Indexing Accuracy ± 30 arc sec Note: All machines listed on this page must be anchored to reinforced concrete foundations for proper operation. Please see installation manual or contact Haas for exact requirements. Max. Capacity 26 *EC1600, ZT, YZT & 2000 only Capacity and Affordable Ø 77.00" (front doors open) Ø 1956 mm Ø 49.50" (front doors closed) Ø 1257 mm Maximum fixture/workpiece size for EC1600 with 4th axis; visit www.HaasCNC.com for specs on other models. With optional enclosure HS Series HMCs HS3 | Axis travels (xyz) HS4 | Axis travels (xyz) HS6 | Axis travels (xyz) HS7 | Axis travels (xyz) 150" x 50" x 60" 150" x 66" x 60" 84" x 50" x 60" 84" x 66" x 60" 3810 x 1270 x 1524 mm 3810 x 1676 x 1524 mm 2134 x 1270 x 1524 mm 2134 x 1676 x 1524 mm Specifications subject to change without notice. Not responsible for typographical errors. 28 Handle Large Workpieces Expand the Possibilities Big parts require big machines. Haas HS Series 50taper horizontals use a modular configuration that allows you to choose a machine with the travels and footprint you need, rather than paying for a machine that's too big. Each of these extralargetravel HMCs features a fully supported X axis to handle extremely heavy loads, and a 50taper spindle that provides 450 ftlb of cutting torque for serious metal removal. A 38tool sidemount tool changer comes standard, with options for 60, 90 and 120 tools. For additional flexibility, each model is available with a full 4thaxis platter set into the table. A 10,000 lb capacity and 50" swing radius mean you can easily machine all four sides of very large parts in a single setup. Maximum workpiece size for full 4th axis without coolant shield Ø 100" Ø 2450 mm Full 4th Axis HS3R, 4R, 6R and 7R models include an integrated full 4thaxis rotary table. See page 39 for specifications, and page 26 for a description of the platter braking system. 152" (3861 mm) Max Depth 189" (4801 mm) 366" Max (9296 mm) Note: All machines listed on this page must be anchored to reinforced concrete foundations for proper operation. Please see installation manual or contact Haas for exact requirements. 29 The Haas Control LED Beacon Light The Haasdesigned beacon light features ultrabright LEDs that can easily be seen from anywhere in the shop. The LEDs generate very little heat and have a life expectancy of more than 10 years. 15" Color LCD Screen Our fullcolor, 15" TFT LCD display is designed to work in the machine shop environment. The highintensity, highcontrast LCD features a very wide viewing angle, and will not fade out in bright light. The panel is mounted behind antiglare, tempered glass for protection and easy viewing. USB Port USB port allows the use of customersupplied external drives or flash memory devices. MultiFunction Jog Handle Most machines use the jog handle only to move the axes around. On Haas machines, the jog handle can also be used in other modes to cursor through the program for faster editing, override spindle speeds and feedrates, or scan through offsets, parameters, etc. Advanced Program Editing A unique feature of the Haas control is an advanced program editor that allows the operator to edit programs in a dualwindow format. Dedicated Keypad OneButton Features Common multistep functions, such as powering up the machine or setting tool offsets, have been reduced to the push of a single button. Other often used functions, such as setting part zeros, homing the machine and selecting the next tool during set up, are also onebutton commands. The Haas keypad has more than 130 keys. All common functions, including a full alphanumeric keypad, are clearly labeled for operator ease. If you've ever fumbled with hot keys, or had to page through screens looking for a specific function, then you will appreciate the simplicity of the Haas control. There are no encrypted codes to memorize, and many functions can be performed simply with the push of a single button. Dedicated Closed System Our focus is to provide Haas users with a robust, dependable control that is seamlessly integrated with the machine. Our closed system is not reliant on PCbased controls or thirdparty NC suppliers. When you call Haas, you get a company that takes full responsibility for the entire machine. Stainless Steel Bezel Constructed of heavygauge T304 stainless steel with a finegrained finish, the bezel of the Haas control not only looks great, it's also easy to clean, resists wear and will not corrode. Specifications subject to change without notice. Not responsible for typographical errors. 30 Control Features Control Specifications General Microprocessor Program execution speed Axis control Interpolation Min. input increment inch mode metric mode Min. output resolution Feed Functions Rapid Traverse Override Feedrate Override Jog Handle Resolution inch mode metric mode Jog Feeds Zero Return Spindle Functions Speed Command Override Tool Functions Length Compensation Diameter/Radius Compensation Length Measurement Life Management Selection Programming Compatibility ISO standard G code Absolute (G90), incremental (G91) 22 functions standard G12, G13 G70, G71, G72 G150 Switchable 105 sets Automatic storage 5 spare G40, G41, G42 G43, G44, G49 G141 G143 RS232, USB To 115,200 baud 1 MB; up to 16 MB optional 500 Positioning Canned Cycles Circular Pocket Milling BoltHole Drilling Advanced Pocket Milling Inch/Metric Work Coordinates Part Zero Set M Code Outputs 2D Cutter Diameter Compensation 2D Cutter Length Compensation 3D+ Cutter Diameter Compensation 5Axis Tool Length Compensation Data Input/Output Communications Port Data Rate Memory Capacity Standard Number of Programs 200 sets, geometry & wear 200 sets, geometry & wear Automatic length storage 200 sets w/alarms Txx command S = 1 to max spindle rpm 0% to 999% in 1% increments inch mode metric mode 5%, 25%, 50%, 100% 0% to 999% in 1% increments 0.0001"/0.001"/0.01"/0.1" per handle division 0.001/0.01/0.1/1.0 mm per handle division 0.1/1.0/10.0/100.0 ipm 1.0/10/100/1000 mm/min. One key (G28) Triple highspeed 32bit 1,000 blocks/sec standard 3 axes linear, 4th and 5th axes optional G01, G02, G03, helical 0.0001" 0.001 mm 0.0000072" (0.000 18 mm) User friendly Advanced program editor Brushless AC servo drives Up to 833ipm cutting feedrates Triple 32bit processors Executes up to 1,000 blocks/second ISO standard Gcode compatibility Haas onebutton powerup Haas onebutton tool offset entry 200 tool offsets 105 work coordinates Tool load monitoring Tool life management Helical interpolation Background editing Splitscreen program review Trig calculator Tangent calculators Speeds and feeds calculator Arc calculator RS232 / DNC link / USB / optional Ethernet Midprogram restart Inch or metric programming Message page Selectable languages Selfdiagnostics Fully descriptive alarms Programmable mirror imaging Advanced pocket milling Bolthole drilling Graphic dry run 5 spare M functions Contour accuracy control Text engraving Made in the USA May be used by options. With 6' or shorter cable. Some items shown in this brochure are optional. Please contact your local distributor for assistance. 31 Visual Quick Code Commonsense, textdriven, VQC programming V isual Quick Code uses a graphical interface to make creating simple Gcode programs nearly effortless. Machinists simply select the operation they wish to perform from an onscreen list (e.g., bolthole circle, drilling, tapping, pocket milling). Once the operation is selected, a series of graphical part templates is displayed, along with a text description of the operation to be performed for each template. Select the template that best matches what you want to do, and Visual Quick Code prompts you to fill in part dimensions, speeds, feeds, etc. Using the information you input, Visual Quick Code generates the correct Gcode program to match the operation. Complex parts can be programmed a piece at a time by using individual templates to generate G code for each part feature, and then inserting the G code into a single (or an existing) program. Because Visual Quick Code is a program stored in the Haas control's memory, rather than embedded, machinists can modify existing templates, or even create their own templates for common operations or families of parts. Intuitive Programming System Simple, intuitive and more powerful than ever Thanks to Haas' Intuitive Programming System, it's no longer necessary for a machine operator to know G code to perform basic milling operations. The IPS software comes standard on our Toolroom Mills, and is optional on all other Haas vertical machining centers. The Haas Intuitive Programming System is a proprietary conversational operating system that uses an easytounderstand tabbed format with fullcolor graphics to guide the operator through the steps necessary to machine a part. First, the control leads the operator through basic job setup: setting tool and work offsets, selecting the tool type and specifying the material being cut. The operator then selects an operation to perform and fills in basic information as prompted. Default values are automatically filled in for spindle speed, depth of cut and feedrate based on the information provided, but the operator can change these conservative values if desired. Once all necessary information is entered, pushing Cycle Start performs the desired operation. Multiple operations can be recorded and saved as a single Gcode program that can be played back to duplicate the part. This program can be transferred to any other Haas VMC and run without editing. Help menus are available directly on screen, and a graphic dryrun feature allows operators to check their work before running a part. Novice operators quickly learn both basic programming and the finer points of using the Haas control by working with the Intuitive Programming System. Hard Drive with Ethernet Interface Store and transfer data between your Haas and a network or PC with the Ethernet connection. Program files are easily transferred to and from memory or the internal hard drive, and large files can be accessed by multiple machines. Highspeed data transfers allow DNC of large files at up to 1,000 blocks per second. Compatible with Windows 95, 98, ME, 2000 and XP. Also works with server versions NT 4.0, 2000 and 2003. IPX/SPX or TCP/IP protocol. Easily set up from the control screen. 32 Memory Lock Keyswitch Locks memory to prevent program editing by unauthorized personnel. It can also be used to lock settings, parameters, offsets and macro variables. 8 M Functions Adds 8 additional M functions for a total of up to 13 user interfaces. Use these to activate probes, auxiliary pumps, clamping devices, part loaders, etc. HighSpeed Machining The HighSpeed Machining option is a powerful tool to reduce cycle times and improve accuracy. Testing on complex 3to 5axis applications has shown drastic reductions in cycle times, as well as increased accuracy and smoother motion. Using a motion algorithm called "acceleration before interpolation," combined with up to 80 blocks of lookahead, the HSM option allows contouring feedrates up to 833 ipm without risk of distortion to the programmed path. Programmed motions are accelerated before interpolation to ensure that the movement of each axis does not exceed the acceleration capability of the machine. The lookahead algorithm determines the fastest feedrate at which each stroke can be blended into the next without stopping. This results in higher accuracy, smoother motion and a higher actual feedrate even with complex part geometry. Many of today's "highspeed" controls are either very expensive or require a preprocessing mode or special post, which is time consuming and alters the Gcode program. The Haas HSM option accepts ISO standard G code from all major CAM systems, and is nly a fraction of the cost of other highspeed controls. Engraving By using a single block of code, you can easily engrave any text string enclosed in parentheses. Sequential part numbers can be engraved by using the standard serializing function. UserDefinable Macros Create subroutines for custom canned cycles, probing routines, operator prompting, math equations or functions, and familyofparts machining with variables. Memory Upgrades up to 16 MB Allows loading of large programs directly into the machine, rather than from DNC, for faster feedrates. Batterypowered, highspeed static RAM is faster than dynamic RAM and retains data even when the power is turned off. 4th and 5thAxis Control Allows the use of 4th and 5thaxis rotary tables for multiside machining or machining complex contours and shapes, such as impellers. Increases productivity and reduces the number of setups required. USB Port The USB port allows the use of customersupplied external drives or flash memory devices. Coordinate Rotation/Scaling Use rotation in conjunction with work offset probing to speed workpiece set up, or use it to rotate a pattern to another location or around a circumference, etc. Use scaling to reduce or enlarge a toolpath or pattern Second Home Position Allows the operator to quickly send the axes to a userdefined Home position other than the machine's Home position. Color Remote Jog Handle The patented Haas color remote jog handle expands the capabilities of our standard remote jog handle by adding a 2.8" color graphic display, an 11button keypad, a tripleknob motioncontrol system and a builtin LED inspection light. You can set tool and work offsets, jog up to 9 axes, display machine position, show the current program running and much more all from the jog handle. Some items shown in this brochure are optional. Please contact your local distributor for assistance. 33 The Hidden Power Inside the HELP/CALC The Help function is a builtin, searchable operator's manual that explains the various functions of a Haas machine. Simply type in a keyword to quickly find a specific topic, or hit F1 for Gcode help and F2 for Mcode help. The Calculator pages are another powerful tool. There are calculators for solving triangle equations, circlecircletangent equations and circlelinetangent equations, as well as a speedsandfeeds calculator. Also included are a standard math calculator, a drillandtap chart, a decimalequivalent chart and a timeanddate function. These calculators simplify machining operations and speed math calculations, and the solution to any equation can easily be pasted into a program directly from the calculators. The Power of a Single Button Some of the most powerful features of the Haas control features that every machinist will truly appreciate take only the push of a single button. For example, you can set tool offsets with the push of a single button without having to enter numbers manually into the control. Simply jog a tool to the surface of the part, push the Tool Offset Measure button, and the tool's length is automatically stored in the tool length register. Now, push the Next Tool button and repeat the process for each tool. That's it! Setting work offsets is just as easy. These timeconsuming processes have been reduced to a few simple steps, and that's just two of the special features inside every Haas control. Ask your distributor for a complete demonstration, and see for yourself how a Haas will change the way you work. Tool Load Monitoring Maximizing tool life is another key to increasing productivity. The Haas control can monitor the spindle load for each tool and automatically adjust the feeds for that tool if the load exceeds a limit set by the operator. If a tool exceeds the preset limit, the control can be set to reduce the commanded feedrate, alert the operator, go into feedhold mode or generate a tooloverload alarm. The first time a program is run, the Haas control automatically records the highest load seen for each tool. Using this information and the Tool Load Monitoring feature of the control, the operator can set load limits for each tool. This maximizes tool life, and protects the workpiece and machine from the effects of tool wear. Specifications subject to change without notice. Not responsible for typographical errors. 34 Haas Control Advanced Tool Management To maximize productivity, the Haas control has an integrated Advanced Tool Manager that allows you to create a group of redundant tools for use within a program. From a single screen, you can view the different tool groups and their parameters. Simply define which tool numbers are part of a group, and what parameter will determine when to change to a redundant tool. This can be based on feed time, the number of tool calls, the number of holes drilled or tapped, or a preset load limit. To use a group of redundant tools in a program, simply enter the group number as your tool callout. The tool offsets you defined during set up will automatically be loaded for each tool as it's called up. SETNG /GRAPH Push this button to access the Settings pages of the Haas control, where you'll find a wide selection of operatordefinable preferences. Use these settings to optimize the way you work. You can set program restarts and automatic poweroff, select languages and units of measure, lock out overrides and parameters, access special features like electronic thermal compensation and much more. The Graphics page provides a 2D representation of the programmed toolpath. Use this graphic dry run to identify possible problems and avoid mishaps. CURNT/COMDS The Current Commands page displays the current running status of the machine, including the current program running, the current position, which tool is in the spindle, the spindle and axis loads, the current spindle speed and the feedrate. Additional screens show which commands and G code are being used in the current program; and a timer shows cycle time, cutting time, poweron time and M30 count (number of parts). Other displays show which macro variables are being used, provide toollife information, and show the minimum and maximum spindle load for each tool. Some items shown in this brochure are optional. Please contact your local distributor for assistance. 35 Haas Wireless Intuitive Probing System The Haas Wireless Intuitive Probing System (WIPS), with optical transmission for part setting, tool setting and inspection, consists of the following elements: · Spindle Probe Module (work probe) · Tool Setter Module (tool probe) · Intuitive Probing System Sofware The Haas Wireless Intuitive Probing System makes probing easy to understand and use through simple language, a graphical interface and clear instructions. Stepbystep graphical instructions show machine operators how to set up the probing cycles. The Haas Intuitive Probing System software guides the operator through the probing setup process, prompting them to enter each necessary dimension. Once all dimensions are entered, the operator executes the probing cycle by pushing the Cycle Start button. The probing cycle can then be saved in memory, and recalled when needed. With the Haas Intuitive Probing System, no knowledge of Gcode programming is needed to use the probing system. WIPS is available as a factoryinstalled option on most new Haas HMCs. Operator Convenience Features Enclosed Tool Presetter The WIPS tool probe is attached to a rigid, fixed arm for accuracy, and located outside the work envelope, so it does not interfere with machining. A sheetmetal cover protects the probe, and prevents chips from sticking to the probe tip. Tool Rack System This versatile rack provides convenient storage for toolholders, cutting tools and accessories right at the machine, eliminating the need for a separate tool cart. The system comes with one rack, a shelf and a storage box; extra racks are available. 36 Machine Dimensions 300 400 500 A 1600 2000 3000 A EC MODEL LINE EC MODEL LINE B B C C A B C D E F G H J K EC300 122.8" 3119 mm 133.5" 3391 mm 93.9" 2385 mm 20.3" 516 mm 2.35" 60 mm 1.55" 39 mm 14.0" 356 mm 18.0" 457 mm 10.0" 254 mm 10.0" 254 mm EC400 134.0" 3404 mm 143.8" 3653 mm 103.4" 2626 mm 22.2" 564 mm 2.1" 53 mm 4.0" 102 mm 20.0" 508 mm 20.0" 508 mm 14.5"1 368 mm 10.0" 254 mm EC500 145.8" 3703 mm 165.0" 4191 mm 101.4" 2576 mm 21.1" 536 mm 1.1" 28 mm 3.94" 100 mm 28.0" 711 mm 20.0" 508 mm 20.8"1 528 mm 16.0" 406 mm EC1600 172.8"2 4389 mm 142.6"2 3622 mm 119.0"2 3023 mm *51.5" 1308 mm *11.5" 292 mm 8.0" 203 mm 32.0" 813 mm 40.0" 1016 mm 32.0" 813 mm 32.0" 813 mm EC2000 194.5"2 4940 mm 142.6"2 3622 mm 119.0"2 3023 mm 51.5" 1308 mm 11.5" 292 mm 8.0" 203 mm 32.0" 813 mm 40.0" 1016 mm 42.0" 1067 mm 42.0" 1067 mm EC3000 265.8"2 6751 mm 142.6"2 3622 mm 119.0"2 3023 mm 51.5" 1308 mm 11.5" 292 mm 8.0" 203 mm 32.0" 813 mm 40.0" 1016 mm 60.0" 1524 mm 60.0" 1524 mm HS3 366.0" 9296 mm 189.0" 4801 mm 152.0" 3861 mm 55.5" 1410 mm 5.5" 140 mm 5.8" 147 mm 60.0" 1524 mm 50.0" 1270 mm 75.0" 1905 mm 75.0" 1905 mm HS4 366.0" 9296 mm 189.0" 4801 mm 168.0" 4267 mm 71.5" 1816 mm 5.5" 140 mm 5.8" 147 mm 60.0" 1524 mm 66.0 1676 mm 75.0" 1905 mm 75.0" 1905 mm HS6 253.0" 6426 mm 189.0" 4801 mm 152.0" 3861 mm 55.5" 1410 mm 5.5" 140 mm 5.8" 147 mm 60.0" 1524 mm 50.0" 1270 mm 42.0" 1067 mm 42.0" 1067 mm HS7 253.0" 6426 mm 189.0" 4801 mm 169.0" 4293 mm 71.5" 1816 mm 5.5" 140 mm 5.8" 147 mm 60.0" 1524 mm 66.0" 1676 mm 42.0" 1067 mm 42.0" 1067 mm 1) Includes additional travel to reach tool probe. 2) With optional enclosure. C L K J H D C L HS 3 / 4 / 6 / 7 Max. Depth B C G Line F E C L Gage D E 45.5" 1156 mm 5.5" 140 mm *These measurements reflect only the EC1600 with optional builtin 4th axis. A Specifications subject to change without notice. Not responsible for misprints or typographical errors. Note: Overall shipping dimensions vary; contact Haas for details. 37 Machine Specifications 40Taper Models EC300 X 20" 508 mm 18" 457 mm 14" 356 mm 11.81" 300 mm 4.7 sec 550 lb 250 kg 210 ftlb 285 Nm 200 ftlb 271 Nm ± 15 arcsec 5.6 sec CT 40 or BT 40 8,000 max rpm Inline Direct Drive 75 ftlb @ 1,400 102 Nm @ 1400 20 hp 14.9 kW 12,000 max rpm Inline Direct Drive 75 ftlb @ 2,100 102 Nm @ 2100 30 hp 22.4 kW 2,400 lb 10 676 N 1,000 ipm 25.4 m/min 500 ipm 12.7 m/min 24+1 | 40+1 CT 40 std | BT 40 opt 3" | 6" 76 mm | 152 mm 2.8 sec 4.5 sec ±0.0002" ±0.00 5 mm ±0.0001" ±0.00 3 mm 15,500 lb 7031 kg 55 gallon (208 liter) 9 scfm @ 100 psi 255 lpm @ 6.9 bar 195 260 VAC 354 488 VAC (Find more specifications, dimensions and detailed information online at 50Taper Models EC400 | 400PP 20" 508 mm 20" 508 mm 20" 508 mm 15.75" 400 mm 8.0 sec 1,000 lb 454 kg ± 3 arcsec 3.6 sec 660 lb 300 kg 300 ftlb 407 Nm 500 ftlb 678 Nm ± 15 arcsec 5.5 sec CT 40 or BT 40 8,000 max rpm Inline Direct Drive 75 ftlb @ 1,400 102 Nm @ 1400 20 hp 14.9 kW 12,000 max rpm Inline Direct Drive 75 ftlb @ 2,100 102 Nm @ 2100 30 hp 22.4 kW 4,600 lb 20 462 N 1,000 ipm 25.4 m/min 500 ipm 12.7 m/min 24+1 | 40+1, 70+12 CT 40 std | BT 40 opt 3" | 6" 76 mm | 152 mm 2.1 sec2 3.7 sec2 ±0.0002" ±0.00 5 mm ±0.0001" ±0.00 3 mm 20,000 lb | 27,000 lb 9 072 kg | 12 247 kg 80 gallon (303 liter) 9 scfm @ 100 psi 255 lpm @ 6.9 bar 195 260 VAC 354 488 VAC EC500 32" 813 mm 20" 508 mm 28" 711 mm 19.69" 500 mm 9.0 sec 1,000 lb 454 kg ± 3 arcsec 3.6 sec 660 lb 300 kg 300 ftlb 407 Nm 500 ftlb 678 Nm ± 15 arcsec 5.5 sec CT 40 or BT 40 8,000 max rpm Inline Direct Drive 75 ftlb @ 1,400 102 Nm @ 1400 20 hp 14.9 kW 12,000 max rpm Inline Direct Drive 75 ftlb @ 2,100 102 Nm @ 2100 30 hp 22.4 kW 4,600 lb 20 462 N 1,000 ipm 25.4 m/min 500 ipm 12.7 m/min 40+1 | 70 +1 CT 40 std | BT 40 opt 3" | 6" 76 mm | 152 mm 1.6 sec. 2.8 sec. ±0.0002" ±0.00 5 mm ±0.0001" ±0.00 3 mm 28,000 lb 12 701 kg 95 gallon (360 liter) 9 scfm @ 100 psi 255 lpm @ 6.9 bar 195 260 VAC 354 488 VAC X Travels Y Z Size Travels Y Z Width Length Pallets Pallet Change Time Capacity: Indexer Table TSlot Width Max Weight on Table Platter Diameter Indexer (standard) Indexing Accuracy 90° Rotation Time Capacity: Full 4th Axis Optional 4th Axis Rotational Torque Brake Torque Indexing Accuracy 90° Rotation Time Taper Speed Drive System Max Torque Spindle Motor Max Rating1 Speed Drive System Optional 4th Axis Rotational Torque Brake Torque Max Weight on Platter Taper Speed Drive System Max Torque Standard Spindle Motor Max Rating1 Speed Drive System Spindle (standard) Spindle (standard) Spindle (optional) Max Torque Standard Spindle Motor Max Rating1 Axis Motors Max Thrust Rapids Max Cutting Capacity Standard | Optional Tool Type / Taper Max Tool Diameter full | adjacent empty Tool to Tool Chip to Chip Positioning Spindle (optional) Max Torque Spindle Motor Max Rating1 Axis Motors Max Thrust Axis Motors Axis Motors Rapids Max Cutting Capacity Standard | Optional Tool Type / Taper Max Tool Diameter full | adjacent empty Tool to Tool Chip to Chip Positioning Tool Changer Tool Changer Accuracy Accuracy Repeatability Machine Weight Coolant Capacity Air Required Power Required (min) Repeatability Machine Weight Coolant Capacity Air Required Power Required (min) Miscellaneous Miscellaneous 1) 5minute rating. 2) The EC400PP comes standard with 70+1 tools. Change times are 1.6 sec (TT) and 2.8 sec (CC). 3) With optional builtin 4th axis, subtract 4" (100 mm). 4) Linear scales required to achieve stated accuracy. Please go to www.HaasCNC.com for more product details and information. 38 www.HaasCNC.com. Select HMCs and then Model Guide for specific information right at your finger tips.) EC1600 64" 1 626 mm 40" 1 016 mm 32" 813 mm 36"3 914 mm 64" 1626 mm 5/8" 16 mm 10,000 lb 4536 kg 30" 762 mm 2000 ftlb 2712 Nm 4,000 ftlb 5423 Nm 10,000 lb 4536 kg #50 Taper 6,000 max rpm 2Speed Geared Head 450 ftlb @ 500 rpm 610 Nm @ 500 30 hp 22.4 kW 10,000 max rpm 2Speed Geared Head 250 ftlb @ 600 rpm 339 Nm @ 600 rpm 30 hp 22.4 kW x = 5,600 lb | 24 910 N y = 5,600 lb | 24 910 N z = 7,500 lb | 33 362 N x = 540 ipm | 13.7 m/min y = 540 ipm | 13.7 m/min z = 540 ipm | 13.7 m/min 500 ipm 12.7 m/min 30+1 | 50+1 CT 50 std | BT 50 opt 4" | 10" 102 mm | 254 mm 10.3 sec 12.6 sec ±0.0003"4 ±0.008 mm ±0.0002"4 ±0.005 mm 30,000 lb 13 608 kg 95 gallon (360 liter) 4 scfm @ 100 psi 113 lpm @ 6.9 bar 195 260 VAC 354 488 VAC EC2000 84" 2 134 mm 40" 1 016 mm 32" 813 mm 36" 914 mm 84" 2134 mm 5/8" 16 mm 10,000 lb 4536 kg 30" 762 mm 2000 ftlb 2712 Nm 4,000 ftlb 5423 Nm 10,000 lb 4536 kg #50 Taper 6,000 max rpm 2Speed Geared Head 450 ftlb @ 500 rpm 610 Nm @ 500 30 hp 22.4 kW 10,000 max rpm 2Speed Geared Head 250 ftlb @ 600 rpm 339 Nm @ 600 rpm 30 hp 22.4 kW x = 3,400 lb | 15 124 N y = 5,600 lb | 24 910 N z = 7,500 lb | 33 362 N x = 540 ipm | 13.7 m/min y = 540 ipm | 13.7 m/min z = 540 ipm | 13.7 m/min 500 ipm 12.7 m/min 30+1 | 50+1 CT 50 std | BT 50 opt 4" | 10" 102 mm | 254 mm 10.3 sec 12.6 sec ±0.0003"4 ±0.008 mm ±0.0002"4 ±0.005 mm 31,500 lb 14 288 kg 95 gallon (360 liter) 4 scfm @ 100 psi 113 lpm @ 6.9 bar 195 260 VAC 354 488 VAC EC3000 120" 3 048 mm 40" 1016 mm 32" 813 mm 28" 711 mm 120" 3048 mm 5/8" 16 mm 10,000 lb 4536 kg #50 Taper 6,000 max rpm 2Speed Geared Head 450 ftlb @ 500 rpm 610 Nm @ 500 30 hp 22.4 kW 10,000 max rpm 2Speed Geared Head 250 ftlb @ 600 rpm 339 Nm @ 600 rpm 30 hp 22.4 kW x = 3,400 lb | 15 124 N y = 5,600 lb | 24 910 N z = 7,500 lb | 33 362 N x = 360 ipm | 9.1 m/min y = 540 ipm | 13.7 m/min z = 540 ipm | 13.7 m/min 360 ipm 9.1 m/min 30+1 | 50+1 CT 50 std | BT 50 opt 4" | 10" 102 mm | 254 mm 10.3 sec 12.6 sec ±0.0003"4 ±0.008 mm ±0.0002"4 ±0.005 mm 37,500 lb 17 010 kg 95 gallon (360 liter) 4 scfm @ 100 psi 113 lpm @ 6.9 bar 195 260 VAC 354 488 VAC HS3 150" 3 810 mm 50" 1 270 mm 60" 1524 mm 40" 1016 mm 146" 3708 mm 0.87" 22 mm 10,000 lb 4536 kg (HS3R) 37" 940 mm 2000 ftlb 2712 Nm 4,000 ftlb 5423 Nm 10,000 lb 4536 kg #50 Taper 5,000 max rpm 2Speed Geared Head 450 ftlb @ 500 rpm 610 Nm @ 500 30 hp 22.4 kW x = 5,040 lb | 22 419 N y = 5,600 lb | 24 910 N z = 7,500 lb | 33 362 N x = 500 ipm | 12.7 m/min y = 500 ipm | 12.7 m/min z = 710 ipm | 18.0 m/min 500 ipm 12.7 m/min 38 | 60, 90, 120 CT 50 std | BT 50 opt 4.9" | 9.8" 125 mm | 250 mm 4.9 sec 15.8 sec ±0.0002" per 24" 0.005 mm per 610 mm ±0.0002"2 ±0.005 mm 62,000 lb 28 123 kg 95 gallon (360 liter) 9 scfm @ 100 psi 255 lpm @ 6.9 bar 195 260 VAC 354 488 VAC HS4 150" 3 810 mm 66" 1676 mm 60" 1524 mm 40" 1016 mm 146" 3708 mm 0.87" 22 mm 10,000 lb 4536 kg (HS4R) 37" 940 mm 2000 ftlb 2712 Nm 4,000 ftlb 5423 Nm 10,000 lb 4536 kg #50 Taper 5,000 max rpm 2Speed Geared Head 450 ftlb @ 500 rpm 610 Nm @ 500 30 hp 22.4 kW x = 5,040 lb | 22 419 N y = 5,600 lb | 24 910 N z = 7,500 lb | 33 362 N x = 500 ipm | 12.7 m/min y = 500 ipm | 12.7 m/min z = 710 ipm | 18.0 m/min 500 ipm 12.7 m/min 38 | 60, 90, 120 CT 50 std | BT 50 opt 4.9" | 9.8" 125 mm | 250 mm 4.9 sec 15.8 sec ±0.0002" per 24" ±0.005 mm per 610 mm ±0.0001" ±0.003 mm 63,000 lb 28 576 kg 95 gallon (360 liter) 9 scfm @ 100 psi 255 lpm @ 6.9 barr 195 260 VAC 354 488 VAC HS6 84" 2134 mm 50" 1 270 mm 60" 1524 mm 40" 1016 mm 80" 2032 mm 0.87" 22 mm 10,000 lb 4536 kg (HS6R) 37" 940 mm 2000 ftlb 2712 Nm 4,000 ftlb 5423 Nm 10,000 lb 4536 kg #50 Taper 5,000 max rpm 2Speed Geared Head 450 ftlb @ 500 rpm 610 Nm @ 500 30 hp 22.4 kW x = 5,040 lb | 22 419 N y = 5,600 lb | 24 910 N z = 7,500 lb | 33 362 N x = 500 ipm | 12.7 m/min y = 500 ipm | 12.7 m/min z = 710 ipm | 18.0 m/min 500 ipm 12.7 m/min 38 | 60, 90, 120 CT 50 std | BT 50 opt 4.9" | 9.8" 125 mm | 250 mm 4.9 sec 15.8 sec ±0.0002" per 24" 0.005 mm per 610 mm ±0.0001" ±0.003 mm 57,000 lb 25 855 kg 95 gallon (360 liter) 9 scfm @ 100 psi 255 lpm @ 6.9 bar 195 260 VAC 354 488 VAC HS7 84" 2134 mm 66" 1676 mm 60" 1524 mm 40" 1016 mm 80" 2032 mm 0.87" 22 mm 10,000 lb 4536 kg (HS7R) 37" 940 mm 2000 ftlb 2712 Nm 4,000 ftlb 5423 Nm 10,000 lb 4536 kg #50 Taper 5,000 max rpm 2Speed Geared Head 450 ftlb @ 500 rpm 610 Nm @ 500 30 hp 22.4 kW x = 5,040 lb | 22 419 N y = 5,600 lb | 24 910 N z = 7,500 lb | 33 362 N x = 500 ipm | 12.7 m/min y = 500 ipm | 12.7 m/min z = 710 ipm | 18.0 m/min 500 ipm 12.7 m/min 38 | 60, 90, 120 CT 50 std | BT 50 opt 4.9" | 9.8" 125 mm | 250 mm 4.9 sec 15.8 sec ±0.0002" per 24" 0.005 mm per 610 mm ±0.0001" ±0.003 mm 58,000 lb 26 308 kg 95 gallon (360 liter) 9 scfm @ 100 psi 255 lpm @ 6.9 bar 195 260 VAC 354 488 VAC NOTE: FLA/kVA requirements determined by motor horsepower. Check with your Haas distributor for various requirements. Differing VAC/kVA options available. Specifications subject to change without notice. Not responsible for misprints or typographical errors. 39 Worldwide Support U.S. headquarters & manufacturing facility headquarters & showroom · Euarcohpienaeninventory and spare parts with m distribution center (Brussels) headquarters & · Asaicahnine inventory andshowroom with m spare parts distribution center (Shanghai) More than $50,000,000 in spare parts are stocked at 160 locations worldwide. European Headquarters, Brussels, Belgium Asian Headquarters, Shanghai, China Head Office, California, USA Our network of dedicated Haas Factory Outlets provides local attention to detail, fully stocked service vans, and the training and backing of an international organization. In total, more than $50,000,000 in spare parts are stocked at 160 locations worldwide. Local parts inventories are supported by overnight availability from main headquarters. Haas Automation, Inc. 2800 Sturgis Road, Oxnard, California 93030 · Toll Free: 8003316746 Fax: 8052788540 www.HaasCNC.com Haas Automation, Europe Mercuriusstraat 28, B1930 Zaventem, Belgium · Tel: 01132 2 522 99 05 Fax: 01132 2 523 08 55 Haas Automation, Asia No. 96 Yi Wei Road, Building 67, Waigaoqiao FTZ, Shanghai 200131 PR.C. · Tel: 01186 21 3861 6666 Fax: 01186 21 3861 6799 . 39902028
You need to upgrade your Flash Player
Viewing this eBook requires Adobe Flash Player version 8 or above.
Click below to download the latest version: