VERTICAL MACHINING CENTERS V Haas Automation Inc. onstant improvement is a way of life at Haas Automation. We're always looking for ways to improve our CNC products and give you our customers more value. Normally, we roll these incremental improvements into production without fanfare you simply get a better machine. For our newgeneration vertical machining centers, however, we redesigned the entire product line to incorporate a wide range of enhancements that make Haas VMCs better than ever before. Our engineers reviewed all aspects of the machines including motion control, coolant containment, chip evacuation, ergonomics, and serviceability then made improvements, and put everything into an allnew package. In this brochure you'll find all the latest technological advancements, new machine sizes, and capabilities that Haas Automation has developed through constant research and ongoing product refinement. C Contents The Haas control Rigid foundation Motion control Spindle & spindle drive Toolchangers Chip removal & coolant systems Operator convenience Model variations Machine configurations Performance enhancements Rotary tables & indexers Dimensions & specifications 413 1415 1617 1821 2223 2427 2829 30 31 3235 3839 4145 Haas Automation, Inc. 8003316746 www.HaasCNC.com | 1 MODEL Our customerfirst focus: · Published pricing policy The published price is what you pay. We're still the only CNC builder to make this promise. · Ontime delivery We build the entire machine and control inhouse utilizing the most advanced shop floor ERP (enterprise resource planning) system in the world. There's no fingerpointing around here. 2 | America's Leading Machine Tool Builder 2010 010 SE OF COMMON COMPONENTS, OSEBUILT FACTORY, HIP IIN THE INDUSTRY. N T H E I N D U S T RY · Fast service promise Every local HFO fields fully stocked service vans and provides a "rightnow" response. · Fair spares pricing We're not interested in gouging a customer in need. Your loyalty is more important. · Great resale value Year after year, Haas machines bring the highest documented resale value in the industry. Haas Automation, Inc. 8003316746 www.HaasCNC.com | 3 TAKE CONTROL The Haas CNC Control The command center of your Haas machine tool. Years of development have gone into designing the best control hardware and software in the industry. Our newgeneration VMCs pack even more innovation into what was already the industry's greatest overall CNC control. To ensure smooth, precise motion control, Haas VMCs use nextgeneration digital servomotors and highresolution encoders on all axes. Combined with significant software and motorcontrol advancements, these yield better surfacefinish performance than ever before. Main Features Closed System Our focus is to provide a robust, dependable control that is seamlessly integrated with the machine. Our closed system is optimized specifically for Haas machines, and does not rely on thirdparty NC suppliers. When you call Haas, you get a company that takes full responsibility for the entire machine. The Haas keypad has a full array of keys, including a complete alphanumeric keypad, and all common functions are clearly labeled for operator ease. If you've ever fumbled with hot keys, or had to page through screens looking for a specific function, you will appreciate the simplicity of the Haas control. There are no encrypted codes to memorize, and most functions can be performed with the push of a single button. Dedicated Keypad OneButton Features Common multistep functions, such as poweringup the machine or setting tool offsets, have been reduced to the push of a single button. Other oftenused functions, such as setting work offsets, homing the machine, and selecting the next tool during set up, are also onebutton commands. Most machines use the jog handle only to move the axes around. On Haas machines, the jog handle can also be used in other modes to cursor through the program for faster editing, override spindle speeds and feedrates, or scan through offsets, parameters, etc. MultiFunction Jog Handle 15" Color LCD Screen Our fullcolor, 15" TFT LCD display is designed to work in the machine shop environment. The highintensity, highcontrast LCD features a very wide viewing angle, and will not fade out in bright light. The panel is mounted behind antiglare, tempered glass for protection and easy viewing. Advanced Program Editing A unique feature of the Haas control is an advanced program editor that allows the operator to edit programs in a dualwindow format. The builtin USB port allows the use of customersupplied USB flash memory devices or external hard drives. 4 | America's Leading Machine Tool Builder USB Port RETHINKING THE OBVIOUS Threescreen simplicity From the very beginning, the Haas control was designed to be the industry's most userfriendly CNC available. Reliability and longevity have been its reputation, for sure. But the main thing you hear Haas owners tell other machinists is that a Haas is the easiesttooperate CNC machine tool they have ever seen. It's what a Haas control is all about. The Haas control's threescreen system gives users access to every control feature needed in each mode without having to leave the current display screen. Here are some examples of how the screens look and function. The Setup Screen Above is the Setup screen. It's simple: This is where you do all your machine setups. Let's take a look at the information on the screen: The Active Program box is displayed in the upper left. The Tool Offsets are displayed in the upper right. Below the tool offsets are the Work Zero Offsets. Below left, is the Spindle Information box displaying spindle speed, plus any override values for spindle speed, feedrate, and rapid rate. Next to that is the Position box, showing operator, work offset, machine, and distancetogo coordinates. To the right of the position box is the Tool Management information. Simple, clean, and easy to understand. Notice that the tool offset box (upper right) is white and the other boxes are colored. This indicates the box is active, and the cursor can be moved within the box by pressing the keypad arrow keys. 6 | America's Leading Machine Tool Builder The Edit Screen After setting your offsets in the Setup screen, you'll probably need to load a program. Pressing the List Programs button on the keypad brings up the Edit screen, where you can access programs from any of the devices attached to the machine (i.e., internal memory, USB stick, Ethernet, etc.). A powerful feature in the Edit screen is the QuickKey help menu, which offers a complete list and description of all functions, including List Programs and file navigation. In the QuickKey help menu, you'll see the command name and the associated key for each function, along with a full description of how to perform each function. There are extensive QuickKey help menus available from all three screens of the control interface. In the lowerleft corner of the Edit screen is the Editor Help box, which displays a description for each available topic. At the bottomright side of the edit screen is a viewable Clipboard. Whenever you cut or copy a selection, it will be displayed in the Clipboard box. Within the Edit screen are numerous other functions that relate to program editing, like Program Simulate (now with control over the draw speed), a secondary program display window for alternate programs, the MDI function, and Visual Quick Code capabilities. On the Operation screen, you'll find all the information needed to run the machine organized and available for easy access. Here's a quick look: In the upperleft corner is the Program Display box. When executing programs containing subprograms, both the main and the subprogram will be displayed in a splitscreen box. Just to the right are the Active GCodes, with text descriptions, the Coolant Level Indicator, and the Active Tool information, including a graphic image of the tool type, as specified on the Tool Offset page. In the center of the screen is the Offset Window. Here, you can make adjustments to any offset while the machine is running. You don't have to exit the Operation screen to change an offset. Along the bottom on the left, note the Spindle Information box, with the override displays. In the center is the Position display box, and to the right are the Timers and Counters. Experienced machinists will really like the Remaining timer, which uses information from the Last Cycle timer to display the time remaining in a program. This lets the operator know how much time is remaining in the cycle, allowing better timemanagement decisions when leaving the machine unattended. The Operation Screen Haas Automation, Inc. 8003316746 www.HaasCNC.com | 7 THE HIDDEN POWER IN THE HAAS CONTROL 8 | America's Leading Machine Tool Builder Remote Jog Handle The patented Haas color remote jog handle features a 2.8" color graphic display, an 11button keypad, a tripleknob motioncontrol system, and a builtin LED inspection light. You can set tool and work offsets, jog up to 9 axes, display machine position, show the current program running, and much more all from the jog handle. The Current Commands page displays the current running status of the machine, including the current program running, the current position, which tool is in the spindle, the spindle and axis loads, the current spindle speed, and the feedrate. Additional screens show which commands and Gcodes are being used in the current program; and a timer shows cycle time, cutting time, poweron time, and M30 count (number of parts). Other displays show which macro variables are being used, provide toollife information, and show the minimum and maximum spindle load for each tool. CURNT/COMDS The Help function is a builtin, searchable operator's manual that explains the various functions of a Haas machine. Simply type in a keyword to find a specific topic, or hit F1 for Gcode help and F2 for Mcode help. The Calculator pages are another powerful tool. There are calculators for solving triangle equations, circlecircletangent equations, and circlelinetangent equations, as well as a speedsandfeeds calculator. Also included are a standard math calculator, a drillandtap chart, and a decimalequivalent chart. These calculators simplify machining operations and speed math calculations, and the solution to any equation can be pasted into a program directly from the calculators. HELP/CALC The Power of a Single Button Some of the most powerful features of the Haas control features every machinist will appreciate take only the push of a single button. For example, you can set tool offsets with the push of a single button without having to manually enter numbers into the control. Simply jog a tool to the surface of the part, push the Tool Offset Measure button, and the tool's length is automatically stored in the tool length register. Push the Next Tool button to repeat the process for each tool. That's it! Setting work offsets is just as easy. These timeconsuming processes have been reduced to a few simple steps. Maximizing tool life is another key to increasing productivity. The Haas control can monitor the spindle load for each tool, and automatically adjust the feeds if the load exceeds a limit set by the operator. If a tool exceeds the preset limit, the control can be set to reduce the commanded feedrate, alert the operator, go into feedhold mode, or generate a tooloverload alarm. The first time a program runs, the Haas control automatically records the highest load seen for each tool. Using this information and the Tool Load Monitoring feature of the control, the operator can set load limits for each tool. This maximizes tool life, and protects the workpiece and machine from the effects of tool wear. ToolLoad Monitoring To maximize productivity, the Haas control has an integrated Advanced Tool Manager that allows you to create a group of redundant tools for use within a program. From a single screen, you can view the different tool groups and their parameters. Simply define which tool numbers are part of a group, and what parameter will determine when to change to a redundant tool. This can be based on feed time, the number of tool calls, the number of holes drilled or tapped, or a preset load limit. To use a group of redundant tools in a program, simply enter the group number as your tool callout. The tool offsets you defined during set up are automatically loaded for each tool as it's called up. Advanced Tool Management Haas Automation, Inc. 8003316746 www.HaasCNC.com | 9 UPGRADES: options With the Haas Intuitive Programming System, it's no longer necessary for a machine operator to know Gcode to perform basic milling operations. The Haas Intuitive Programming System is a proprietary conversational operating system that uses an easytounderstand tabbed format with fullcolor graphics to guide the operator through the steps necessary to machine a part. First, the control leads the operator through basic job setup: setting tool and work offsets, selecting the tool type, and specifying the material being cut. The operator then selects an operation to perform and fills in basic information as prompted. Default values for spindle speed, depth of cut, and feedrate are filled in automatically, based on the information provided. The operator can change these conservative values if desired. Once all necessary information is entered, pushing Cycle Start performs the desired operation. Multiple operations can be recorded and saved as a single Gcode program that can be played back to duplicate the part. This program can be transferred to any other Haas VMC and run without editing. Help menus are available directly on screen, and a graphic dryrun feature allows operators to check their work before running a part. Intuitive Programming System 1. Use the top tab menu to select the type of operation to perform. 1 3 2. Further define your specific cutting operation by choosing from the lower set of tabs. 3. Fill in the information when prompted by the control and press Cycle Start. 2 Using plain language, simple graphics, and easytofollow steps, the Haas Intuitive Programming System guides the operator through the steps necessary to machine a part. 4th and 5thAxis Control Allows the use of 4th and 5thaxis rotary tables for multiside machining or machining complex contours and shapes, such as impellers. Increases productivity and reduces setups. Coordinate Rotation/Scaling Use rotation in conjunction with work offset probing to speed workpiece set up, or use it to rotate a pattern to another location or around a circumference, etc. Use scaling to reduce or enlarge a toolpath or pattern. Second Home Position Allows the operator to quickly send the axes to a userdefined Home position other than the machine's default Home position. Transfer data between your Haas and a network or PC with the Ethernet interface. Transfer program files easily to and from the machine, and access large files with multiple machines. Highspeed data transfers allow DNC of large files at up to 1000 blocks per second. Easily set up from the control screen. Ethernet Interface 10 | America's Leading Machine Tool Builder DXF File Import The *.dxf import capability of the Haas Intuitive Programming System allows a programmer to easily import a *.dxf file into the Haas control, select features on the file holes, threading, pockets, islands, or contours and generate the toolpath. The program output is standard Gcode easy to understand and edit. By taking advantage of the editing functions of the Haas control, the user can modify features, change the order of operations, or even conveniently put them into other programs all at the control, without going back to a computer to repost a CAMgenerated program. The Haas control provides the best of both Gcode and conversationalstyle systems. It doesn't force the user into one method of operation. The Haas control weaves them into a simple, coherent control system: Use manual or CAMgenerated Gcode, or use the Intuitive Programming System, or mix them. Use the programming strategy that is best for the part; the Haas control accepts them all. UserDefinable Macros Create subroutines for custom canned cycles, probing routines, operator prompting, math equations or functions, and familyofparts machining with variables. Engraving Using a single block of code, you can easily engrave any text string enclosed in parentheses. Engrave sequential part numbers using the standard serializing function. Adds 8 additional M functions for a total of up to 13 user interfaces. Use these to activate probes, auxiliary pumps, clamping devices, part loaders, etc. 8 M Functions Memory Lock Keyswitch Memory Upgrades Locks memory to prevent program editing by unauthorized personnel. Can also be used to lock settings, parameters, offsets, and macro variables. Expandable onboard solidstate memory allows storing, running, and editing large programs directly at the machine. Haas Automation, Inc. 8003316746 www.HaasCNC.com | 11 HSM BENEFITS · Greatly reduces cycle times The HighSpeed Machining option is a powerful tool to reduce cycle times and improve accuracy. Testing on complex 3 to 5axis applications shows drastic reductions in cycle times, as well as increased accuracy and smoother motion. Using a motion algorithm called "acceleration before interpolation," combined with full lookahead, the HSM option allows contouring feedrates up to 1200 ipm without risk of distortion to the programmed path. All programmed motions are accelerated before interpolation to ensure the movement of each axis does not exceed the acceleration capability of the machine. The lookahead algorithm determines the fastest feedrate at which each stroke can be blended into the next without stopping. This results in higher accuracy, smoother motion, and a higher actual feedrate even with complex part geometry. The Haas HSM option accepts ISO standard Gcode from all major CAM systems, and is only a fraction of the cost of other highspeed controls. HIGHSPEED MACHINING · Full lookahead · Up to 1200 ipm contouring · Acceleration before interpolation · ISO standard Gcode programming · Higher accuracy · Smoother motion 12 | America's Leading Machine Tool Builder Control Features Control Specifications General Microprocessor Program execution speed Axis control Interpolation Min. input increment Min. output resolution Feed Functions Rapid Traverse Override Feedrate Override Jog Handle Resolution Jog Feeds Zero Return Spindle Functions Speed Command Override Tool Functions Length Compensation Diameter/Radius Compensation Length Measurement Life Management Selection Programming Compatibility Positioning Canned Cycles Circular Pocket Milling BoltHole Drilling Advanced Pocket Milling Inch/Metric Work Coordinates Part Zero Set M Code Outputs 2D Cutter Diameter Compensation 2D Cutter Length Compensation 3D+ Cutter Diameter Compensation 5Axis Tool Length Compensation Data Input/Output Communications Port Data Rate Memory Capacity Standard Number of Programs Triple highspeed 32bit 1000 blocks/sec standard 3 axes linear, 4th and 5th axes optional G01, G02, G03, helical inch mode 0.0001" metric mode 0.001 mm 0.0000072" (0.000 18 mm) Userfriendly Advanced program editor Brushless AC servo drives Up to 1200 ipm cutting feedrates Triple 32bit processors Executes up to 1000 blocks/second ISO standard Gcode compatibility Haas onebutton powerup Haas onebutton tool offset entry 200 tool offsets 105 work coordinates Tool load monitoring Tool life management Helical interpolation Background editing Splitscreen program review Trig calculator Arc & tangent calculators Speeds and feeds calculator Run/stop/jog/continue RS232 / DNC / USB / optional Ethernet Midprogram restart Inch or metric programming Message page 15 selectable languages More than 200 userdefinable settings Selfdiagnostics Fully descriptive alarms Programmable mirrorimaging Advanced pocket milling Bolthole drilling Graphic dry run 5 spare M functions Contour accuracy control Text engraving Made in the USA 5%, 25%, 50%, 100% 0% to 999% in 1% increments inch mode 0.0001"/0.001"/0.01"/0.1" per handle division metric mode 0.001/0.01/0.1/1.0 mm per handle division inch mode 0.1/1.0/10.0/100.0 ipm metric mode 1.0/10/100/1000 mm/min. One key (G28) S = 1 to max spindle rpm 0% to 999% in 1% increments 200 sets, geometry & wear 200 sets, geometry & wear Automatic length storage 200 sets w/alarms Txx command ISO standard G code Absolute (G90), incremental (G91) 22 functions standard G12, G13 G70, G71, G72 G150 Switchable 105 sets Automatic storage 5 spare G40, G41, G42 G43, G44, G49 G141 G143 RS232, USB, optional 100BaseT Ethernet To 115,200 baud 1 MB; up to 250 MB optional 500 May be used by options. With 6' or shorter cable. Haas Automation, Inc. 8003316746 www.HaasCNC.com | 13 THE FOUNDATION FOR SUCCESS 14 | America's Leading Machine Tool Builder No matter what the project a family house, a skyscraper, or a suspension bridge the soundness of the structure is determined by the sturdiness of the foundation. The same principle applies to vertical machining centers. It all starts with the base and column structures. How well the machine cuts is tied to the sturdiness of the basic structure. A Rigid Platform Massive CastIron Construction Cast iron provides up to ten times the damping capacity of steel. That's why Haas uses cast iron for all major components. Our castings are reinforced with heavy ribs to resist flex and damp vibrations, and inspected thoroughly before and after machining to ensure they are free of flaws. Our triangulated widestance castings allow maximum structural loading with efficient use of materials. They provide a rigid and stable machining platform that resists flex, distributes cutting forces effectively, and is very thermally stable. Triangulated WideStance Castings All structural components are optimized using finite element analysis (FEA) to produce the most rigid designs. AntiFlex, Reinforced Base & Column Castings Our specially designed base and column castings feature antiflex, vibrationabsorbing ribs that transfer vibration away from the cutting area. The columns feature an internal torquetube design that yields superior rigidity and provides the most antiflex properties of any design. Haas Automation, Inc. 8003316746 www.HaasCNC.com | 15 MOTION CONTROL DoubleAnchored Ballscrews Haas uses only premiumquality ballscrews and guides from the world's top manufacturers. Although more expensive, their premium quality is the only way to achieve the high accuracy and long life that our customers demand. Ballscrews are anchored at both ends and inspected for 100% parallelism to the axis guides. Preloaded ball nuts eliminate backlash. Brushless Servomotors Haas uses stateoftheart, energyefficient brushless servomotors that offer more torque in a smaller frame than almost any other motors available. These highperformance servos provide more power for heavy cuts, and higher acceleration/deceleration rates to reduce cycle times. Highresolution encoders and closedloop digital feedback ensure ultraprecise positioning. Our servomotors are coupled directly to the ballscrews with steel disc couplings to eliminate windup, even under severe loading. This greatly improves positioning accuracy, and provides more accurate threading and contouring. And they don't wear out or lose accuracy over time. DirectCoupled Servomotors Haas uses a stateoftheart ballbar test to check the linear accuracy and geometry of every machine. Accurate to ±0.5 micron (±0.0000197"), with a 0.1micron (0.00000394") resolution, the ultraprecise ballbar tracks movement as the machine is put through a series of circular moves to certify synchronous movement and verify machine squareness. This generates a chart illustrating machine accuracy. Any deviations in squareness or accuracy show up as distorted circles that are very easy to spot. A copy of this chart ships with each Haas VMC as assurance that the machine is accurate and properly aligned. 100% Ballbar Tested 16 | America's Leading Machine Tool Builder Automatic Lubrication The Haas automatic lubrication system meters and distributes lube to guideways and ballscrews as the machine operates. This ensures that all critical components are properly lubricated at all times, saving time and reducing maintenance costs. Our system uses the minimal amount of lubrication necessary, eliminating waste oil and lessening environmental impact. Recirculating Ball Guideways Haas uses recirculating ball guideways for each axis of every VMC. These guideways are preloaded for zero clearance, and provide full loadcarrying capacity in all directions. They consume less power, do not require adjustment, and are proven to outperform sliding box ways for accuracy and speed. Each guideway is automatically lubricated to guarantee long life. Linear scales ensure positioning accuracy along X, Y, and Z axes by compensating for the thermal variations inherent in all machine tools. With a 1micron resolution, these scales deliver the extreme accuracy required for mold making and other highprecision machining applications. Linear Scales Recirculating Ball Guideways Outperform Box Ways Recirculating ball guideways are preloaded to provide zero clearance between the moving surfaces. This increases rigidity and stiffness in all directions, while providing higher accuracy and reliability. They have a very low coefficient of friction, which allows faster movements without sacrificing repeatability or positioning accuracy. Box ways require clearance between the moving surfaces in order to operate. They have a high coefficient of friction, which produces stickslip effects that can lead to machine errors. Electronic Thermal Compensation System Ballscrews generate heat when they rotate, which can cause them to expand. With high duty cycles, ballscrew growth can lead to cutting errors. Our electronic thermalcompensation (ETC) algorithm accurately models this heating effect and compensates for screw position. Recirculating Ball Guideway Box Way Zero Clearance Required Clearance Haas Automation, Inc. 8003316746 www.HaasCNC.com | 17 MAIN SPINDLE FEATURES Spindle Configurations Model TM · MM · VF1 · VF2 · VF3 · · VF4 · VF5 · · VF6 · · · VF7 · · · VF8 · · · VF9 · · · VF10 · · · VF11 · · · VF12 · · · VM · VR · VS GR · MDC · 40 TAPER 50 TAPER 2SPEED GEARBOX · · · (5K) · · · · · 4,000 / 5,000 RPM * · (4K) 6,000 RPM * 7,500 RPM 10,000 RPM HIGH 10,000 RPM * TORQUE 12,000 RPM * 15,000 RPM * 30,000 RPM * · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · *Not available on 50taper machines. Gearbox standard w/50taper spindle. Gearbox not compatible with all spindle options. All machines available in CT or BT. TM1P and TM3P only. Some items shown in this brochure are optional. Please contact your local distributor for assistance. 18 | America's Leading Machine Tool Builder The advanced design of our spindles provides high axialthrust capability, yet generates minimal heat. The front and rear bores of the housing and the OD of the spindle are finished in one operation. This guarantees perfect alignment between the bores and ODs, thus reducing bearing heat. Our spindles use preloaded angularcontact bearings throughout, with the two forward bearings separated by a large spacer to enhance radial stability enabling heavy cuts in steel. To ensure long life, the spindle is pressurized with air to prevent coolant contamination, and an air/oil mixture is injected automatically to ensure precise lubrication and long bearing life. HighCapacity Cartridge Spindle The Haasdesigned vector spindle drive uses closedloop, digital servo technology to provide precise speed control and peak performance under heavy cutting loads. The system optimizes the slip angle between the rotor and stator of the spindle motor to greatly increase lowspeed torque and accelerations, resulting in the fastest, most powerful spindle ever. These drives allow you to push the spindle to 150 percent of the motor's continuous power rating for 15 minutes, and to 200 percent for 5 minutes. That's more performance headroom than other spindle drives on the market. Powerful Vector Spindle Drives OnTheFly WyeDelta Switching Many Haas VMCs feature a dualwinding motor wye and delta with an electronic switch to change between the two windings. Selecting the best winding for lowrpm cutting and the best winding for highrpm cutting yields higher torque over a wider rpm range. Onthefly switching maximizes acceleration/deceleration rates for more chip making and less waiting. PEAK POWER RPM Typical power curve Enhanced power range with onthefly wyedelta Haas Automation, Inc. 8003316746 www.HaasCNC.com | 19 MAIN SPINDLE FEATURES 3 SPINDLE TYPES The standard configuration for many 40taper VMCs is a Haasbuilt cartridge spindle that is driven by the motor via belt. This provides a good combination of torque and rpm for a wide selection of machining operations. It is a great overall value. Belt Drive The most advanced Haas spindle design is an innovative 12,000rpm, inline directdrive spindle that is coupled directly to the motor. This provides smooth operation for excellent surface finishes, and reduces operating heat for greater thermal stability. (Available only on VM & SS models.) Inline Drive Gear Drive The Haas gearedhead spindle provides increased lowend torque for heavy cutting, while retaining the ability to run up to 10,000 rpm for highspeed machining. It is standard on 50taper machines, providing 450 ftlb of torque, and optional on 40taper machines, providing 250 ftlb of torque. Synchronized Tapping Haas has invested more than $4 million in the finest gearmaking and inspection equipment in the world. Haas gears are CNC machined and hobbed out of alloy steel, heattreated to 60 Rc, and then precision CNC ground to AGMA Class 13 quality. A drysump oiling system circulates oil to all vital areas of the gearbox, and polyurethane mounts eliminate vibrations that could show up on finishing passes. VibrationIsolated Gearbox An encoder attached to the Haas highperformance spindle synchronizes Zaxis motion with the spindle's rotation. Synchronized tapping eliminates the need for expensive floating tap holders, and prevents leadthread distortion and startthread pullout. The tap can also reverse out of a rigidtapped hole faster than it went in, which can reduce cycle times. (Standard on all machines except GR, Mini Mill and Toolroom Mill.) 20 | America's Leading Machine Tool Builder More Spindle Torque Cutting performance and material removal rates are a product of torque, speed, and power. These charts show two of the enhancedperformance options available for your Haas VMC. The top shows a geardriven, 7500rpm spindle, and the bottom chart shows a geardriven, hightorque, 10,000rpm spindle. Spindle Head Thermal Stability Enhancements An independent jacket in our head casting surrounds the spindle. Coolant circulates through this jacket to remove heat generated by the spindle, which minimizes thermal distortion of the head, eliminating Y and Zaxis changes. Because the coolant touches all parts of the machining area, it accurately reflects the overall temperature of the machine. To improve thermal stability further, we've insulated the head and increased the air flow through the spindlehead assembly. Cool air enters from the rear of the machine, flows around the spindle and exits at the top, away from the spindle head. A chillerready provision is also available for VF1 through VF12 40taper models for customers wanting to add an aftermarket spindle chiller. Specifications subject to change without notice. Not responsible for typographical errors. Haas Automation, Inc. 8003316746 www.HaasCNC.com | 21 TOOL MANAGEMENT Economical Electronic Tool Changer The standard Haas 40taper tool changer is an economical choice for costconscious shops. A sinusoidal motion arm accelerates and decelerates the shuttle for smooth operation, and each pocket has a retractable cover that prevents chips from entering the changer and sticking on the tool tapers. Simple design and minimal moving parts guarantee long life and reliable service. (Standard on Mini Mill and VF1 through VF5 40taper models. VF6 through VF12 and all 50taper models come standard with a sidemount tool changer.) Tool Changer Specifications Tool Changer Type # Tools Machine Models TooltoTool ChiptoChip Max Diameter full (adj empty) Standard configuration 40taper umbrellastyle 40taper sidemount 40taper sidemount 50taper sidemount Optional configuration 40taper sidemount 40taper sidemount 24+1 40+1 VF1 thru VF5 VF2YT thru VF12 2.8 sec 2.8 sec 3.6 sec 3.6 sec 3" (5"2) 3" (5"3, 6"4) 20 24+1 24+1 30+1 VF1 thru VF5 VF2SS thru VF6SS VF6 thru VF12 VF5/50 thru VF12/50 4.2 sec 1.6 sec 2.8 sec 4.2 sec 4.5 sec 2.2 sec 3.6 sec 6.3 sec 3.5" 3" (5") 3" (6") 4" (10"1) 1) VF5/50 max diameter 4" ( 7 ") 2) VF5/40 max diameter 3" ( 6 ") 3) VF2YT to VF4 4) VF5 to VF12 22 | America's Leading Machine Tool Builder From concept to reality The Haasdesigned and built sidemount tool changer symbolizes our focus on inhouse design, development, and manufacturing. It's the best way to ensure total control. We use this approach to refine our processes, control costs, and ensure a consistent high level of quality in everything we build. Inside The Haas SideMount Tool Changer The synchronized cycloidal motion of our sidemount tool changers is controlled by precision cams that are manufactured inhouse on standard Haas 5axis machines. This rugged, dependable design uses a special Haas wormgear drive and an electronically controlled start/stop system for long life and maintenancefree operation. Every Haas SMTC is manufactured completely inhouse to guarantee fast, smooth, reliable operation. 50 Taper Offers More Gage diameter (A) Taper length (B) Tool clamp force* Max tool weight Max tool diameter *Nominal 40 Taper 1.750" 44.45 mm 2.687" 68.25 mm 1,800 lb 8 007 N 12 lb 5.4 kg 6" 152.4 mm 50 Taper 2.750" 69.85 mm 4.000" 101.60 mm 4,000 lb 17 793 N 30 lb 13.6 kg 10" 254 mm A B Haas Automation, Inc. 8003316746 www.HaasCNC.com | 23 CHIP AND COOLANT MANAGEMENT Chip Removal Systems People buy CNC machines to make parts faster. The last thing they want is to waste time removing chips. Haas VMCs are available with an optional single or multiauger system that automatically removes chips from the enclosure and conveniently discharges them at the side of the machine. 24 | America's Leading Machine Tool Builder Single Auger All Haas VMCs are available with a single, augerstyle chip conveyor that automatically removes chips from the machine, while compressing them and wringing out the coolant at the same time. For added reliability, the system reverses automatically if a jam occurs. VF1 and VF2 machines (all models) are available with a highvolume chipremoval system comprising dual side augers to transport chips to the front of the pan, and a primary chip auger to discharge the chips from the machine. Triple Auger VF3 through VF6 machines (all models) are available with a highvolume chipremoval system comprising four side augers to transport chips to the front of the pan, and a belttype chip conveyor to discharge chips from the machine at barrel height. The belt conveyor may be installed on either side of the machine. Quad Auger Haas Automation, Inc. 8003316746 www.HaasCNC.com | 25 CHIP AND COOLANT MANAGEMENT Programmable Coolant Nozzle We spent time watching operators machining parts and noticed they were constantly opening the doors of the machine to readjust coolant lines. Our programmable coolant nozzle is controlled automatically by the part program to direct coolant precisely at the cutting area, eliminating constant adjustments by the operator. The nozzle can also be adjusted from the keypad while a program is running. Rear Coolant Discharge Haas VMCs now discharge coolant at the rear of the machine, directly into a chip tray spanning the highvolume, rollout coolant tank. The largecapacity chip tray prevents chips from entering the coolant tank, and is easily cleaned without removing the tank. All electrical and hose connections at the tank can be removed easily, and the lid and pump can be lifted up and out without removing any fasteners. · Largecapacity chip tray · Keeps chips out of the coolant tank · Reliable and troublefree · Convenient and easy to maintain · Accessible from the back of the machine · In plain view 26 | America's Leading Machine Tool Builder 300 psi or 1000 psi ThroughSpindle Coolant Throughspindle coolant uses an auxiliary pump to supply coolant through the tool, directly to the cutting edge. This increases tool life, allows higher cutting speeds, and clears chips during deephole drilling and blindpocket milling. Two systems are available. One provides up to 300 psi to the cutting edge, and the other provides up to 1000 psi. The 1000 psi system includes the auxiliary coolant filter (described below). The actual pressure of both systems will vary with the size of the coolant passages in the tool. Flow Rate Dynamics For both the 300 psi and 1000 psi throughspindle coolant options, the highest pressure occurs at the lowest flow rate. The actual pressure delivered to the cutting edge depends on the size of the coolant passages in the tool. Smaller coolant passages restrict the flow, causing the pressure to increase (up to the maximum provided by the system). Conversely, larger coolant passages in the tool allow more fluid to pass through, resulting in lower pressure at the cutting edge. 8.0 Volume (GPM) 7.0 6.0 5.0 4.0 3.0 2.0 1.0 0 300 1,000 300 psi TSC output 1,000 psi TSC output This 25micron, #2 bagtype filter system removes contamination and minute particles from the coolant before they can be recirculated through the coolant pump. Auxiliary Coolant Filter Coolant Level Sensor A sensor in the coolant tank allows you to monitor coolant level directly on the control screen, preventing damaged tools and saving time. During normal operation, tramp oil and coolant can collect inside a machine's base casting. This unit removes the oil before it can enter the machine's coolant system, significantly increasing coolant life and reducing costs. Waste Oil/Coolant Separator Haas Automation, Inc. 8003316746 www.HaasCNC.com | 27 OPERATOR CONVENIENCE This versatile work station offers a convenient place to keep toolholders, change cutting tools, store accessories, and much more right at the machine. The heavyduty stainlesssteel work table offers a stable surface for inspecting parts or changing inserts, and a builtin worklight provides plenty of light for checking prints or viewing surface finish. The large storage shelf has plenty of room for larger tools, and features a turnedup lip to keep small items from rolling out. An additional rack on the side holds smaller hand tools, such as wrenches and screwdrivers. Operator Work Station Automatic Air Gun Provides a constant blast of air to the cutting tool to clear chips · Builtin work light during dry machining. Activated by Mcode, the air gun can be programmed to turn on while the · Large storage shelf spindle is turning, or at the end of a cycle. Air consumption for the auto air gun is 6 scfm. · Toolholder tray holds more tools bright, even illumination of the work area for part inspection, job set up, and changeovers. Lights turn · Side rack for wrenches and screwdrivers on and off automatically when doors open and close, or can be activated manually via a switch. · Builtin toolholder vise (40taper machines) DoorActivated HighIntensity Lighting Halogen lights provide · Heavyduty stainless steel work table Servo Auto Door This option opens and closes the machine doors automatically via the part program. This reduces operator fatigue during repetitive machining operations, or allows for unattended operation when used with a robotic loader. (Available on VF1 through VF5.) Pendant Storage Cabinet Our new thin control pendant is lighter, but more stable and easier to maneuver. A large cabinet behind the pendant houses the operator's manual, and provides plenty of storage for tools, gauges, spare inserts, and much more. A convenient "glove box" below the pendant provides additional storage, and the hinged door folds down to form a convenient shelf. 28 | America's Leading Machine Tool Builder Work and Tool Probe Features · Excellent repeatability · Cycletime reduction · High protection against coolant · High reliability · High performance · No wires in the work envelope · Easy and intuitive programming of measuring cycles Haas Wireless Intuitive Probing System The Haas Wireless Intuitive Probing System (WIPS), with optical transmission for part setting, tool setting, and inspection, consists of the following elements: · Spindle Probe Module (work probe) · Tool Setter Module (tool probe) · Intuitive Probing System Software The Haas Wireless Intuitive Probing System makes probing easy to understand and use through simple language, a graphical interface, and clear instructions. Stepbystep graphical instructions show machine operators how to set up the probing cycles. The Haas Intuitive Probing System software guides the operator through the probing setup process, prompting them to enter each necessary dimension. Once all dimensions are entered, the operator executes the probing cycle by pushing the Cycle Start button. The probing cycle can then be saved in memory, and recalled when needed. With the Haas Intuitive Probing System, no knowledge of Gcode or macro programming is needed to use the probing system. WIPS is available as a factoryinstalled option on most new Haas VMCs. Haas Automation, Inc. 8003316746 www.HaasCNC.com | 29 2010 VMC PRODUCT LINE Office Mills OM1A OM2A 8"x8"x12" (xyz) 203x203x305 mm 12"x10"x12" (xyz) 305x254x305 mm 40Taper Standard VMCs VF1 VF1YT VF2 20"x16"x20" (xyz) 508x406x508 mm 20"x20"x20" (xyz) 508x508x508 mm 30"x16"x20" (xyz) 762x406x508 mm 30"x20"x20" (xyz) 762x508x508 mm 40"x20"x25" (xyz) 1 016x508x635 mm 40"x26"x25" (xyz) 1 016x660x635 mm 50"x20"x25" (xyz) 1 270x508x635 mm 50"x26"x25" (xyz) 1 270x660x635 mm 60"x26"x25" (xyz) 1 524x660x635 mm 64"x32"x30" (xyz) 1 626x813x762 mm 84"x32"x30" (xyz) 2 134x813x762 mm 64"x40"x30" (xyz) 1 626x1 016x762 mm 84"x40"x30" (xyz) 2 134x1 016x762 mm 120"x32"x30" (xyz) 3 048x813x762 mm 120"x40"x30" (xyz) 3 048x1 016x762 mm 150"x32"x30" (xyz) 3 810x813x762 mm 50Taper Standard VMCs 40"x26"x25" (xyz) 1 016x660x635 mm VF5/50 50"x26"x25" (xyz) 1 270x660x635 mm VF5/50XT 60"x26"x25" (xyz) 1 524x660x635 mm VF6/50 64"x32"x30" (xyz) 1 626x813x762 mm VF7/50 84"x32"x30" (xyz) 2 134x813x762 mm VF8/50 64"x40"x30" (xyz) 1 626x1 016x762 mm VF9/50 84"x40"x30" (xyz) 2 134x1 016x762 mm VF10/50 120"x32"x30" (xyz) 3 048x813x762 mm VF11/50 120"x40"x30" (xyz) 3 048x1 016x762 mm VF12/50 150"x32"x30" (xyz) 3 810x813x762 mm VF3YT/50 VF6TR Toolroom Mills TM1 TM1P TM2 TM3 TM3P 30"x12"x16" (xyz) 762x305x406 mm 30"x12"x16" (xyz) 762x305x406 mm 40"x16"x16" (xyz) 1 016x406x406 mm 40"x20"x16" (xyz) 1 016x508x406 mm 40"x20"x16" (xyz) 1 016x508x406 mm VF2YT VF3 VF3YT VF4 VF5 VF5XT 64"x32"x30" (xyz) 1 626x813x762 mm VF6/50TR 64"x32"x30" (xyz) 1 626x813x762 mm VR8 64"x40"x30" (xyz) 1 626x1 016x762 mm VR11 120"x40"x30" (xyz) 3 048x1 016x762 mm Gantry SR100 GR510 GR712 100"x52"x8" (xyz) 2 540x1 321x203 mm 121"x61"x11" (xyz) 3 073x1 549x279 mm 145"x85"x11" (xyz) 3 683x2 159x279 mm Mold Machines VMCs with APC (Automatic Pallet Changer) VM2 VM3 VM6 VF3APC VF3SSAPC VF4APC VF4SSAPC Mini VMCs Mini Mill Mini Mill 2 Super Mini Mill Super MM 2 16"x12"x10" (xyz) 406x305x254 mm 20"x16"x14" (xyz) 508x406x356 mm 16"x12"x10" (xyz) 406x305x254 mm 20"x16"x14" (xyz) 508x406x356 mm VF6 VF7 VF8 VF9 VF10 VF11 VF12 40"x20"x25" (xyz) 1 016x508x635 mm 40"x20"x25" (xyz) 1 016x508x635 mm 50"x20"x25" (xyz) 1 270x508x635 mm 50"x20"x25" (xyz) 1 270x508x635 mm 30"x20"x20" (xyz) 762x508x508 mm 40"x26"x25" (xyz) 1 016x660x635 mm 64"x32"x30" (xyz) 1 626x813x762 mm Mill Drill Center MDC500 20"x14"x20" (xyz) 508x356x508 mm SuperSpeed VMCs VF2SS 30"x16"x20" (xyz) 762x406x508 mm 30"x20"x20" (xyz) 762x508x508 mm 40"x20"x25" (xyz) 1 016x508x635 mm 40"x26"x25" (xyz) 1 016x660x635 mm 50"x20"x25" (xyz) 1 270x508x635 mm 50"x26"x25" (xyz) 1 270x660x635 mm 64"x32"x30" (xyz) 1 626x813x762 mm Drill/Tap Center DT1 20"x16"x15.5" (xyz) 508x406x394 mm LargeCapacity VMCs VS1 VS3 84"x50"x50" (xyz) 2 134x1 270x1 270 mm 150"x50"x50" (xyz) 3 810x1 270x1 270 mm VF2SSYT VF3SS VF3SSYT 5Axis VMCs VF2TR VF5TR VF5/50TR 30"x16"x20" (xyz) 762x406x508 mm 38"x26"x25" (xyz) 965x660x635 mm 38"x26"x25" (xyz) 965x660x635 mm VF4SS VF5SS VF6SS 30 | America's Leading Machine Tool Builder Machine Configurations & Options = Available configuration = Standard on 40taper machines = Optional on 40taper machines = Standard on 50taper machines = Optional on 50taper machines SPINDLE CONFIGURATIONS 40TAPER SPINDLE 50TAPER SPINDLE 2SPEED GEARBOX CT SPINDLE BT SPINDLE 4,000 RPM 5,000 RPM 6,000 RPM 10,000 RPM HIGHTORQUE 10,000 RPM 12,000 RPM 15,000 RPM 30,000 RPM TOOL CHANGERS 24POCKET SMTC 30POCKET SMTC 40POCKET SMTC SPECIAL MACHINES SUPERSPEED MODEL 5AXIS TRUNNION MODEL SPECIAL OPTIONS AUTO AIR GUN AUX. COOLANT FILTER AUTO PALLET CHANGER AUTOMATIC CHIP AUGER EXTENDED ZAXIS CLEARANCE EXTENDED Y AXIS EXTENDED X AXIS 95GALLON COOLANT TANK LINEAR SCALES PROGRAMMABLE COOLANT THROUGHSPINDLE COOLANT EXTRA RAPID TRAVERSE HIGHINTENSITY LIGHTING AUTOMATIC DOOR CONTROL OPTIONS EXPANDED MEMORY 4THAXIS DRIVE 5THAXIS DRIVE 8 ADDITIONAL M FUNCTIONS COORD. ROTATION/SCALING ETHERNET INTERFACE RIGID TAPPING HIGHSPEED MACHINING USERDEFINABLE MACROS REMOTE JOG HANDLE SPINDLE ORIENTATION INTUITIVE PROGRAMMING TOOL & PART PROBING TM MM VF1 VF2 VF3 VF4 TM MM VF1 TM MM VF1 VF2 VF2 VF3 VF5 VF6 VF7 VF8 VF9 VF10 VF11 VM VR VS GR MDC * VF4 VF3 VF4 TM MM VF1 VF2 VF3 VF4 VF5 VF5 VF5 VF6 VF6 VF6 VF7 VF8 VF9 VF10 VF11 VF12 VM VR VS GR MDC VF7 VF7 VF8 VF8 VF9 VF9 VF10 VF10 VF11 VF11 VF12 VF12 VM VR VS GR MDC VM VR VS GR MDC TM MM VF1 VF2 VF3 VF4 VF5 VF6 VF7 VF8 VF9 VF10 VF11 VF12 VM VR VS GR MDC Important: The above chart represents the standard configurations of machines distributed in North America. Machine configurations and availability may differ for other countries and regions. This chart is for reference only. Check with your local Haas distributor for exact pricing, configuration, and availability of machines and options. *Xaxis scale only. HIGHPERFORMANCE VMCs 5Axis Trunnion Machines The Haas Trunnion Series machines are versatile 5axis machining centers that provide full, simultaneous 5axis motion for machining complex parts, or can position a workpiece to almost any angle for multiside machining. The VF5TR and VF6TR have a dualaxis trunnion table mounted directly to the bearing trucks in place of the standard Tslot table. Both machines are available in 40 or 50taper configurations. The VF2TR has a removable dualaxis trunnion mounted to the standard Tslot table, which provides the flexibility to run the machine with or without the trunnion table installed. · DualAxis Table · ±120° Tilt, 360° Rotation · SideMount Tool Changer · Automatic Chip Auger · Programmable Coolant Nozzle · 250 MB Program Memory · USB Port · Remote Jog Handle · HighSpeed Machining w/LookAhead · UserDefinable Macros Available Models VF2TR VF5TR 40 or 50 taper VF6TR 40 or 50 taper 32 | America's Leading Machine Tool Builder HIGH PERFORMANCE The VM Series Speed and Accuracy for the Mold Making Industry Designed specifically for mold makers, the VM Series machines feature the Haas 12,000rpm, inline directdrive spindle, a unique 40taper design that provides superior surface finishes, excellent thermal stability, and quiet operation. VM machines come standard with an automatic chip auger, remote jog handle, automatic air gun, highspeed machining, Ethernet interface, 250 MB program memory, USB port, userdefinable macros, programmable coolant nozzle, and more. A unique, multifixture table provides Tslots in both X and Y directions, as well as drilled and tapped holes and precision dowelpin bores. Available Models VM2 VM3 VM6 Haas Automation, Inc. 8003316746 www.HaasCNC.com | 33 HIGHPERFORMANCE DRILL/TAP The DT1 is a compact, highspeed drill and tap machine with full milling capabilities. The machine has a 20" x 16" x 15.5" (xyz) work cube and a 26" x 15" Tslot table. A powerful BT30 taper inline directdrive spindle provides 15,000 rpm, and allows rigid tapping at speeds to 5000 rpm. A highspeed sidemount tool changer swaps tools quickly, while 2400 ipm rapids on all axes and 1G acceleration/deceleration rates combine to shorten cycle times and reduce noncutting time. Steeply sloped internal sheet metal and available dual chip augers efficiently move chips to the rear of the DT1 for discharge. The DT1's highspeed 20+1 tool sidemount tool changer swaps tools in 0.8 seconds. The 15,000rpm inline directdrive spindle allows rigid tapping to 5000 rpm, with up to 4times retract speed. The userfriendly Haas control and available Intuitive Programming System make the DT1 easy to program and operate. 34 | America's Leading Machine Tool Builder HIGH PERFORMANCE VFSS SuperSpeed VMCs Affordable HighSpeed Performance The Haas SS Series highperformance vertical machining centers come standard with an innovative 12,000rpm, inline directdrive spindle, a highspeed sidemount tool changer and highspeed rapids for reduced cycle times. The allaround enhanced performance of the SuperSpeed machines yields shorter cycle times and more parts per shift, making them some of the more popular innovations offered by Haas Automation. Available Models VF2SS VF2SSYT VF3SS VF3SSYT VF4SS VF5SS VF6SS Haas Automation, Inc. 8003316746 www.HaasCNC.com | 35 MACHINING WITH HAAS VMCs What's new The latest Haas vertical machining centers feature refinements focused both on the machine owner and on the operator. The latest version of the Haas control features a simplified user interface and powerful operator features. The newgeneration Haas VMCs are easier than ever to operate, and they perform with more speed, better chip evacuation, better coolant containment, smoother surface finishes, and more operatorfriendly features than ever. Whether you focus on highproduction output or specialized shortrun work, there's a Haas machining center with the features and price tag to help you succeed. 36 | America's Leading Machine Tool Builder Here are some examples of what's new: Chip evacuation We redesigned the chip pans and reviewed coolant flow of the new VMCs to reduce chip buildup and efficiently flush chips into the auger trough for removal. For highvolume production applications, the VF1 through VF6 VMCs are available with optional chip removal systems that combine multiple side augers with either a front discharge auger or belttype conveyor to move chips out of the machines faster and easier than ever. Coolant containment To prevent chip and coolant egress during machining, we optimized the enclosures on the new VMCs, paying close attention to panel fit, service access, and internal routing of plumbing and cables. The result is a far better enclosure and a much simpler overall design that thoroughly contains chips and coolant, while increasing reliability and simplifying service. Ergonomics Our engineers worked hard to make everything the operator touches work better. For example, the machines' windows and doors are now stiffer, move more smoothly, and close tightly. And our new thindesign control pendant is mounted directly to the enclosure, providing a lighter but more stable operator interface than the previous version, with a convenient storage compartment behind the pendant. Enhanced motion control To ensure smooth, precise motion control, the new Haas VMCs use nextgeneration digital servomotors and highresolution encoders on all axes. Combined with significant software and motorcontrol advancements on the new machines, these yield better surfacefinish performance and higher accelerations. These latest versions of the wildly popular Haas VMCs are the best machines we've ever made providing more performance and value than ever before. Haas Automation, Inc. 8003316746 www.HaasCNC.com | 37 WORK SMART 4TH AND 5THAXIS OPTIONS Adding a fully integrated 4th or 5thaxis Haas brushless rotary table to your Haas VMC creates a supercharged machining center package that boosts your productivity and reduces setups. Fully synchronized 4th and 5thaxis configurations are available on most Haas VMC models. NEW, FASTER ROTARY SPEEDS Rotary Models HA5C (5C collet rotary) HRT160, HRT160SP, HRTA5 160 mm platter table HRT210, HRT210SP, HRTA6 210 mm platter table HRT310, HRT310SP 310 mm platter table 4thAxis Speed 25% Increase (now 410°/sec) 30% Increase (now 130°/sec) Acceleration 45% Increase 33% Increase Brake Dwell Time 89% Reduction 34% Increase (now 100°/sec) 125% Increase 89% Reduction 26% Increase (now 75°/sec) 33% Increase 95% Reduction 38 | America's Leading Machine Tool Builder Some items shown in this brochure are optional. Please contact your local distributor for assistance. ROTARY TABLES & INDEXERS SCOLCR SC02ACR HA5CSB HA5C HA5C 2 HA5C 3 HA5C 4 T5C T5C 2 T5C 3 T5C 4 HRT110 HRT160 HRT210 HRT310 HRT320/FB HRT450 HRT600 HRT160SP HRT210SP HRT310SP HRTA5 HRTA6 HRT1602 HRT2102 HRT210SHSHD TRT160 TRT210 TR110 TR160Y TR160 TR1602 TR210 TR310 Haas Automation, Inc. 8003316746 www.HaasCNC.com | 39 GOING GREEN Long before "Green" meant lessening one's carbon footprint, Haas machines had the ability to save you money by reducing electricity usage while the machine was in idle mode. While Haas engineers continue to improve the electrical efficiency of Haas machines, below are several things you can do today to further lower electricity usage in your Haas machining center. SAVING ENERGY MEANS SAVING MONEY · Auto PowerOff setting turns the machine off after a specified number of minutes idle · PowerOff at M30 sets the control to start a 30second timer that will turn off all power unless interrupted · Sleep Mode puts the machine into a lowpower mode for a programmed length of time · Screen Saver setting · LCD Backlight Off setting blanks the LCD after a specified number of minutes idle · Conveyor Off setting automatically turns off the chip conveyor after a specified number of minutes idle · Servos and Hydraulics Off setting automatically turns off the servos and hydraulic pump after a specified number of minutes idle Refer to your operator's manual for detailed information on these settings and more. 40 | America's Leading Machine Tool Builder Machine Dimensions D A Y B Z W C E X L2 L1 0.640" 16.3 mm 0.630" 16 mm F M K J H G 1.06" 26.9 mm I 0.42" 10.7 mm Side View A B (40 Taper) B (50 Taper) C D Front View E F G H I (Door Opening) J K L1 L2 M VF1 92.80" 2357 mm 104.50" 2654 mm 58.00" 1473 mm 36.00" 914 mm VF1 94.00" 2388 mm 64.00" 1626 mm 42.95" 1091 mm 32.00" 813 mm 35.50" 902 mm 30.00" 762 mm 27.54" 700 mm 21.81" 554 mm VF2 92.80" 2357 mm 104.50" 2654 mm 58.00" 1473 mm 36.00" 914 mm VF2 94.00" 2388 mm 64.00" 1626 mm 42.95" 1091 mm 32.00" 813 mm 35.50" 902 mm 30.00" 762 mm 27.54" 700 mm 21.81" 554 mm 33.00" 838 mm VF2 2.08" 52.8 mm 36.00" 914 mm 14.00" 356 mm 4.92" 125.0 mm VF2 3 VF3 110.00" 2794 mm 117.50" 2985 mm 74.40" 1890 mm 36.00" 914 mm VF3 122.00" 3099 mm 67.20" 1707 mm 46.15" 1172 mm 30.30" 770 mm 48.50" 1232 mm 42.50" 1080 mm 27.31"1 694 mm 20.86" 530 mm 38.81" 986 mm 36.50"3 927 mm VF3 2.70" 68.6 mm 48.00" 1219 mm 18.00" 457 mm 3.15" 80.0 mm VF3 5 VF4 110.00" 2794 mm 117.50" 2985 mm 74.40" 1890 mm 36.00" 914 mm VF4 122.00" 3099 mm 67.20" 1707 mm 46.15" 1172 mm 30.30" 770 mm 48.50" 1232 mm 42.50" 1080 mm 27.31"1 694 mm 20.86" 530 mm 38.81" 986 mm 36.50"3 927 mm VF4 2.70" 68.6 mm 52.00" 1321 mm 18.00" 457 mm 3.15" 80.0 mm VF4 5 33.00" 838 mm Table VF1 W 2.08" 52.8 mm X 26.00" 660 mm Y 14.00" 356 mm Z 4.92" 125.0 mm TSlots VF1 Number on Table 3 VF5 114.00" 2895 mm 118.20" 3002 mm 126.50" 3213 mm 82.88" 2105 mm 36.00" 914 mm VF5 137.00" 3480 mm 70.50" 1791 mm 49.15" 1248 mm 33.20" 843 mm 54.00" 1372 mm 42.50" 1080 mm 27.31"1 694 mm 11.18" 284 mm 38.81" 986 mm 36.50"3 927 mm VF5 2.05" 52.1 mm 52.00" 1321 mm 23.00" 584 mm 3.15" 80.0 mm VF5 7 VF6 111.00" 2819 mm 124.00" 3150 mm 138.00" 3505 mm 94.00" 2388 mm 30.00" 762 mm VF6 156.00" 3962 mm 70.00" 1778 mm 55.15" 1401 mm 34.00" 864 mm 69.00" 1753 mm 60.00" 1524 mm 23.20"2 589 mm 21.72" 552 mm 47.45" 1205 mm 43.00"4 1092 mm VF6 4.16" 105.7 mm 64.00" 1626 mm 28.00" 711 mm 4.92" 125.0 mm VF6 5 VF7 111.00" 2819 mm 124.00" 3150 mm 138.00" 3505 mm 94.00" 2388 mm 30.00" 762 mm VF7 183.00" 4648 mm 70.00" 1778 mm 55.15" 1401 mm 34.00" 864 mm 95.20" 2418 mm 60.00" 1524 mm 23.20" 589 mm 8.00" 203 mm 43.00" 1092 mm VF7 4.16" 105.7 mm 84.00" 2134 mm 28.00" 711 mm 4.92" 125.0 mm VF7 5 VF8 139.00" 3531 mm 124.00" 3150 mm 138.00" 3505 mm 110.00" 2794 mm 30.00" 762 mm VF8 156.00" 3962 mm 70.00" 1778 mm 55.15" 1401 mm 34.00" 864 mm 69.00" 1753 mm 60.00" 1524 mm 23.20" 589 mm 21.72" 552 mm 43.00" 1092 mm VF8 3.24" 82.3 mm 64.00" 1626 mm 36.00" 914 mm 4.92" 125.0 mm VF8 7 VF9 139.00" 3531 mm 124.00" 3150 mm 138.00" 3505 mm 110.00" 2794 mm 30.00" 762 mm VF9 183.00" 4648 mm 70.00" 1778 mm 55.15" 1401 mm 34.00" 864 mm 95.20" 2418 mm 60.00" 1524 mm 23.20" 589 mm 8.00" 203 mm 43.00" 1092 mm VF9 3.24" 82.3 mm 84.00" 2134 mm 36.00" 914 mm 4.92" 125.0 mm VF9 7 VF10 111.00" 2819 mm 124.00" 3150 mm 138.00" 3505 mm 98.00" 2489 mm 30.00" 762 mm VF10 257.00" 6528 mm 70.00" 1778 mm 55.15" 1401 mm 34.00" 864 mm 125.00" 3175 mm 60.00" 1524 mm 23.20" 589 mm 8.00" 203 mm 43.00" 1092 mm VF10 4.16" 105.7 mm 120.00" 3048 mm 28.00" 711 mm 4.92" 125.0 mm VF10 5 VF11 139.00" 3531 mm 124.00" 3150 mm 138.00" 3505 mm 110.00" 2794 mm 30.00" 762 mm VF11 257.00" 6528 mm 70.00" 1778 mm 55.15" 1401 mm 34.00" 864 mm 125.00" 3175 mm 60.00" 1524 mm 23.20" 589 mm 8.00" 203 mm 43.00" 1092 mm VF11 4.16" 105.7 mm 120.00" 3048 mm 28.00" 711 mm 4.92" 125.0 mm VF11 5 VF12 111.00" 2819 mm 124.00" 3150 mm 138.00" 3505 mm 94.00" 2388 mm 30.00" 762 mm VF12 330.00" 8382 mm 70.00" 1778 mm 55.15" 1401 mm 34.00" 864 mm 125.50" 3188 mm 60.00" 1524 mm 23.20" 589 mm 8.00" 203 mm 43.00" 1092 mm VF12 4.16" 105.7 mm 150" 3810 mm 28.00" 711 mm 4.92" 125.0 mm VF12 5 1) Add 23.06" (586 mm) for conveyor. 2) Add 27.18" (690 mm) for conveyor. 3) Add 31.18" (792 mm) for conveyor. 4) Add 24.68" (627 mm) for conveyor. MACHINE SPECIFICATIONS (Standard 40Taper Machines) VF1 | VF1YT X Y 20" 508 mm 16" | 20" 406 mm | 508 mm 20" 508 mm 4 24" 102 610 mm 26" 660 mm 14" | 18" 356 mm | 457 mm 3,000 lb 1 361 kg 5/8" 16 mm 4.92" 125 mm #40 Taper 7,500 max rpm Direct Speed Belt Drive 75 ftlb @ 1,400 102 Nm @ 1400 250 ftlb @ 450 339 Nm @ 450 Air/Oil Injection Liquid Cooled 1 VF2 | VF2YT 30" 762 mm 16" | 20" 406 mm | 508 mm 20" 508 mm 4 24" 102 610 mm 36" 914 mm 14" | 18" 356 mm | 457 mm 3,000 lb 1 361 kg 5/8" 16 mm 4.92" 125 mm #40 Taper 7,500 max rpm Direct Speed Belt Drive 75 ftlb @ 1,400 102 Nm @ 1 400 250 ftlb @ 450 339 Nm @ 450 Air/Oil Injection Liquid Cooled 20 hp 14.9 kW 2,550 lb 1 343 N 2,550 lb 1 343 N 4,200 lb 18 683 N 1,000 ipm 25.4 m/min 1,000 ipm 25.4 m/min 1,000 ipm 25.4 m/min 650 ipm 16.5 m/min 20 (24+1) CT or BT / 40 3.5" (full) 89 mm 12 lb 5.4 kg Carousel (SMTC) 4.2 sec (2.8) 4.5 sec (3.6) ±0.0002" ±0.005 mm ±0.0001" ±0.003 mm 7,300 lb | 7,500 lb 3 311 kg | 3 402 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC VF3 | VF3YT 40" 1 016 mm 20" | 26" 508 mm | 660 mm 25" 635 mm 4 29" 102 737 mm 48" | 54" 1 219 mm | 1372 mm 18" | 25" 457 mm | 635 mm 3,500 lb 1 588 kg 5/8" 16 mm 3.15" 80 mm #40 Taper 7,500 max rpm Direct Speed Belt Drive 75 ftlb @ 1,400 102 Nm @ 1 400 250 ftlb @ 450 339 Nm @ 450 Air/Oil Injection Liquid Cooled 20 hp 14.9 kW 2,550 lb 11 343 N 2,550 lb 11 343 N 4,200 lb 18 683 N 1,000 ipm 25.4 m/min 1,000 ipm | 710 ipm 25.4 m/min | 18.0 m/min 1,000 ipm | 710 ipm 25.4 m/min | 18.0 m/min 650 ipm 16.5 m/min 20 (24+1, 40+1) CT or BT / 40 3.5" (full) 89 mm 12 lb 5.4 kg Carousel (SMTC) 4.2 sec (2.8) 4.5 sec (3.6) ±0.0002" ±0.005 mm ±0.0001" ±0.003 mm 12,500 lb | 14,000 lb 5 670 kg | 6 350 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC VF4 50" 1 270 mm 20" 508 mm 25" 635 mm 4 29" 102 737 mm 52" 1 321 mm 18" 457 mm 3,500 lb 1 588 kg 5/8" 16 mm 3.15" 80 mm #40 Taper 7,500 max rpm Direct Speed Belt Drive 75 ftlb @ 1,400 102 Nm @ 1 400 250 ftlb @ 450 339 Nm @ 450 Air/Oil Injection Liquid Cooled 20 hp 14.9 kW 2,550 lb 11 343 N 2,550 lb 11 343 N 4,200 lb 18 683 N 1,000 ipm 25.4 m/min 1,000 ipm 25.4 m/min 1,000 ipm 25.4 m/min 650 ipm 16.5 m/min 20 (24+1, 40+1) CT or BT / 40 3.5" (full) 89 mm 12 lb 5.4 kg Carousel (SMTC) 4.2 sec (2.8) 4.5 sec (3.6) ±0.0002" ±0.005 mm ±0.0001" ±0.003 mm 13,300 lb 6 033 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC VF5 | VF5XT 50" | 60" 1 270 mm | 1 524 mm 26" 660 mm 25" 635 mm 7 32" 178 813 mm 52" | 62" 1321 mm | 1 575 mm 23" 584 mm 4,000 lb 1 814 kg 5/8" 16 mm 3.15" 80 mm #40 Taper 7,500 max rpm Direct Speed Belt Drive 75 ftlb @ 1,400 102 Nm @ 1 400 250 ftlb @ 450 339 Nm @ 450 Air/Oil Injection Liquid Cooled 20 hp 14.9 kW 3,400 lb 15 124 N 3,400 lb 15 124 N 5,600 lb 24 910 N 710 ipm | 540 ipm 18.0 m/min | 13.7 m/min 710 ipm 18.0 m/min 710 ipm 18.0 m/min 500 ipm 12.7 m/min 20 (24+1, 40+1) CT or BT / 40 3.5" (full) 89 mm 12 lb 5.4 kg Carousel (SMTC) 4.2 sec (2.8) 4.5 sec (3.6) ±0.0002" ±0.005 mm ±0.0001" ±0.003 mm 14,600 lb | 15,150 lb 6 623 kg | 6 872 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC VF6 64" 1 626 mm 32" 813 mm 30" 762 mm 4 34" 102 864 mm 64" 1 626 mm 28" 711 mm 4,000 lb 1 814 kg 5/8" 16 mm 4.92" 125 mm #40 Taper 7,500 max rpm Direct Speed Belt Drive 75 ftlb @ 1,400 102 Nm @ 1 400 250 ftlb @ 450 339 Nm @ 450 Air/Oil Injection Liquid Cooled 20 hp 14.9 kW 3,400 lb 15 124 N 3,400 lb 15 124 N 5,600 lb 24 910 N 540 ipm 13.7 m/min 600 ipm 15.2 m/min 600 ipm 15.2 m/min 500 ipm 12.7 m/min 24+1 (40+1) CT or BT / 40 3" / 6" 76 mm / 152 mm 12 lb 5.4 kg SMTC 2.8 sec 3.6 sec ±0.0003"3 ±0.008 mm ±0.0002"3 ±0.005 mm 21,000 lb 9 526 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC Travels Z Spindle Nose to Table Length Width Table Max Weight on Table TSlot Width TSlot Center Distance Taper Size Speed Drive System Max Torque Standard Spindle with Optional Gearbox Bearing Lubrication Cooling Spindle Motor Max Rating 20 hp 14.9 kW X 2,550 lb 11 343 N 2,550 lb 11 343 N 4,200 lb 18 683 N 1,000 ipm 25.4 m/min 1,000 ipm 25.4 m/min 1,000 ipm 25.4 m/min 650 ipm 16.5 m/min 20 (24+1) CT or BT / 40 3.5" (full) 89 mm 12 lb 5.4 kg Carousel (SMTC) 4.2 sec (2.8) 4.5 sec (3.6) ±0.0002" ±0.005 mm ±0.0001" ±0.003 mm 7,100 lb | 7,400 lb 3 220 kg | 3 357 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC Max Thrust Rating Y Z Axis Motors Rapids X Y Z Max Cutting Capacity Standard (optional)2 Tool Type / Taper Max Tool Diameter Standard (full / adjacent empty) Tool Changer Max Tool Weight Changer Type Standard (Optional) Tool to Tool (optional) Chip to Chip (optional) Positioning Accuracy Repeatability Machine Weight Miscellaneous Air Required Power Required (min) 42 | America's Leading Machine Tool Builder 1) 5minute rating. 2) See page 22 for optional tool changer specifications. 3) Linear scales required to achieve accuracy listed. VF7 84" 2 134 mm 32" 813 mm 30" 762 mm 4 34" 102 864 mm 84" 2 134 mm 28" 711 mm 4,000 lb 1 814 kg 5/8" 16 mm 4.92" 125 mm #40 Taper 7,500 max rpm Direct Speed Belt Drive 75 ftlb @ 1,400 102 Nm @ 1 400 250 ftlb @ 450 339 Nm @ 450 Air/Oil Injection Liquid Cooled 20 hp 14.9 kW 3,400 lb 15 124 N 3,400 lb 15 124 N 5,600 lb 24 910 N 600 ipm 15.2 m/min 600 ipm 15.2 m/min 600 ipm 15.2 m/min 500 ipm 12.7 m/min 24+1 (40+1) CT or BT / 40 3" / 6" 76 mm / 152 mm 12 lb 5.4 kg SMTC 2.8 sec 3.6 sec ±0.0003" ±0.008 mm ±0.0002"3 ±0.005 mm 23,000 lb 10 433 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC 3 VF8 64" 1 626 mm 40" 1 016 mm 30" 762 mm 4 34" 102 864 mm 64" 1 626 mm 36" 914 mm 4,000 lb 1 814 kg 5/8" 16 mm 4.92" 125 mm #40 Taper 7,500 max rpm Direct Speed Belt Drive 75 ftlb @ 1,400 102 Nm @ 1 400 250 ftlb @ 450 339 Nm @ 450 Air/Oil Injection Liquid Cooled 20 hp 14.9 kW 3,400 lb 15 124 N 3,400 lb 15 124 N 5,600 lb 24 910 N 540 ipm 13.7 m/min 600 ipm 15.2 m/min 600 ipm 15.2 m/min 500 ipm 12.7 m/min 24+1 (40+1) CT or BT / 40 3" / 6" 76 mm / 152 mm 12 lb 5.4 kg SMTC 2.8 sec 3.6 sec ±0.0003" ±0.008 mm ±0.0002"3 ±0.005 mm 24,000 lb 10 886 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC 3 VF9 84" 2 134 mm 40" 1 016 mm 30" 762 mm 4 34" 102 864 mm 84" 2 134 mm 36" 914 mm 4,000 lb 1 814 kg 5/8" 16 mm 4.92" 125 mm #40 Taper 7,500 max rpm Direct Speed Belt Drive 75 ftlb @ 1,400 102 Nm @ 1 400 250 ftlb @ 450 339 Nm @ 450 Air/Oil Injection Liquid Cooled 20 hp 14.9 kW 3,400 lb 15 124 N 3,400 lb 15 124 N 5,600 lb 24 910 N 600 ipm 15.2 m/min 600 ipm 15.2 m/min 600 ipm 15.2 m/min 500 ipm 12.7 m/min 24+1 (40+1) CT or BT / 40 3" / 6" 76 mm / 152 mm 12 lb 5.4 kg SMTC 2.8 sec 3.6 sec ±0.0003" ±0.008 mm ±0.0002"3 ±0.005 mm 25,000 lb 11 340 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC 3 VF10 120" 3 048 mm 32" 813 mm 30" 762 mm 4 34" 102 864 mm 120" 3 048 mm 28" 711 mm 4,000 lb 1 814 kg 5/8" 16 mm 4.92" 125 mm #40 Taper 7,500 max rpm Direct Speed Belt Drive 75 ftlb @ 1,400 102 Nm @ 1 400 250 ftlb @ 450 339 Nm @ 450 Air/Oil Injection Liquid Cooled 20 hp 14.9 kW 3,400 lb 15 124 N 3,400 lb 15 124 N 5,600 lb 24 910 N 360 ipm 9.1 m/min 600 ipm 15.2 m/min 600 ipm 15.2 m/min 360 ipm 9.1 m/min 24+1 (40+1) CT or BT / 40 3" / 6" 76 mm / 152 mm 12 lb 5.4 kg SMTC 2.8 sec 3.6 sec ±0.0003" ±0.008 mm ±0.0002"3 ±0.005 mm 28,000 lb 12 701 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC 3 VF11 120" 3 048 mm 40" 1 016 mm 30" 762 mm 4 34" 102 864 mm 120" 3 048 mm 28" 711 mm 4,000 lb 1 814 kg 5/8" 16 mm 4.92" 125 mm #40 Taper 7,500 max rpm Direct Speed Belt Drive 75 ftlb @ 1,400 102 Nm @ 1 400 250 ftlb @ 450 339 Nm @ 450 Air/Oil Injection Liquid Cooled 20 hp 14.9 kW 3,400 lb 15 124 N 3,400 lb 15 124 N 5,600 lb 24 910 N 360 ipm 9.1 m/min 600 ipm 15.2 m/min 600 ipm 15.2 m/min 360 ipm 9.1 m/min 24+1 (40+1) CT or BT / 40 3" / 6" 76 mm / 152 mm 12 lb 5.4 kg SMTC 2.8 sec 3.6 sec ±0.0003" ±0.008 mm ±0.0002"3 ±0.005 mm 29,400 lb 13 336 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC 3 VF12 150" 32" 813 mm 30" 762 mm 4 34" 102 864 mm 120" 3 048 mm 28" 711 mm 4,000 lb 1 814 kg 3/4" 22 mm 4.92" 125 mm #40 Taper 7,500 max rpm Direct Speed Belt Drive 75 ftlb @ 1,400 102 Nm @ 1 400 250 ftlb @ 450 339 Nm @ 450 Air/Oil Injection Liquid Cooled 20 hp 14.9 kW 3,400 lb 15 124 N 3,400 lb 15 124 N 5,600 lb 24 910 N 360 ipm 9.1 m/min 600 ipm 15.2 m/min 600 ipm 15.2 m/min 360 ipm 9.1 m/min 24+1 (40+1) CT or BT / 40 3" / 6" 76 mm / 152 mm 12 lb 5.4 kg SMTC 2.8 sec 3.6 sec ±0.0003" ±0.008 mm ±0.0002"3 ±0.005 mm 28,000 lb 12 701 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC 3 VM2 30" 762 mm 20" 508 mm 20" 508 mm 4 24" 102 610 mm 36" 914 mm 18" 457 mm 3,000 lb 1 361 kg 5/8" 16 mm 4.375" 111 mm #40 Taper 12,000 max rpm Inline Direct Drive 75 ftlb @ 2,100 102 Nm @ 2 100 Air/Oil Injection Liquid Cooled 30 hp 22.4 kW 3,400 lb 15 124 N 3,400 lb 15 124 N 5,600 lb 24 910 N 710 ipm 18.0 m/min 710 ipm 18.0 m/min 710 ipm 18.0 m/min 500 ipm 12.7 m/min 24+1 (40+1) CT/40 3" / 6" 76 mm / 152 mm 12 lb 5.4 kg SMTC 2.8 sec 3.6 sec ±0.0002" ±0.005 mm ±0.0001" ±0.003 mm 7500 lb 3 402 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC VM3 40" 1016 mm 26" 660 mm 25" 635 mm 4 29" 102 737 mm 54" 1 372 mm 25" 635 mm 4,000 lb 1 814 kg 5/8" 16 mm 3.973" 100 mm #40 Taper 12,000 max rpm Inline Direct Drive 75 ftlb @ 2,100 102 Nm @ 2 100 Air/Oil Injection Liquid Cooled 30 hp 22.4 kW 5,600 lb 24 910 N 5,600 lb 24 910 N 5,600 lb 24 910 N 710 ipm 18.0 m/min 710 ipm 18.0 m/min 710 ipm 18.0 m/min 500 ipm 12.7 m/min 24+1 (40+1) CT/40 3" / 6" 76 mm / 152 mm 12 lb 5.4 kg SMTC 2.8 sec 3.6 sec ±0.0002" ±0.005 mm ±0.0001" ±0.003 mm 14,000 lb 6 350 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC VM6 64" 1626 mm 32" 813 mm 30" 762 mm 4 34" 102 864 mm 64" 1626 mm 28" 711 mm 4,000 1 814 kg 5/8" 16 mm 4.92" 125 mm 12,000 max rpm Inline Direct Drive 75 ftlb @ 2,100 102 Nm @ 2 100 Air/Oil Injection Liquid Cooled 30 hp 22.4 kW 3,400 lb 15 124 N 3,400 lb 15 124 N 5,600 lb 24 910 N 540 ipm 13.7 m/min 600 ipm 15.2 m/min 600 ipm 15.2 m/min 500 ipm 12.7 m/min 24+1 (40+1) CT/40 76 mm / 152 mm 12 lb 5.4 kg SMTC 2.8 sec 3.6 sec ±0.0003" ±0.008 mm ±0.0002" ±0.005 mm 21,000 lb 9526 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC MDC 20" 508 mm 14" 356 mm 20" 508 mm 4 24" 102 610 mm 20" 508 mm 12.75" 324 mm 700 lb per pallet 318 kg 5/8" 16 mm 4.92" 125 mm #40 Taper 7,500 max rpm Direct Speed Belt Drive 75 ftlb @ 1,400 102 Nm @ 1 400 Air/Oil Injection Liquid Cooled 20 hp 14.9 kW 2,550 lb 11 343 N 2,550 lb 11 343 N 5,600 lb 24 910 N 1,000 ipm 25.4 m/min 1,000 ipm 25.4 m/min 1,000 ipm 25.4 m/min 833 ipm 21.1 m/min 24+1 (40+1) CT/40 3" / 6" 76 mm / 152 mm 12 lb 5.4 kg SMTC 2.2 sec 4.8 sec ±0.0002" ±0.005 mm ±0.0001" ±0.003 mm 14,000 lb 6 350 kg 9 scfm, 100 psi 4.25 lpm, 6.9 bar 200 250 VAC 380 480 VAC NOTE: FLA/kVA requirements determined by motor horsepower. Check with your Haas distributor for various requirements. Differing VAC/kVA options available. Specifications subject to change without notice. Not responsible for misprints or typographical errors. Haas Automation, Inc. 8003316746 www.HaasCNC.com | 43 MACHINE SPECIFICATIONS (Standard 50Taper Machines) VF3YT/50 X Y 40" 1016 mm 26" 660 mm 25" 635 mm 7 32" 178 813 mm 52" 1321 mm 23" 584 mm 4,000 lb 1814 kg 5/8" 16 mm 3.15" 80 mm #50 Taper 7,500 max rpm 2Speed Geared Head 450 ftlb @ 500 610 Nm @ 500 Air/Oil Injection Liquid Cooled 30 hp 22.4 kW 5,600 lb 24910 N 5,600 lb 24910 N 5,600 lb 24910 N 710 ipm 18.0 m/min 710 ipm 18.0 m/min 710 ipm 18.0 m/min 500 ipm 12.7 m/min 30+1 CT or BT / 50 4" / 7" 102 mm / 178 mm 30 lb 13.6 kg SMTC 4.2 sec 6.3 sec ±0.0002" ±0.005 mm ±0.0001" ±0.003 mm 15,900 lb 7212 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC VF5/50 | VF5/50XT 50" | 60" 1270 mm | 1524 mm 26" 660 mm 25" 635 mm 7 32" 178 813 mm 52" | 62" 1321 mm | 1575 mm 23" 584 mm 4,000 lb 1814 kg 5/8" 16 mm 3.15" 80 mm #50 Taper 7,500 max rpm 2Speed Geared Head 450 ftlb @ 500 610 Nm @ 500 Air/Oil Injection Liquid Cooled 30 hp 22.4 kW 5,600 lb 24910 N 5,600 lb 24910 N 5,600 lb 24910 N 710 ipm 18.0 m/min 710 ipm 18.0 m/min 710 ipm 18.0 m/min 500 ipm 12.7 m/min 30+1 CT or BT / 50 4" / 7" 102 mm / 178 mm 30 lb 13.6 kg SMTC 4.2 sec 6.3 sec ±0.0002" ±0.005 mm ±0.0001" ±0.003 mm 16,100 lb | 16,650 lb 7303 kg | 7552 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC VF6/50 64" 1626 mm 32" 813 mm 30" 762 mm 5 35" 127 889 mm 64" 1626 mm 28" 711 mm 4,000 lb 1814 kg 5/8" 16 mm 4.92" 125 mm #50 Taper 7,500 max rpm 2Speed Geared Head 450 ftlb @ 500 610 Nm @ 500 Air/Oil Injection Liquid Cooled 30 hp 22.4 kW 5,600 lb 24910 N 5,600 lb 24910 N 5,600 lb 24910 N 540 ipm 13.7 m/min 600 ipm 15.2 m/min 600 ipm 15.2 m/min 500 ipm 12.7 m/min 30+1 CT or BT / 50 4" / 10" 102 mm / 254 mm 30 lb 13.6 kg SMTC 4.2 sec 6.3 sec ±0.0003"2 ±0.008 mm ±0.0002"2 ±0.005 mm 22,500 lb 10206 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC VF7/50 84" 2134 mm 32" 813 mm 30" 762 mm 5 35" 127 889 mm 84" 2134 mm 28" 711 mm 4,000 lb 1814 kg 5/8" 16 mm 4.92" 125 mm #50 Taper 7,500 max rpm 2Speed Geared Head 450 ftlb @ 500 610 Nm @ 500 Air/Oil Injection Liquid Cooled 30 hp 22.4 kW 3,400 lb 15124 N 5,600 lb 24910 N 5,600 lb 24910 N 600 ipm 15.2 m/min 600 ipm 15.2 m/min 600 ipm 15.2 m/min 500 ipm 12.7 m/min 30+1 CT or BT / 50 4" / 10" 102 mm / 254 mm 30 lb 13.6 kg SMTC 4.2 sec 6.3 sec ±0.0003"2 ±0.008 mm ±0.0002"2 ±0.005 mm 24,500 lb 11113 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC Travels Z Spindle Nose to Table Length Width Table Max Weight on Table TSlot Width TSlot Center Distance Taper Size Speed Drive System Spindle Max Torque Standard Bearing Lubrication Cooling Spindle Motor Max Rating1 X Max Thrust Rating Y Z Axis Motors Rapids X Y Z Max Cutting Capacity Standard Tool Type / Taper Max Tool Diameter Standard (full / adjacent empty) Max Tool Weight Changer Type Standard Tool to Tool (avg) Chip to Chip (avg) Positioning Tool Changer Accuracy Repeatability Machine Weight Miscellaneous Air Required Power Required (min) 44 | America's Leading Machine Tool Maker 1) 5minute rating. 2) Linear scales required to achieve accuracy listed. W W W. H AA SC NC .COM HAAS AUTOMATION INC. VF8/50 64" 1626 mm 40" 1016 mm 30" 762 mm 5 35" 127 889 mm 64" 1626 mm 36" 914 mm 4,000 lb 1814 kg 5/8" 16 mm 4.92" 125 mm #50 Taper 7,500 max rpm 2Speed Geared Head 450 ftlb @ 500 610 Nm @ 500 Air/Oil Injection Liquid Cooled 30 hp 22.4 kW 5,600 lb 24910 N 5,600 lb 24910 N 5,600 lb 24910 N 540 ipm 13.7 m/min 600 ipm 15.2 m/min 600 ipm 15.2 m/min 500 ipm 12.7 m/min 30+1 CT or BT / 50 4" / 10" 102 mm / 254 mm 30 lb 13.6 kg SMTC 4.2 sec 6.3 sec ±0.0003"2 ±0.008 mm ±0.0002"2 ±0.005 mm 25,500 lb 11567 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC VF9/50 84" 2134 mm 40" 1016 mm 30" 762 mm 5 35" 127 889 mm 84" 2134 mm 36" 914 mm 4,000 lb 1814 kg 5/8" 16 mm 4.92" 125 mm #50 Taper 7,500 max rpm 2Speed Geared Head 450 ftlb @ 500 610 Nm @ 500 Air/Oil Injection Liquid Cooled 30 hp 22.4 kW 3,400 lb 15124 N 5,600 lb 24910 N 5,600 lb 24910 N 600 ipm 15.2 m/min 600 ipm 15.2 m/min 600 ipm 15.2 m/min 500 ipm 12.7 m/min 30+1 CT or BT / 50 4" / 10" 102 mm / 254 mm 30 lb 13.6 kg SMTC 4.2 sec 6.3 sec ±0.0003"2 ±0.008 mm ±0.0002"2 ±0.005 mm 26,500 lb 12020 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC VF10/50 120" 3048 mm 32" 813 mm 30" 762 mm 5 35" 127 889 mm 120" 3048 mm 28" 711 mm 4,000 lb 1814 kg 5/8" 16 mm 4.92" 125 mm #50 Taper 7,500 max rpm 2Speed Geared Head 450 ftlb @ 500 610 Nm @ 500 Air/Oil Injection Liquid Cooled 30 hp 22.4 kW 3,400 lb 15124 N 5,600 lb 24910 N 5,600 lb 24910 N 360 ipm 9.1 m/min 600 ipm 15.2 m/min 600 ipm 15.2 m/min 360 ipm 9.1 m/min 30+1 CT or BT / 50 4" / 10" 102 mm / 254 mm 30 lb 13.6 kg SMTC 4.2 sec 6.3 sec ±0.0003"2 ±0.008 mm ±0.0002"2 ±0.005 mm 29,500 lb 13381 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC VF11/50 120" 3048 mm 40" 1016 mm 30" 762 mm 5 35" 127 889 mm 120" 3048 mm 28" 711 mm 4,000 lb 1814 kg 5/8" 16 mm 4.92" 125 mm #50 Taper 7,500 max rpm 2Speed Geared Head 450 ftlb @ 500 610 Nm @ 500 Air/Oil Injection Liquid Cooled 30 hp 22.4 kW 3,400 lb 15124 N 5,600 lb 24910 N 5,600 lb 24910 N 360 ipm 9.1 m/min 600 ipm 15.2 m/min 600 ipm 15.2 m/min 360 ipm 9.1 m/min 30+1 CT or BT / 50 4" / 10" 102 mm / 254 mm 30 lb 13.6 kg SMTC 4.2 sec 6.3 sec ±0.0003"2 ±0.008 mm ±0.0002"2 ±0.005 mm 30,900 lb 14016 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC VF12/50 150" 32" 813 mm 30" 762 mm 5 35" 127 889 mm 120" 3048 mm 28" 711 mm 4,000 lb 1814 kg 3/4" 22 mm 4.92" 125 mm #50 Taper 7,500 max rpm 2Speed Geared Head 450 ftlb @ 500 610 Nm @ 500 Air/Oil Injection Liquid Cooled 30 hp 22.4 kW 3,400 lb 15124 N 5,600 lb 24910 N 5,600 lb 24910 N 360 ipm 9.1 m/min 600 ipm 15.2 m/min 600 ipm 15.2 m/min 360 ipm 9.1 m/min 30+1 CT or BT / 50 4" / 10" 102 mm / 254 mm 30 lb 13.6 kg SMTC 4.2 sec 6.3 sec ±0.0003"2 ±0.008 mm ±0.0002"2 ±0.005 mm 32,150 lb 14583 kg 4 scfm, 100 psi 113 lpm, 6.9 bar 200 250 VAC 380 480 VAC C E R T I F I E D NOTE: FLA/kVA requirements determined by motor horsepower. Check with your Haas distributor for various requirements. Differing VAC/kVA options available. Specifications subject to change without notice. Not responsible for misprints or typographical errors. Haas Automation, Inc. 2800 Sturgis Road, Oxnard, California 93030 Toll Free: 8003316746 Fax: 8052788540 www.HaasCNC.com Haas Automation, Europe Mercuriusstraat 28, B1930 Zaventem, Belgium Tel: +32 2 522 99 05 Fax: +32 2 523 08 55 Haas Automation, Asia No. 96 Yi Wei Road, Building 67, Waigaoqiao FTZ, Shanghai 200131 PR.C. . Tel: +86 21 3861 6666 Fax: +86 21 3861 6799 Haas Automation, India Pvt Ltd Plot EL35, TTC Industrial Area, Mahape MIDC, Navi Mumbai 400 709 TEL: +912266098830, 31, 32, 33, 34 39.101038
You need to upgrade your Flash Player
Viewing this eBook requires Adobe Flash Player version 8 or above.
Click below to download the latest version: