INTERNATIONAL SITE MORE LANGUAGES
CAREERS
SITE MAP
Programmed from the centerline using tool offsets.
Allows programs created in the Intuitive Programming System to be saved and rerun at a later date, or transferred to a Haas SL series production turning center as standard G-code.
IPS upgraded threading feature:
Machine tapered threads based on the amount of taper per foot.
Choose right- or left-hand threads.
Chamfer out or straight pull-out at thread's end
Thread repair operations for straight, tapered, right-hand or left-hand, inside or outside diameter threads, without the need to orient the spindle to a known position.