My Haas Welcome,
!
Haas Tooling MyHaas/HaasConnect Sign In Register Haas Tooling MyHaas/HaasConnect Sign Out Welcome, My Machines Latest Activity My Quotes My Account My Users Sign Out
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
      EU SERIES EU SERIES BUILD & PRICE | PRICE LIST BUILD & PRICE | PRICE LIST In-Stock Machines In-Stock Machines WHAT’S NEW WHAT’S NEW YOUR FIRST CNC YOUR FIRST CNC
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
      EU SERIES EU SERIES BUILD & PRICE | PRICE LIST BUILD & PRICE | PRICE LIST In-Stock Machines In-Stock Machines WHAT’S NEW WHAT’S NEW YOUR FIRST CNC YOUR FIRST CNC
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
      EU SERIES EU SERIES BUILD & PRICE | PRICE LIST BUILD & PRICE | PRICE LIST In-Stock Machines In-Stock Machines WHAT’S NEW WHAT’S NEW YOUR FIRST CNC YOUR FIRST CNC
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
Haas Tooling MyHaas/HaasConnect Sign In Register Haas Tooling MyHaas/HaasConnect Sign Out Welcome, My Machines Latest Activity My Quotes My Account My Users Sign Out
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
Chip Auger, Side Discharge (AUGER-SIDE DISCHARGE)

Product Image

DOWNLOAD AN INSTANT CUSTOM QUOTE FOR ANY HAAS MACHINE

GET QUOTE


Chip Auger, Side Discharge

    CNY ONLY
Automatically remove chips from the machine
  • Option Info
  • Details

OVERVIEW

DOCUMENTS

AVAILABLE ON THESE MACHINES

This side-facing auger-style chip conveyor automatically removes chips from the machine, while compressing them and wringing out the coolant. The side-facing chute discharges chips to the side of the machine. 

The auger is ideal for both short runs and high-production environments, eliminating the downtime required for manual chip removal. It can be activated via M-code or directly from the control pendant, and there are settings to control the interval and duration of the auger cycle for automatic operation. Smart-sensing technology automatically reverses the auger if a jam occurs.

  • Discharges chips to the side of the machine
  • Compresses chips, saving space in the chip bin
  • Lift angle minimizes coolant carryout
  • Automatically reverses if a jam occurs
  • Activated via M-code, or from the control pendant
  • Energy efficient via control settings for automatic operation
DOCUMENTS
AVAILABLE ON THE FOLLOWING MACHINES

Chip Auger

Our side-discharge auger-style chip conveyor automatically removes chips from the machine, while compressing them and wringing out the coolant. The side-facing chute discharges chips to the side of the machine

  • Automatically reverses if a jam occurs
  • Activated via M-code, or from the control pendant
  • Settings control the interval and duration of operation
  • Automatic operation increases energy efficiency
  • Lift angle minimizes coolant carryout
  • Compresses chips, saving space in the chip bin

Settings That Control Automatic Auger Operation

  • Setting 114 CONVEYOR CYCLE controls the interval at which the auger (multi-auger, or belt-style conveyor) will start automatic operation during a cycle.
  • Setting 115 CONVEYOR ON-TIME controls the duration the auger (multi-auger, or belt-style conveyor) will run during automatic operation.
  • Setting 196 CONVEYOR SHUTOFF specifies the amount of time to wait without activity prior to stopping the auger.

NOTE: The operator doors must be closed to operate the auger (multi-auger, or belt-style conveyor).

Program Auger Operation

  • M31 starts the auger (multi-auger, or belt-style conveyor) in the forward direction to remove chips. 
    • Once started, and the machine is in cycle, the auger will run for the time specified in Setting 115 CONVEYOR ON-TIME, and then shut off.
    • Once started, and the machine is in cycle, the auger will restart after the time in Setting 114 CONVEYOR CYCLE, and run for the time specified in Setting 115.
    • While the machine is in cycle, you can start the auger by pressing the [CHIP FWD] button on the keyboard. Once started, Settings 114 and 115 have the same effect as described above.
    • If Setting 114 is set to zero, automatic auger operation will not occur.
       
  • M33 stops all automatic auger operation while in cycle.
    • Manually stop the auger while in cycle by pressing the [CHIP STOP] button on the keyboard. This stops all automatic auger operation while in cycle.

Manual Operation

  • Press the [CHIP FWD] button on the keyboard to start the auger (multi-auger, or belt-style conveyor) in the forward direction to remove chips. 
  • Press the [CHIP REV] button on the keyboard to start the auger (multi-auger, or belt-style conveyor) in the reverse direction to clear a jam.
  • Press the [CHIP STOP] button on the keyboard to stop the auger (multi-auger, or belt-style conveyor).
Recently Updated

Auger - Option Spotlight


Here's a quick look at the Haas Chip Auger option available on all Haas VMCs. If you want to spend more time making chips and less time shoveling them out of your machine, check this out.

All prices and specifications subject to change without notice. Freight, rigging, state & local taxes, and dealer installed accessories are not included. Not responsible for misprints or typographical errors. Machines shown with optional equipment. Actual product appearance may differ.

Recently Viewed Items

You Have No Recently Viewed Items Yet

Feedback
Haas Logo

Haas Delivered Price

This price includes shipping cost, export and import duties, insurance, and any other expenses incurred during shipping to a location in France agreed with you as a buyer. No other mandatory costs can be added to the delivery of a Haas CNC Product.