My Haas Welcome,
!
Haas Tooling MyHaas/HaasConnect Sign In Register Haas Tooling MyHaas/HaasConnect Sign Out Welcome, My Machines Latest Activity My Quotes My Account My Users Sign Out
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
      EU SERIES EU SERIES BUILD & PRICE | PRICE LIST BUILD & PRICE | PRICE LIST In-Stock Machines In-Stock Machines WHAT’S NEW WHAT’S NEW YOUR FIRST CNC YOUR FIRST CNC
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
      EU SERIES EU SERIES BUILD & PRICE | PRICE LIST BUILD & PRICE | PRICE LIST In-Stock Machines In-Stock Machines WHAT’S NEW WHAT’S NEW YOUR FIRST CNC YOUR FIRST CNC
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
      EU SERIES EU SERIES BUILD & PRICE | PRICE LIST BUILD & PRICE | PRICE LIST In-Stock Machines In-Stock Machines WHAT’S NEW WHAT’S NEW YOUR FIRST CNC YOUR FIRST CNC
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
Haas Tooling MyHaas/HaasConnect Sign In Register Haas Tooling MyHaas/HaasConnect Sign Out Welcome, My Machines Latest Activity My Quotes My Account My Users Sign Out
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
Haas Oil Skimmer - Installation - AD0480

Service Home How To Procedures Haas Oil Skimmer - Installation - AD0480

Haas Oil Skimmer - Installation - AD0480

- Jump to Section - Back to Top

4.1 Haas Oil Skimmer - Installation

Recently Updated Last updated: 01/19/2023

Haas Oil Skimmer - Installation


AD0480

Rev C - 10/2025

Introduction

This procedure tells you how to install the Haas Oil Skimmer system. The Oil Skimmer does these functions:

  • Automatically removes tramp oil. This decreases bacteria and helps to keep the coolant clean
  • Constant rotation removes oil from the surface of the coolant and deposits it into an external collection container.
  • Starts and stops easily with the toggle switch on the side of the unit. You can also add an electrical timer to automatically start and stop the Oil Skimmer.

For information on maintenance, refer to the Haas Oil Skimmer - Maintenance procedure.

For information on troubleshooting, refer to the Haas Oil Skimmer - Troubleshooting Guide. 

This procedure applies to the following service kits:

  • 93-1000195: OIL SKIMMER HAAS
  • 93-1001137: OIL SKIMMER FIELD INSTALL KIT ST-10/15
  • 93-5046: BRACKET OIL SKIMMER DC-1

Note: 93-5046 is a bracket to help the oil skimmer mount to the coolant tank on DC style machines. 93-5046 needs to be ordered in addition to 93-1000195 when installing the oil skimmer option on a DC-1, DC-2, or DC-4.

Machine Compatibility

  • You can install the Oil Skimmer on machines that have an external 55-gallon (208 L) or 95-gallon (360 L) coolant tank. 
  • UMC-400/SS with a 45-gallon (170 L) coolant tank.
  • SMM/MM/MM-EDU with a 45-gallon (170 L) coolant tank.
  • SMM2/MM2 with a 45-gallon (170 L) coolant tank.
  • Machines ST-10/15/L Machines shipped before 5/14/25: Requires OIL SKIMMER MOUNT BRKT EXT from the Oil Skimmer Mount Bracket Kit (P/N: 93-1001137). ST-10/15/L HPC option is not compatible with the Oil Skimmer.
  • Machines ST-10/15/L Machines shipped after 5/14/25: OIL SKIMMER MOUNT BRKT EXT included. Oil Skimmer Mount Bracket Kit (P/N: 93-1001137) not required. ST-10/15/L HPC option is not compatible with the Oil Skimmer.

The coolant tanks in the list below have a hole and a slot in the coolant tank cover for the Oil Skimmer:

  • 55-gallon (208L) coolant tanks made after May, 2019.
  • 95-gallon (360L) coolant tanks made after Feb, 2019.

For all other machines, you must use the Tank Cover Template to make the hole and the slot in the coolant tank cover.

For all machines made before October 2014, you must use the Enclosure Apron Template to makes holes in the enclosure apron for the female connector on the 25 FT EXTENSION CABLE [B].

 Note: This procedure shows a vertical machine. The installation on lathes and horizontal machines is similar.

Tools Required
  • Drill
  • Jigsaw
  • Drill Bit - 5/32" (0.156")
  • Hole Saw - 1.75"

Templates

Tank Cover -Template

Use this template to make the hole and the slot in the coolant tank cover.

Cut the hole and slot on the left or right side of the cover. Choose the side for your machine that gives you access the Oil Skimmer.

On the top of the cover for the coolant tank, measure and mark the dimensions o the holes.

  • A - 1.20" (3 cm).
  • B - 12.50" (32 cm).
  • C - 8.10" (21 cm).
  • D - 2.20" (6 cm).
  • E - 5.00" (13 cm).
  • F - 3.50" (9 cm).
  • G - 1.50" (4 cm).
  • H - 1.10" (3 cm).

Cut and de-burr the hole and the slot.

Enclosure Apron - Template

For all machines made before October 2014, you must use this template to make (3) holes in the enclosure apron for the female connector on the 25 FT EXTENSION CABLE.

Choose a location in the apron that is near the Oil Skimmer. Put a mark in the apron [A] for the center of the hole.

Measure and mark these dimensions for the holes:

  • B - Ø1.75" (4.4 cm).
  • C - 0.07" (0.1 cm).
  • D - 1.00" (2.5 cm).
  • E - 0.90" (2.3 cm).
  • F - 0.25" (0.6 cm).
  • G - Ø0.156" (0.4 cm).
  • H - 0.156" (0.4 cm).

Cut and de-burr the (3) holes.

Oil Skimmer Installation

1

Note: This step is for DC-Series machines only.

Install OIL SKIMMER BRACKET [1] onto the coolant tank edge before hanging the OIL SKIMMER BASE [2]. 

Hang the OIL SKIMMER BASE [2] over the OIL SKIMMER BRACKET [1].

2

 Note: This step is for ST-10/15/L machines only.

 Note: For machines that were purchased with the oil skimmer option, the Mount Bracket Extension and Oil Skimmer Bracket must be adjusted to match the images.

Fit the OIL SKIMMER MOUNT BRKT EXT [1] to the oil skimmer snout.

Use the OIL SKIMMER MOUNT BRKT EXT [1] as a guide to mark the holes [3] to the oil skimmer snout [2]. 

Remove the OIL SKIMMER MOUNT BRKT EXT [1] and use a #7 drill to make .201" (5.105mm) diameter holes with the drill through both sides of the oil skimmer snout. 

 Note: This step is for ST-10/15/L machines only.

Install the (2) x SHCS 10-32 x 1 1/2 through the OIL SKIMMER MOUNT BRKT EXT [2]. Install the (2) x 10-32 HEX W/ LCKWASHER [3].

Install OIL SKIMMER BRACKET [4] onto the coolant tank edge before hanging the OIL SKIMMER BASE [5]. 

Hang the OIL SKIMMER BASE [5] over the OIL SKIMMER BRACKET [4].

3

Hang the OIL SKIMMER BASE [A] from the Coolant Tank with the hanging hooks engaged onto the Coolant Tank Lid [1].  The horizontal surface of the hanging hooks should be flat on the top of the Coolant Tank Lid edge.

 

 

4

Fill the Oil Skimmer Chambers with clean coolant up to the drain [1] facing the coolant tank.

NOTE: The two chambers are connected with a slot at the bottom [2]. Make sure both chambers are filled. 

5

Install the OIL SKIMMER TOP ASSEMBLY [H] by positioning the narrow end of the Oil Skimmer into the Coolant Tank lid opening and then fitting the motor end onto the base engaging the alignment slots [1].

6

Attach the female connector on the 25 FT EXTENSION CABLE [B] to the enclosure apron. Use the (2) BOLTS [G].

Apply the DECAL [C] to the enclosure apron.

7

Connect the 25 FT EXTENSION CABLE [B] to the GFCI outlet [1] on the control cabinet.

Use the CABLE TIES [D], the CLAMPS [E], and the MOUNTS [F] as necessary to route the cable.

Connect the power cable [2] for the Oil Skimmer to the female connector on the 25 FT EXTENSION CABLE [B] in the enclosure apron.

Oil Skimmer Operation

Turn the switch [1] to the on position.

Empty the Oil Container when full.

The oil skimmer is equipped with replacement scraper rings and replacement skimmer belt. Replace these components periodically based on their condition.

Overtime, coolant will get dirty. Replace with clean coolant periodically based on its condition. 

Recently Viewed Items

You Have No Recently Viewed Items Yet

Feedback
Haas Logo

Haas Delivered Price

This price includes shipping cost, export and import duties, insurance, and any other expenses incurred during shipping to a location in France agreed with you as a buyer. No other mandatory costs can be added to the delivery of a Haas CNC Product.