My Haas Welcome,
!
Haas Tooling MyHaas/HaasConnect Sign In Register Haas Tooling MyHaas/HaasConnect Sign Out Welcome, My Machines Latest Activity My Quotes My Account My Users Sign Out
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
      EU SERIES EU SERIES BUILD & PRICE | PRICE LIST BUILD & PRICE | PRICE LIST In-Stock Machines In-Stock Machines WHAT’S NEW WHAT’S NEW YOUR FIRST CNC YOUR FIRST CNC
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
      EU SERIES EU SERIES BUILD & PRICE | PRICE LIST BUILD & PRICE | PRICE LIST In-Stock Machines In-Stock Machines WHAT’S NEW WHAT’S NEW YOUR FIRST CNC YOUR FIRST CNC
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
      EU SERIES EU SERIES BUILD & PRICE | PRICE LIST BUILD & PRICE | PRICE LIST In-Stock Machines In-Stock Machines WHAT’S NEW WHAT’S NEW YOUR FIRST CNC YOUR FIRST CNC
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
Haas Tooling MyHaas/HaasConnect Sign In Register Haas Tooling MyHaas/HaasConnect Sign Out Welcome, My Machines Latest Activity My Quotes My Account My Users Sign Out
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
UMC Hydraulic Vise - Troubleshooting Guide - TG0089

Service Home UMC Hydraulic Vise - Troubleshooting Guide - TG0089

UMC Hydraulic Vise - Troubleshooting Guide - TG0089

- Jump to Cause - Back to Top
Recently Updated Last updated: 10/15/2025

UMC Hydraulic Vise - Troubleshooting Guide


TG0089

Introduction

The UMC series machines have two types of workholding and vises: hydraulic [1] and pneumatic [2]. This troubleshooting guide will have information in regards to the hydraulic workholding [1]. 

For further information on how to install the hydraulic or pneumatic workholding mechanisms/vises please refer to the links below:

Hydraulic Workholding Links: 

  • Hydraulic Workholding Installation (mechanism)
  • Hydraulic Vise Installation

Symptom Table

Symptom Probable Casue Corrective Action
Hydraulic fluid is coming out of the air blast port. Verify orientation of the ports between the coupler and the spud of the vise. The open and close ports may be lined up with the air blast port.  Remove the vise from the platter and verify if the orientation is correct. Newer versions of the coupler will have the air port labeled "AIR" 
Vise jaws are not closing when commanded and HPU is functioning properly.
Hydraulic lines are clogged.  Debris may have been introduced when installing or removing the hydraulic vise from the machine. 

If the system has a the hydaulic filter fitting on the side attached to the HPU, check the filter fittings to see if any debris is present. 

If debris is present clean the fitting off, replace the hydruaulic oil and continuously check the fitting so it does not get clogged. Replace the fittings as needed

Clamp and unclamp solenoids have failed due to debris present in the hydraulic oil.

If the system does not have the hydraulic filter fitting on the side attached to the HPU, update the system by ordering two 58-2127 FILTER 65 MICRON HYD 6ORBM 6JICM STR STL and replace the two 58-0038 FITG ORB6M JIC6M STR STL that were already installed on the hose. 

Replace the hydraulic oil and continuously check the fitting so it does not get clogged. Replace the fittings as needed

HPU - Hydraulic Vise Pressure on the gauges page is dropping . The pressure sensor is monitoring the accumulator pressure not the vise pressure. Visit the Hydraulic Vise -  HPU Dial and Valve section for futher information
Hydraulic Vise - Part is moving while clamped . The clamping force is not set correctly .  Adjust the valve on the HPU to the correct pressure using the decal posted on the HPU. Visit the Hydraulic Vise -  HPU Dial and Valve section for futher information.
Message: Foot pedal 1 is locked out. The foot pedal is pressed when in the EDIT mode or LIST PROGRAM mode. Navigate off of the EDIT mode or LIST PROGRAM mode.
Alarm 391 FEATURE DISABLED Workholding is not setup on Workholding Tab. Enable the workholding on the Workholding tab. See the Programmable Air - Installation procedure for more information.
Broken dove tail jaw. Incorrect part setup on jaws. Refer to the Proper Dovetail Usage reference document. 
Unable to set pressure consistently. Faulty cartridge valve.
Check cartridge valve for any leaks. If there are no leaks, replace cartridge valve. 
Can not reach above 100 psi 

Machines with a Blank Platter

1

This section is for hydraulic vises with 2 mounting bollts.

Blank platters have a no drill zone [1] of  Ø7.25 in. and ↧1.75 in. for custom workholding on these platters.  

Machines sold with a blank platter also have the option of purchasing the Haas hydraulic vise. 

To install the vise the user will need to drill mounting holes outside the no drill zone [1].  Home the B & C-Axis and drill using the hole pattern that follows:

  • Haas Hydraulic Vise: (2x) 1/2-13 holes at 9 in. (on center) [2]

for the mounting bolts, the mounting bolt. Use the brake bleed access hole for reference [3].

NOTE: Pictured is a UMC-500 blank platter but the no drill zone and Haas hydraulic vise hole pattern will be the same throughout all UMC models. 

2

This section is for hydraulic vises with 4 mounting bollts.

Blank platters have a no drill zone [1] of  Ø7.25 in. and ↧1.75 in. for custom workholding on these platters.  

Machines sold with a blank platter also have the option of purchasing the Haas hydraulic vise. 

To install the vise the user will need to drill mounting holes outside the no drill zone [1].  Home the B & C-Axis and drill using the hole pattern that follows:

  • 6 & 8 in. Hydraulic Vise  – 4x ½-13 at 103.6mm [2] x 63mm [3] (on center)
  • 10 in. Hydraulic Vise – 4x ½-13 at 124.7mm [2] x 63mm [3] (on center)

For the mounting bolts, the mounting bolt. Use the brake bleed access hole for reference [3].

NOTE: Pictured is a UMC-500 blank platter but the no drill zone and Haas hydraulic vise hole pattern will be the same throughout all UMC models. 

Hydraulic Vise - HPU Dial and Valve

1

Pressure drop on the controller gauge page is normal as it is monitoring the accumalator pressure [1]. Pressure on the controller should always be higher than on the dial for the system to keep clamping force consistent.

 NOTE: 100 psi/5 minutes is what is considered normal pressure drop.

2

The HPU dial [1] located on the HPU will display the pressure applied to the vise, the controller HPU pressure found on the gauge page will display the pressure monitored from the accumulator [2].

 NOTE: The pressure may vary within 10 psi as long as the accumulator is funtioning properly. 

3

To make adjustments to the pressure applied to the vise, the knob denoted as [1] is used to make the adjustment while knob denoted as [2] is used to lock the adjustment in place.

NOTE: If the pressure value is drifting more than 10 psi on the dial check if knob [2] is locked in place and check for any leaks from the vise or the system. 

 

4

Haas hydraulic vises will have a hydraulic vise clamp force chart that can be used to achieve the correct clamp force in relation to the pressure on the dial. 

NOTE: This chart will NOT apply to third party vises. 

 

Electrical Diagram

1

When running the wires, make sure there isnt excess strain on the cables. Check to make sure all connections are secure and in the correct location based on the diagram above. 

Recently Viewed Items

You Have No Recently Viewed Items Yet

Feedback
Haas Logo

Haas Delivered Price

This price includes shipping cost, export and import duties, insurance, and any other expenses incurred during shipping to a location in France agreed with you as a buyer. No other mandatory costs can be added to the delivery of a Haas CNC Product.