My Haas Welcome,
!
Haas Tooling MyHaas/HaasConnect Sign In Register Haas Tooling MyHaas/HaasConnect Sign Out Welcome, My Machines Latest Activity My Quotes My Account My Users Sign Out
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
      EU SERIES EU SERIES BUILD & PRICE | PRICE LIST BUILD & PRICE | PRICE LIST In-Stock Machines In-Stock Machines WHAT’S NEW WHAT’S NEW YOUR FIRST CNC YOUR FIRST CNC
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
      EU SERIES EU SERIES BUILD & PRICE | PRICE LIST BUILD & PRICE | PRICE LIST In-Stock Machines In-Stock Machines WHAT’S NEW WHAT’S NEW YOUR FIRST CNC YOUR FIRST CNC
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
      EU SERIES EU SERIES BUILD & PRICE | PRICE LIST BUILD & PRICE | PRICE LIST In-Stock Machines In-Stock Machines WHAT’S NEW WHAT’S NEW YOUR FIRST CNC YOUR FIRST CNC
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
Haas Tooling MyHaas/HaasConnect Sign In Register Haas Tooling MyHaas/HaasConnect Sign Out Welcome, My Machines Latest Activity My Quotes My Account My Users Sign Out
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
13 - High Pressure Flood Coolant

Chip Removal and Coolant - Service Manual


  • 1 - Chip and Coolant - Introduction
  • 2 - Auxiliary Coolant Filter
  • 3 - Single-Stage Flood Coolant
  • 4 - Oil Skimmer
  • 5 - Programmable Coolant
  • 6 - Chip Auger
  • 7 - Coolant Chiller
  • 8 - Chip Conveyor - Overview
  • 8a - Standard Belt Chip Conveyor
  • 8c - CDF Chip Conveyor
  • 9 - Chip Conveyor - VMC
  • 10 - Chip Conveyor - UMC
  • 11 - Chip Conveyor - Lathe
  • 12 - Coolant Refill
  • 13 - High Pressure Flood Coolant
  • 14 - Through-Spindle Coolant
  • 15 - Through-Tool Air Blast
  • 15a - Through-Tool Oil Mist
  • 16 - Haas Chip Lift
  • 17 - Mist Condenser
  • 18 - Coolant Level Float Sensor
  • 19 - Mini Conveyor
  • 20 - Coolant VFD
  • 21 - Coolant Sanitizer
  • 22 - Chip Separator
  • 23 - Chip Tray Strainer
  • 24 - Multi-Stage Flood Coolant
  • 25 - Coolant Cart

Go To :

  • 13.1 HPFC Overview
  • 13.2 HPFC Installation
  • 13.3 HPFC Troubleshooting

13.1 HPFC - Overview

High-Pressure Flood Coolant

The number one cause of premature tool failure is re-cutting chips. Our High-Pressure Flood Pump delivers up to 45% more coolant to the cutting zone – at higher pressure – to flush out chips and swarf. High-volume, high-pressure coolant is delivered through our multi-nozzle flood coolant ring to maximize efficiency.

NOTE: This system is louder than the standard flood coolant system, due to the higher pressures involved, and the spur gear drive system. It is operating as expected.

13.2 HPFC - Installation

Recently Updated

High Pressure Flood Coolant (HPFC) - Installation


AD0502

Introduction

This procedure will explain how to install the High Pressure Flood Coolant with TSC, TSC ready, and no TSC.

Prerequisites: 

Software version 100.20.000.1010 will be required to run HPFC, please upgrade to this version if that has not already been done. 

Note: The Auxiliary Filter can not be plumbed directly to the HPFC pump,  it can only be plumbed to the TSC system.

This procedure applies to the Mill kits in the table below. Use the table to determine the correct upgrade kit needed.

Upgrade Type Applicable Kit
HPFC upgrade w/ TSC 300/1000 93-1000705: STD TO HPFC FIELD INSTL KIT ALL MACHINES
HPFC upgrade w/ TSC ready
HPFC upgrade w/ no TSC
HPFC upgrade VFD coolant w/ no TSC

93-1000704: VFD TO HPFC 3' PWR CBL FIELD INSTALL KIT

93-1000706: VFD TO HPFC 23' PWR CBL FIELD INSTALL KIT

93-1000707: VFD TO HPFC 14' PWR CBL FIELD INSTALL KIT

HPFC upgrade VFD coolant w/ TSC 300/1000
HPFC upgrade VFD coolant w/ TSC ready
HPFC pumps sent out between July and December of 2020 upgrade to current production HPFC pumps. 93-3380: HPFC RETROFIT KIT

Note: When this kit is being used for the upgrade, go to step 5.
If the pump on a assembly that was built from July to December of 2020 breaks the whole assembly needs to be replaced.  30-12691A: VFD TO HPFC 3' PWR FIELD INSTALL KIT

Installation

1

Push [POWER OFF]. Set the main circuit breaker to the OFF position.

Open the electrical cabinet door.

Lock the main circuit breaker. Use an approved lock with an approved safety tag.

 Danger: After turning off the machine, wait at least 5 minutes before working in the electrical cabinet, to allow power to dissipate. Wait for the voltage indicator LED on the vector drive to go off completely.

2

Replace the coolant filter cap [1] with the new one [2] as shown. 

If the set screws do not have a hex port for an allen key, use two jam nuts (5/16"-18) and back the set screws out of the filter housing about 0.70" (17.7mm).  

Note: You may need to apply some heat to loosen the Loctite from the set screws.

3

Removing the standard coolant pump. Image [1] shows the TSC option being included image [2] shows the TSC ready/no TSC configuration.

4

Install the High Pressure Flood Coolant (HPFC) pump. Image [1] shows the TSC option being included image [2] shows the TSC ready/no TSC configuration.

5

Convert standard pump to HPFC or Upgrade Existing HPFC to Current Build

Route the hoses from the HPFC pump [A] as shown.

The air hose [1] will come from the TRP solenoid in the lube panel and connect to the air cylinder.

A tee fitting [5] and 1/4 push to connect fitting [4] will need to be attached to the TRP solenoid [3]. Then connect the air hose [1] to the push to connect fitting [4].

The output hose from the HPFC will go to the filter [2].

Note: Machines with TSC previously had the purple air line split between the TSC and HPFC pumps, that is no longer the case and the HPFC pump should be connected to the TRP solenoid [3] as shown in the image.

Through Spindle Coolant - Field Install - Not TSC Ready - NGC

6

For machines that are not TSC ready, refer to this TSC procedure.

7

VFD coolant upgrade to HPFC

If you are upgrading from the VFD coolant system to HPFC remove the current cable on the coolant connection bracket and replace with the cable provided as shown [1].

Route the new cable from the bracket to I/O P29.

Note: VFD will no longer be used, a patch is required to disable the drive. Contact the Service Department for the patch.

Option - Activation Code + Patch - NGC

8

Please refer to the link to verify and load any patches involved with the installation.

13.3 HPFC - Troubleshooting

Recently Updated

High Pressure Flood Coolant (HPFC) - Troubleshooting Guide - NGC


TG0083

Download and fill out the coolant pump Inspection Report Checklist below before replacing any parts.

Coolant pump Inspection Report Checklist

Introduction

The HPFC is an option that replaces the standard coolant. The HPFC can be paired with TSC and TSC ready machines, but cannot be paired with a VFD. 

Within recent years, Haas Automation has made design updates to the HPFC. To identify which generation you are dealing with, look for the following key identifying features below.

1st Generation [A]:

  • Coolant flows through hose [1] surrounded by a spring [2]

2nd Generation [B]: 

  • Coolant flows through PVC pipes [3] with no spring 

Symptoms Table

Symptom Possible Cause Corrective Action
The O-ring in the filter casting is pushed out causing coolant to leak or spray out of the top cover The filter cover was not replaced when installing/upgrading to HPFC Replace the filter cover follow the Filter Cover Replacement section
Excessive noise from the HPFC coolant pump.   The coolant nozzles valves are closed. Makes sure all the coolant nozzle valves are open. If not, HPFC can be noisy at normal conditions. Measure the noise with a DB meter at: the front of the machine when sliding doors open/closed and the back of the machine 3 ft away from the pump.
Low coolant levels.  Check coolant levels and refill as necessary. 
There is an alignment problem due to  the pump not properly seated. Loosen and re-tighten the standoffs supporting the pump. Refer to the Standoff Alignment section below for more information. 
Gear pump coupler misalignment. Order kit 93-4195 Coolant Gear Pump Coupler Conversion Kit. Follow the Pump Head Coupling - Flexible Coupling Replacement procedure. If noise persists, replace pump head.
Low coolant flow, the pump cavitates (cavitation sounds like heavy grit in the pump head, or a suction sound) or is otherwise noisy.
1st Generation Only: The pick-up hose can kink when the pump is running.  Replace the pick-up hose with the new version with a spring.
Low coolant levels.  Check coolant levels and refill as necessary.
Gear pump coupler misalignment. Order kit 93-4195 Coolant Gear Pump Coupler Conversion. Follow the Pump Head Coupling - Flexible Coupling Replacement procedure.  If noise persists, replace pump head. 
Pressure loss is observed The pressure relief set screw may have fallen out Reinstall the set screw adding blue Loctite on it as well. See Pressure relief adjustment section on how to properly replace the set screw.
2nd Generation Only: The PVC plumbing has come undone. Reassemble plumbing. If plumbing is having issues staying intact, use PVC glue from any hardware store to keep plumbing from coming undone. 
HPFC pumps from July to December of 2020 lose functionality after a software upgrade. The HPFC pump needs to be upgraded to match the current production HPFC pumps. Order kit 93-1000705 STD TO HPFC FIELD INSTALL KIT ALL MACHINES, follow the High Pressure Flood Coolant (HPFC) - Installation procedure.
No coolant flow or pump motor running backwards. Incorrect power phasing - the pump motor is running backward. Check the phasing indicators and change the incoming power cables, if necessary.
The 230V system does not turn ON and the red LED on the motor drive PCB is OFF.  The jumper on the motor drive PCB is incorrectly located or defective.  Make sure that the motor drive PCB has a jumper installed on P3 inbetween pin 1 and 2 (the bottom two pins). 
There is no 12V input power.  Make sure that the 12V input power is connected to P2 on the motor drive PCB. 
Machine coolant hose leaks at the fittings or the hose pops off the fittings. 1st Generation Only: The 5/8" Hose Clamp PN: 59-1524 installed on the coolant hose is oversized and does not clamp the hose correctly. Replace the oversized hose clamp with PN: 59-2107 HOSE CLAMP EAR 20.1 - 23.3 MM. Use a crimping tool to secure the new hose clamp.

Filter Cover Replacement

If the O-ring [1] was pushed out of position replace the original filter cover [2] with the new thick filter cover [3]. IF the O-ring is damaged replace the O-ring.

Replace the coolant filter cap [1] with the new one [2] as shown. 

If the set screws do not have a hex port for an allen key, use two jam nuts (5/16"-18) and back the set screws out of the filter housing about 0.70" (17.7mm).  

Note:  You may need to apply some heat to loosen the Loctite from the set screws.

Standoff Alignment

Remove the side panel covering the pump in order to access the standoffs. 

Loosen the (x4) standoff bolts. 

Re-tighten the (x4) standoff bolts. 

Run the pump while listening for excessive noise. 

Pressure Relief Adjustment

Only applicable for 1st Generation:
 
1. If your flow appears low, tighten set screw 1/8 of a turn at a time until you've reached a desired flow at the spindle coolant manifold. 
 
NOTE: Only adjust the set screw 1/8 of a turn at a time. If it is fastened all the way, the flow could be so strong that it could blow a hose off the machine or the lid off the filter. 
 

2. With the pump running, close the valve on the hose assembly and observe the pressure on the valve

3. Remove the pump from the tank. Adjust the set screw to adjust the pressure, the pressure range is from 170-210 PSI. If the set screw gets adjusted, check the blocked pressure at the pump outlet and make sure it doesn't exceed 200 psi.

 NOTE: Tightening the screw will increase pressure, loosening will decrease pressure.

 IMPORTANT: Make sure to add blue Loctite to the set screw

Incorrect Input Power-Phasing

The power supply PCB has a phase detect with neon indicators on the top center portion of the board. Make sure that the electrical power is phased correctly:

  • Green Light: The incoming power is phased correctly.
  • Orange Light: The incoming power is incorrectly phased.
  • Both Lights: A phase is missing (there is a loose cable in the system).

If the electrical power is phased incorrectly:

Set the main circuit breaker on the machine to the OFF position.

Lock the main circuit breaker. Use an approved lock with an approved safety tag.

Swap the #74 and #75 incoming power cables at the main transformer.

Kinked Pick-up hose

Only applicable for 1st Generation:

The pick-up hose can kink when the pump is running. Replace the pick-up hose with the new version with a spring.

Electrical Schematic

1st Generation

2nd Generation

Recently Viewed Items

You Have No Recently Viewed Items Yet

Feedback
Haas Logo

Haas Delivered Price

This price includes shipping cost, export and import duties, insurance, and any other expenses incurred during shipping to a location in France agreed with you as a buyer. No other mandatory costs can be added to the delivery of a Haas CNC Product.