My Haas Welcome,
!
Haas Tooling MyHaas/HaasConnect Sign In Register Haas Tooling MyHaas/HaasConnect Sign Out Welcome, My Machines Latest Activity My Quotes My Account My Users Sign Out
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
      EU SERIES EU SERIES BUILD & PRICE | PRICE LIST BUILD & PRICE | PRICE LIST In-Stock Machines In-Stock Machines WHAT’S NEW WHAT’S NEW YOUR FIRST CNC YOUR FIRST CNC
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
      EU SERIES EU SERIES BUILD & PRICE | PRICE LIST BUILD & PRICE | PRICE LIST In-Stock Machines In-Stock Machines WHAT’S NEW WHAT’S NEW YOUR FIRST CNC YOUR FIRST CNC
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
      EU SERIES EU SERIES BUILD & PRICE | PRICE LIST BUILD & PRICE | PRICE LIST In-Stock Machines In-Stock Machines WHAT’S NEW WHAT’S NEW YOUR FIRST CNC YOUR FIRST CNC
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
Haas Tooling MyHaas/HaasConnect Sign In Register Haas Tooling MyHaas/HaasConnect Sign Out Welcome, My Machines Latest Activity My Quotes My Account My Users Sign Out
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
5 - PulseJet System

Lubrication Systems - Service Manual


  • 1 - Lube Systems - Introduction
  • 2 - Haas Axis Lubrication Oil
  • 3 - Haas Liquid Grease
  • 4 - Minimum Quantity Lubrication
  • 5 - PulseJet System

Go To :

  • 5.1 PulseJet - Installation
  • 5.2 PulseJet - Service Replacement
  • 5.3 PulseJet - Lubrication Chart
  • 5.4 PulseJet - Troubleshooting
Recently Updated

PulseJet - Installation


AD0454

Revision D - 7/2026

Introduction

Updated

This procedure will show you how to install a PulseJet on VMC/UMC mills.

Required Installation Kit:

  • 93-1000191 PULSEJET FIELD INSTALL KIT

Machine Requirements:

  • VMC/UMC built on October 2019 or later.
  • 100.19.000.1123 Software Version or higher.
  • Programmable Coolant option

PulseJet Installation Video

The following service video shows how to install the PulseJet System on VMC and UMC machines.

 NOTE: This service video is for reference only and does not replace the written procedure.

Hoses and Sensor Cable Installation

Note:  This section is required for field installations, go to the next section if the Pulsejet option was purchased from the factory.

1

The illustration shows the PulseJet hose routing on a VF-2: 1: Top View 2: Side View.

Route the nozzle air hose (1/4 inch black hose) from the CALM cabinet, through spindle head,  towards the PulseJet/PCool location.

Route the nozzle oil hose (5/32 inch clear hose): from the Oil reservoir, up onto the roof, into cable carrier, through spindle head, towards the PulseJet/Pcool location.

Route the Oil Reservoir air hose (1/4 inch clear hose) from CALM cabinet solenoid towards the Oil Reservoir location.

NOTE: Make sure you leave enough slack at both ends.

2

Route the Oil Reservoir level sensor cable from the Oil Reservoir location, to the top of the roof to the electrical cabinet.

NOTE: Make sure you leave enough slack to connect the cable to the Oil Reservoir sensor.

Plug in the cable to the I/O PCB at P71.

PulseJet & Tank Installation

1

Turn off air to the machine.

Locate the air manifold [1], remove the third NPT plug below the air gauge.

Install the adapter fitting P/N 58-1521 [2] into the manifold.

Install the solenoid valve [3] oriented as shown.

Connect the solenoid cable to the adapter then connect the adapter to the connector panel labeled "PULSEJET".

 NOTE: If installing on a machine that has the CAN Lube Rack, do not use the air/lube solenoid cable adapter (33-0596). Instead, plug directly into the connector labeled 'PULSEJET" on the CAN Lube Rack.

2

Unpack the PulseJet nozzle assembly.

Loosen the clamp screw [1] and slide the clamp and the PulseJet assembly onto the P-COOL nozzle.

Adjust the PulseJet nozzle so that the oil inlet fitting [2] is on the bottom. 

Aim the nozzle approximately at the spindle centerline (it will be adjusted later).

Tighten the clamp set screw.

Find the 1/4” black air hose [3] and connect it to the air fitting on the nozzle assembly.
Find the 5/32” clear oil hose [4] but DO NOT connect it to the oil fitting.  This hose will be connected during the prime procedure.

3

Mount the Oil Reservoir to the machine enclosure, refer to the illustration.

The oil reservoir assembly has magnets for easy mounting. 

Important: Do not slide the magnets on the enclosure. Instead, if you need to move the reservoir, tilt it to detach the magnets and then gently set it back down.

4

Connect the cable and air hoses to the Oil Reservoir assembly refer to the diagram.

Connect the air hoses to the solenoid. 

  Important: Make sure to connect the correct hoses to the solenoid, matching the color zip ties. If the hoses are swapped, it will send high pressure to the tank and could rupture the tank.

5

Slide the strain relief [1] into the slot on the reservoir assembly and tighten the retaining nut.

Apply the supplied spiral wrap [2] from the enclosure to the top of the machine to help neatly organize and secure the cables.

Make sure the drain valve on the bottom of the reservoir is in the closed (horizontal) position [4].

Remove the reservoir cap and fill the tank with oil [3].  Do not overfill the tank.
NOTE: The tank requires air space above the oil to maintain positive pressure above the oil.

Reinstall cap.

Prime the Oil Line

Make sure there is oil in the PulseJet reservoir and that the lid is tightly installed. Make sure the reservoir air and oil lines are connected. 

Disconnect the oil line [1] from the PulseJet nozzle and let it drape over a container placed on the mill table.

Press [DIAGNOSTIC] and navigate to the Maintenance then to the PulseJet tab [2]. 

Press [F4] to begin a priming cycle. Each cycle lasts 10 minutes.  The reservoir will be pressurized during the cycle. 

Note: Small machines may take only 1 cycle to fully prime the line. Larger machines may take 3 or 4 cycles. Heavier oils may take longer to prime. Continue running priming cycles until oil [4] begins to drip out of the oil line into the container. 

Note: While the machine is in the prime cycle the user can start a program.   However the user will not be able to start the prime cycle again while the program is running.

Reconnect the oil line to the PulseJet nozzle.

In MDI run:

M162 P10;
G04 P10.;
M30;

Test the PulseJet until a strong stream develops. 

PulseJet M-codes

M-CODE

DESCRIPTION

WHAT IT’S USED FOR

M160

Cancel Active PulseJet

To cancel an active PulseJet M-code.

M161 Pnn

Continuous Mode

Will turn PulseJet on whenever a feed move is active in a program. Pnn is how many seconds between oil pulses. Min = 1 sec Max = 99 sec

M162 Pnn

Single Event Mode

Will turn on PulseJet for a defined number of pulses. Pnn is how many pulses. Best used for drilling and tapping or to manually lubricate a tool.
Note:  M162 Pnn Is a non-blocking code.  Anything after the code will be executed immediately.

M163 Pnn

Modal Mode

Activates PulseJet to turn on during any canned drill or tap cycles. Pnn is how many pulses for each hole.

Note: Any PulseJet M-code will override any active previous PulseJet M-code.  
Note: Settings 369 and 370 can be used to change the default values for M161 and M162 when no P is specified.

Tips and Troubleshooting

1.       PulseJet will produce a consistent, fast, and tight oil pulse if the line is well primed, the dispenser needle is not clogged, and a recommended oil is being used.

2.       To always keep the line well primed:

  • Place the reservoir assembly near or above the spindle elevation
  • never let the tank run completely dry

3.       If you suspect that the dispenser needle is clogged, replace it. To do this, unscrew the knurled nozzle cap from the nozzle and gently twist and pull the yellow base of the needle off of the nozzle.

Note: This will expose the small check valve spring, do not lose it. Firmly press the replacement needle onto the nozzle taper. Re-install the nozzle cap finger tight.

4.       Use recommended oil: light viscosity oils and tapping or cutting fluids work the best. Heavy viscosity oils such as motor oil, gear oil, or heavy tapping oils may not produce a high-quality stream.

5.       If the oil line does get air bubbles inside, the pump inside the PulseJet nozzle will pass them through the system. While bubbles are moving through the nozzle, the stream will appear weak, aerated, and inconsistent. After the bubbles pass through, the stream will return to its proper form.

6.       Always make sure the reservoir cap is installed and tightened when running PulseJet to maintain the proper tank pressure.

PulseJet Lubrication

Refer to Lubricant Grease, and Sealant Table to see our recommended oil list.

Recently Updated

Pulsejet - Service Replacement


AD0511

Introduction

Use this procedure to replace the following Pulsejet components in the field:

  • 93-30-12599    Pulsejet nozzle assembly
  • 93-30-12603    PulseJet solenoid assembly
  • 93-30-12600    PulseJet tank assembly

Note: If installing the PulseJet option for the first time, do not use this document.  Refer to Pulsejet - Installation procedure.

Nozzle Replacement

1

To remove the pulsejet nozzle:

  • Disconnect the air and oil lines.
    Note: Inspect the lines for damage or kinks, and replace them if necessary.
  • Loosen the clamp screw [1] and slide the PulseJet nozzle out of the P-COOL nozzle.
    Important: Support the P-COOL nozzle while you loosen the clamp screw.

Unpack the PulseJet nozzle assembly.

  • Loosen the clamp screw [1] and slide the clamp and the PulseJet assembly onto the P-COOL nozzle.
     Important: Support the P-COOL nozzle while you tighten the clamp screw.
  • Adjust the PulseJet nozzle so that the oil inlet fitting [2] is on the bottom. 
  • Aim the nozzle approximately at the spindle centerline (it will be adjusted later).

Tighten the clamp set screw.

Find the 1/4” black air line [3] and connect it to the air fitting on the nozzle assembly.
Find the 5/32” clear oil line [4] connect it to the oil fitting. 

Command 10-20 pulses until oil is properly streaming out of the nozzle.

 Note: If you are only replacing the nozzle (and not the tank) you do not need to run a full priming cycle.

Solenoid Replacement

1

Turn off air to the machine.

Locate the PulseJet solenoid [1].

Disconnect the two air lines [2,3] from the solenoid.

Important:  Mark the position of the two air lines, they will need to be installed in the same position.

Disconnect the solenoid cable from the connector bracket.

Remove the old solenoid and install the new one.

Connect the air lines to the solenoid.

Note:  The 1/4" clear line [2] attahced to the port with an orifice.  The 1/4" black line [3] connects to the port with no orifice.  

Connect the solenoid cable to the connector panel labeled "PULSEJET".

Turn on the incoming air and test the PulseJet.

Tank Replacement

1

Locate the tank [1] assembly on the side of the machine.

Place a large container [2] to drain the oil (at least 3 quarts).  

Note: if you plan to re-use the oil, the container must be thoroughly cleaned.

Open the valve [3] to let it completely drain. Loosen the tank cap to speed up the draining.

Once the oil is drained, close the drain valve.

Carefully lift the magnetic tank off the machine using a tilting motion. Turn the tank so that you can access the rear of the tank.

Carefully disconnect the air line [4] and oil level sensor [5].

Disconnect the oil line [6].

Note: Oil may flow back through the line, so have a container to place the line in to catch the oil.

2

Connect the 5/32" oil line [1], level sensor cable [2] and the 1/4"  tank air line  (see diagram).

Carefully install the tank to the side of the machine with the magnets.

Make sure the drain valve [4] is closed.

Open the tank cap and re-fill the tank with oil. Firmly replace cap until it “clicks”.

There will be air trapped inside the system from disconnecting and reconnecting the oil line. This air must be purged out before PulseJet can be used effectively. 

Refer to the Prime the Oil Line section in this document.

Prime the Oil Line

Make sure there is oil in the PulseJet reservoir and that the lid is tightly installed. Make sure the reservoir air and oil lines are connected. 

Disconnect the oil line [1] from the PulseJet nozzle and let it drape over a container placed on the mill table.

Press [DIAGNOSTIC] and navigate to the Maintanance then to the PulseJet tab [2]. 

Press [F4] to begin a priming cycle. Each cycle lasts 10 minutes.  The reservoir will be pressurized during the cycle. 

Note: Small machines may take only 1 cycle to fully prime the line. Larger machines may take 3 or 4 cycles. Heavier oils may take longer to prime. Continue running priming cycles until oil [4] begins to drip out of the oil line into the container. 

Note: While the machine is in the prime cycle the user can start a program.   However the user will not be able to start the prime cycle again while the program is running.

Reconnect the oil line to the PulseJet nozzle.

In MDI run:

M162 P10;
G04 P10.;
M30;

Test the PulseJet until a strong stream develops. 

Tips and Troubleshooting

1.       PulseJet will produce a consistent, fast, and tight oil pulse if the line is well primed, the dispenser needle is not clogged, and a recommended oil is being used.

2.       To always keep the line well primed:

  • Place the reservoir assembly near or above the spindle elevation
  • never let the tank run completely dry

3.       If you suspect that the dispenser needle is clogged, replace it. To do this, unscrew the knurled nozzle cap from the nozzle and gently twist and pull the yellow base of the needle off of the nozzle.

Note: This will expose the small check valve spring, do not lose it. Firmly press the replacement needle onto the nozzle taper. Re-install the nozzle cap finger tight.

4.       Use recommended oil: light viscosity oils and tapping or cutting fluids work the best. Heavy viscosity oils such as motor oil, gear oil, or heavy tapping oils may not produce a high-quality stream.

5.       If the oil line does get air bubbles inside, the pump inside the PulseJet nozzle will pass them through the system. While bubbles are moving through the nozzle, the stream will appear weak, aerated, and inconsistent. After the bubbles pass through, the stream will return to its proper form.

6.       Always make sure the reservoir cap is installed and tightened when running PulseJet to maintain the proper tank pressure.

PulseJet Lubrication

Refer to Lubricant Grease, and Sealant Table to see our recommended oil list.

PulseJet Lubrication

Product Type ISO VG Safety Data Sheet
White Oil Light Generic Mineral Based Oil 10 N/A 
Mobil DTE 24 Ultra (Included when installed at the factory and in the feild install kit) Mineral Hydraulic Oil 32 Product page | SDS [PDF]
Mobil DTE 25 Ultra Mineral Hydraulic Oil 46 Product page | SDS [PDF]
Mobil DTE Light Mineral Circulating Oil 32 Product page | SDS [PDF]
WD 40 Penetrating Oil 3 N/A
Coolube 2210 EP Metalworking Oil 15 N/A
Tapmatic #1 Gold Tapping Oil 20 N/A
Relton Rapid Tap Tapping Oil 28 N/A
"Lard Oil"  for Aluminum and Soft Metals Cutting/Tapping Oil 40 N/A
Recently Updated

PulseJet - Troubleshooting Guide


TG0115

Introduction

The Haas PulseJet System is a programmable tap/drill oiling system that provides precise, controllable lubrication directly to the cutting tools that require targeted lubrication. This system pressurizes the oil tank that delivers the pressurized oil to the nozzle which is then pressurized and delivered to the cutting tool.

Symptom Table

Symptom Possible Cause Corrective Action
Large amount of air leaking from the cap when the PulseJet is cycling. The tank cap seal is dislodged and the tank no longer holds pressure. Reinstall the cap and verify the PulseJet works correctly. See the cap seal section below.
The PulseJet stream does not have good oil volume or pressure.
The tank does not seem to pressurize/depressurize when the PulseJet is cycling.
Alarm 9140 PULSEJET OIL LEVEL LOW The oil level in the PulseJet tank is low. Refill the PulseJet tank to the Full Line on the tank. Run the PulseJet purge cycle if the PulseJet tank was run dry.
The control gives the message FUNCTION LOCKED when you press [COOLANT], or the control gives Alarm 363 COOLANT LOCKED OFF when a program commands the coolant pump on or off. Setting 32 Coolant Override is set to OFF. See the Setting 32 page for additional details and Alarm 363 video instructions. 
The PulseJet does not turn on for a defined number of pulses. Setting 370 has not been configured. See the Setting 370 page for detailed instructions on how to set the PulseJet squirt count.

Reinstall Cap Seal

1

Remove the tank cap and check to see if the seal is in place. If it is out of position[1] or not visible[2], it will need to be reinstalled. Seal in the correct position[3].

2

Remove the tank cap and check to see if the seal is in place. If it is out of position or not visible, it will need to be reinstalled.

Use a flathead screwdriver to separate the cap assembly. There are four clips that hold it together.

Remove the ratchet plate and the cap seal and thoroughly clean all the components.

Reinstall the ratchet plate. It can only be installed one way. Reinstall the cap seal.

Press both pieces together until the clips snap into place.

Reinstall the cap and verify the PulseJet works correctly.

Prime the Oil Line

Make sure there is oil in the PulseJet reservoir and that the lid is tightly installed. Make sure the reservoir air and oil lines are connected. 

Disconnect the oil line [1] from the PulseJet nozzle and let it drape over a container placed on the mill table.

Press [DIAGNOSTIC] and navigate to the Maintanance then to the PulseJet tab [2]. 

Press [F4] to begin a priming cycle. Each cycle lasts 10 minutes.  The reservoir will be pressurized during the cycle. 

Note: Small machines may take only 1 cycle to fully prime the line. Larger machines may take 3 or 4 cycles. Heavier oils may take longer to prime. Continue running priming cycles until oil [4] begins to drip out of the oil line into the container. 

Note: While the machine is in the prime cycle the user can start a program.   However the user will not be able to start the prime cycle again while the program is running.

Reconnect the oil line to the PulseJet nozzle.

In MDI run:

M162 P10;
G04 P10.;
M30;

Test the PulseJet until a strong stream develops. 

Tips and Troubleshooting

1.       PulseJet will produce a consistent, fast, and tight oil pulse if the line is well primed, the dispenser needle is not clogged, and a recommended oil is being used.

2.       To always keep the line well primed:

  • Place the reservoir assembly near or above the spindle elevation
  • never let the tank run completely dry

3.       If you suspect that the dispenser needle is clogged, replace it. To do this, unscrew the knurled nozzle cap from the nozzle and gently twist and pull the yellow base of the needle off of the nozzle.

Note: This will expose the small check valve spring, do not lose it. Firmly press the replacement needle onto the nozzle taper. Re-install the nozzle cap finger tight.

4.       Use recommended oil: light viscosity oils and tapping or cutting fluids work the best. Heavy viscosity oils such as motor oil, gear oil, or heavy tapping oils may not produce a high-quality stream.

5.       If the oil line does get air bubbles inside, the pump inside the PulseJet nozzle will pass them through the system. While bubbles are moving through the nozzle, the stream will appear weak, aerated, and inconsistent. After the bubbles pass through, the stream will return to its proper form.

6.       Always make sure the reservoir cap is installed and tightened when running PulseJet to maintain the proper tank pressure.

PulseJet Lubrication

Refer to Lubricant Grease, and Sealant Table to see our recommended oil list.

PulseJet - Schematic

Recently Viewed Items

You Have No Recently Viewed Items Yet

Feedback
Haas Logo

Haas Delivered Price

This price includes shipping cost, export and import duties, insurance, and any other expenses incurred during shipping to a location in France agreed with you as a buyer. No other mandatory costs can be added to the delivery of a Haas CNC Product.