My Haas Welcome,
!
Haas Tooling MyHaas/HaasConnect Sign In Register Haas Tooling MyHaas/HaasConnect Sign Out Welcome, My Machines Latest Activity My Quotes My Account My Users Sign Out
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
      EU SERIES EU SERIES BUILD & PRICE | PRICE LIST BUILD & PRICE | PRICE LIST In-Stock Machines In-Stock Machines WHAT’S NEW WHAT’S NEW YOUR FIRST CNC YOUR FIRST CNC
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
      EU SERIES EU SERIES BUILD & PRICE | PRICE LIST BUILD & PRICE | PRICE LIST In-Stock Machines In-Stock Machines WHAT’S NEW WHAT’S NEW YOUR FIRST CNC YOUR FIRST CNC
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
      EU SERIES EU SERIES BUILD & PRICE | PRICE LIST BUILD & PRICE | PRICE LIST In-Stock Machines In-Stock Machines WHAT’S NEW WHAT’S NEW YOUR FIRST CNC YOUR FIRST CNC
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
Haas Tooling MyHaas/HaasConnect Sign In Register Haas Tooling MyHaas/HaasConnect Sign Out Welcome, My Machines Latest Activity My Quotes My Account My Users Sign Out
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
4 - RPL - Zero Point Ready - Installation

Haas Robot Pallet Loader - Operators / Service Manual


  • 0 - RPL - Table of Contents
  • 1 - RPL - Introduction
  • 2 - RPL - Legal Information
  • 3 - RPL - Safety
  • 4 - RPL - Zero Point Ready - Installation
  • 5 - RPL - Installation
  • 6 - RPL - Fence/Interlock Installation
  • 7 - RPL - Light Curtain Installation
  • 8 - RPL - DCS Setup
  • 9- RPL - Pallet Loader Setup
  • 10 - RPL - Operation
  • 11 - RPL - Maintenance
  • 12 - RPL - Troubleshooting

Go To :

  • 4.1 VMC Single Zero Point Installation
  • 4.2 UMC Single Zero Point Installation

4.1 VMC Single Zero Point Installation

Recently Updated

Single Zero Point Ready - Installation - VMC


AD0764

Revision A - 03/2026

Introduction

Updated

The zero point ready installation only needs to be done on machines that are ordering the RPL-25KG to be added to an existing machine. 

 Note: For machines purchased with a RPL-25KG, the zero point ready is already installed on the machine. Skip this section if the machine already has the zero point ready kit installed.

This procedure applies to the following kits:

  • 93-1001314 - Single Zero Point Ready Kit VMC

The corresponding machine kit below will also need to be ordered to be able to do this procedure:

  • 93-1001318 - RPL-25KG Ready Kit VF-SML
  • 93-1001319 - RPL-25KG Ready Kit VF-MED

Note: The Robot Pallet Loader option also requires an auto window option to be installed. Refer to the VMC - Auto Window - Installation - AD0669 to order and install this option on your machine.

 IMPORTANT: Depending on the machine's built by date, separate brackets may need to be ordered to make the machine compatible. The brackets are for routing the hoses through the enclosure. The brackets that are sold separately are 25-12138, 25-14177 & 25-12749. The brackets for machines built after the dates listed below are included in Zero Point Ready Kit VMC. Refer to the below table to determine if and what brackets are needed for each machine:

Machine Date Part Number
VF-2 Built before 7/22/2022 25-12138 & 25-14177
VF-2YT Built before 7/21/2022 25-12138 & 25-14177
VF-3/4 Built before 7/30/2022 25-12749 & 25-14177 
VF-3YT/40 Built before 8/16/2022 25-12749 & 25-14177 
VF-3YT/50 Built before 12/1/2022 25-12749 & 25-14177 
VF-5/40/XT Built before 9/20/22 25-12749 & 25-14177 
VF-5/50/XT Built before 10/16/22 25-12749 & 25-14177 

Zero Point Vise - Installation

1

The zero point receiver comes assembled and needs to be fastened to the table.

The instructions below can be referenced in case the receiver needs to be reassembled or to verify the receiver has all the needed components.

Note: The receiver for a VF machine is different than the receiver for UMC machines. Make sure that the receiver is compatible with the machine.

2

Turn the clamp assembly upside down.

Use dielectric grease to install the 3 O-rings onto the clamp assembly.

Install the smallest O-ring on the clamp port [1].

Install the large O-ring [2] and the medium O-ring [3] onto the clamp assembly as shown in the image.

3

Install the clamp assembly [1] onto the zero point receiver [2].

Make sure that the clamp port [3] is aligned with the port on the pallet receiver plate [4].

Note: If the clamp port is not aligned, the zero point will not clamp/unclamp properly.

4

Place the alignment keys [1] on the pallet receiver plate spacer [4] and pallet receiver plate [3].

Fasten the alignment keys [2] to the plates using the M6 x 1 x 12MM SHCS [1]

Torque the bolts to their required specifications.

Use the SHCS ½-13 X 3.5" bolts [5] to align the pallet receiver plate [3] to the pallet receiver plate spacer [4].

5

Bolt the zero point receiver [3] to the table in the orientation as shown in the image using the SHCS ½-13 X 3.5" bolts [1] and the 1/2-13 5/8 WIDE T-SLOT [2].

Check the table below to determine how far the zero point can be placed from the right edge of the table depending on the machine it is going on.

Note: Make sure the zero point receiver is oriented the correct direction. See the next step for details.

Machine Right edge of machine table to left side of Zero Point
VF-2 16.25 in (412.75 mm)
VF-3 28.00 in (711.2 mm)
VF-4 32.00 in (812.8 mm)
VF-5 29.00 in (736.6mm)

6

When bolting down the zero point receiver to the table, make sure the receiver is oriented the correct direction.

The clamp and unclamp fittings should be pointed towards the back of the machine.

Also, make sure that deep bore [1] on the receiver is located on the opposite side of the auto window. 

Note: The deep bore [1] is for the dowel pin of the pallet. This needs to be oriented away from the window since the robot can only load pallets in one orientation.

7

Install the foot pedal cable [1] to P14 on the I/O board.

From there route the cable to the hole of the front skirt of the machine. 

Connect the foot pedal cable 32-1286 to the other cable 32-1303 [1] routed to the front skirt of the machine. 

Note: The cable routed to the machine skirt must be cable 32-1303 [1]. If there is another cable that is a different part number already routed to the foot pedal, it needs to be replaced with the 32-1303 cable included in the Zero Point Ready Kit.

Rotate Lube Panel

Note: This section is only for medium VF machines. Skip to the next section if you are installing this option on a small VF machine.

1

Close the air valve [1] at the bottom of the lube cabinet.

Bleed the remaining air out of the manifold by pulling on the air release [2]. Make sure the gauge on the manifold reads zero.

Disconnect the cables, lube lines, and air hoses from the lube cabinet. 

2

Take off the top cover [1] of the cable guide. Take off the cable channel [2] so that the lube cabinet can be taken off of the machine. 

3

Remove the lube cabinet [1] from the machine. 

Note: Keep the lube cabinet upright so the lube inside the cabinet does not spill out. 

4

Install the rotated lube cabinet mount [1] onto the machine. Once it is mounted, install the lube cabinet [2] onto to the new mount.

 

5

Reinstall the cable channel guides from before and have the hoses and cables go the same route through it as before. 

Install the rotated lube cabinet top sheet metal [1] onto the top of the lube cabinet and rotated lube cabinet mount. Install the rotated cabinet strap [2] on to the top of the cable channel guide cover and the rotated lube cabinet top sheet metal.

6

Route the cables, lube lines, and air hoses [1] down through the cable channel guide and through the rotated lube cabinet mount as shown. 

Lube Panel - Installation

1

Close the air valve [1] at the bottom of the lube cabinet.

Bleed the remaining air out of the manifold by pulling on the air release [2]. Make sure the gauge on the manifold reads zero.

2

Install the elbow fitting [1] directly into the air manifold on the front face as shown in the image. 

3

Use the included magnets to attach the Air Booster onto the back of the enclosure for small VFs [1] and onto the side of the lube cabinet for medium VFs [2].

Hose and Cable Routing

1

Route the steel braided air lines [1] through the through the conduit spring holder [2].

Route the opposite ends of the air lines through the hole in the enclosure..

Note: The hole in the enclosure shown is for a VF-2. The enclosure hole for the VF-3 through 5 is on the right enclosure wall.

 Note: Both hoses coming from the work holding are steel braided. They are shown as green and red in the image to differentiate between them.

2

Attach the mounting bracket [1] to the sheet metal on the exterior side of the machine, around the enclosure hole. Use ¼-20 bolts [2].

Run each steel braided hose through a cable clamp [3] and bolt these to the mounting bracket. 

Route the hoses to the lube panel.

 Note: Both hoses coming from the work holding are steel braided. They are shown as green and red in the image to differentiate between the clamp (red) and unclamp (green) hoses.

3

Connect the green hose to the unclamp port [1] of the solenoid denoted with a green zip tie on it.

Connect the red hose to the clamp port [2] of the solenoid denoted with a red zip tie on it.

 

4

Connect the air booster to the manifold [1] using the included HOSE 1/4 OD PE RED HIGH PRESSURE.

5

Connect cable 33-1359 CBL AIR VISE PRESS SWS PP ROBOT 12FT  [1] to the pressure sensor as shown. 

Route the cable back to the I/O board and plug this into P13 using the adapter cable provided in the kit.

Note: The pressure sensor should be on the fitting where the red hose is connected. This sensor makes sure the zero point is clamped.

6

Connect cable 33-1355 CBL DUAL AIR VISE ROBOT LOAD STATION to P36 [5] on the IO PCB. Connect the coolant refill to the pigtail if needed.

Route the other end directly to the Air Booster.

Connect the V-1 end [1] to the solenoid going to the zero point in the machine [4].

Connect the V-2 end [2] to the solenoid going to the load station zero point [3].

7

Re-introduce air to the manifold by turning the valve [1].

Check for leaks and tighten fittings as needed. 

Note: Adjust the regulator on the air booster to change the pressure of the zero point receivers. Set the pressure of the booster at a minimum of 100 PSI to ensure proper clamping and unclamping.

Update Configuration Files

If this is a field installation, the configuration file will need to be updated to implement the necessary parameters. 

Visit HBC.HAASCNC.COM to download the latest configuration file.

Note: Only Haas Certified Service technicians can log into this website.

Load the configuration patch file to the control. Refer to the NEXT GENERATION CONTROL - CONFIGURATION FILE - DOWNLOAD/LOAD procedure. 

 

Zero Point Ready - Testing

1

To test the clamp and unclamp of the zero point ready kit go to the Pallet Changer Recovery page.

Press [F2] [1] to unclamp the zero point pallet. 

Place a pallet [2] into the zero point receiver [3].

 Note: Make sure that pallet is oriented correctly so that the dowel pin aligns with the zero point receiver.

Press [F2] again to clamp the zero point pallet.

Verify that the pallet is clamped to the receiver and that no alarms are generated.

4.2 UMC Single Zero Point Installation

Recently Updated

Single Zero Point Ready - Installation - UMC


AD0765

Revision B - 06/2026

Introduction

Updated

The single zero point ready installation only needs to be done on machines that are ordering the RPL-25KG to be added to an existing machine. 

Note: For machines purchased with an RPL-25KG, the single zero point ready is already installed on the machine. Skip this section if the machine already has the single zero point ready kit installed.

This procedure applies to the following kits:

  • 93-1001315 - Single Zero Point Ready Kit UMC-500
  • 93-1001316 - Single Zero Point Ready Kit UMC-750   
  • 93-1001317 - Single Zero Point Ready Kit UMC-1000

The corresponding machine kit below will also need to be ordered to be able to do this procedure:

  • 93-1001320 - RPL-25KG READY KIT UMC-500
  • 93-1001321 - RPL-25KG READY KIT UMC-750
  • 93-1001322 - RPL-25KG READY KIT UMC-1000

The purpose of the single zero point ready kit is to allow for the pneumatics to be routed to the single zero point clamp through the body of the tilt rotary. Installing this involves removing the platter and rotating the machine B-axis. Make sure this is possible before starting this procedure.

Note: The Robot Pallet Loader option also requires an auto window option to be installed. Refer to the UMC Auto Window - Installation - AD0663 to order and install this option on your machine.

Note: The only difference between these kits is the bottom cover panel for the TRT body on the different size machines.

UMC Zero Point Ready - Installation

1

Start by assembling the pneumatic manifold [1] that goes inside the C-body of the machine.

Tighten the NPT 1/4" plug fitting [2] to the single port.

Tighten the 2 Brass 1/4" fittings [3] to the angled ports.

Tighten the 2 ORB6M NPT 1/4" steel fittings [4].

Install the 4 O-Ring 2-212 [5] into the grooves of the manifold. 

Note: Install the four O-rings into alternating grooves on the top face of the manifold block, leaving one empty groove between each installed O-ring.

2

Connect the 3 Port Rotary Union Shaft to the 3 Port Rotary Union Shaft Extension using [2] SHCS 1/4-20 X 5/8 make sure the O-Ring 2-011 [1] are seated in the cavities of the shaft.

Torque the bolts to their required specs.

 

3

Press the dowel pin [1] into the anti-rotation block [2] until it bottoms out. 

4

Assemble the platter coupler [3] by placing the O-rings in position.

Place 3 of the 2-011 O-Rings [1] on the air ports shown in the image.

Place the larger 2-031 O-Ring [2] onto the middle groove of the coupler.

5

Rotate the B-axis +90 degrees and remove the cover [1]. Return the B-axis to its original position at 0 degrees.

This cover will be replaced by the cover included in the zero point ready field install kit.

6

Updated

Remove the platter by following the removal section of the UMC C-Axis Platter Replacement linked below.

 WARNING: IF YOU DO NOT DEPRESSURIZE THE SYSTEM BEFORE REMOVING THE PLATTER YOU CAN PERMANENTLY DAMAGE THE BRAKE BY REMOVING THE PLATTER.

Note: Take note of the platter orientation before removing to make sure to install the platter in the same orientation later on.

UMC C-Axis Platter Replacement
UMC Rotary Unit – Weight Reference Guide

7

Updated

Place the platter on a bench and bolt the coupler [1] to the platter using SHCS 1/4-20 X 5/8 [2].

While the platter is on the bench insert the felt strip included in the kit in the groove [3]

NOTE: If the UMC is not exchanging platters reuse the felt strip already in the groove. 

Torque the bolts to their required specs.

8

Updated

When using the same platter:

The height measurement between the top of the platter and the top of the coupler needs to be taken to ensure proper fitment of the workholding spud. 

Use a depth micrometer to measure between the two surfaces. The measurement should be 0.7000 ± .0010" for machines built before 5/22/2026 and 0.7560 ± .0010" for machines built after 5/22/2026 [1]. 

Note: The measurement is taken without the seal.

Install shims P/N 59-2350 and 59-2351 as needed to achieve proper workholding height. The shims are installed between the workholding and the platter face [2].

9

Install the coupler onto the shaft assembly [1] by using 1/4-20 X 1 1/4 bolts [3]. Make sure the O-Rings 2-011 [2] are in the cavaties of the shaft and not where the bolts attach.

Torque the bolts to their required specs.

10

Install the coupler and platter assembly [2] back onto the rotary using M12 bolts [1].

Tighten the bolts, but do not torque them down yet.

Follow the installation section of the UMC C-Axis Platter Replacement linked below for the full instruction on how to correctly re-install the platter.

UMC C-Axis Platter Replacement

11

The Zero point receiver will come assembled. Depending on the machine type, the receiver can have different features.

UMC-500:

  • Zero Point Receiver Assembly has no spacer plate [2] as shown in the left image.

UMC-750/1000:

  • Zero Point Receiver Assembly has a spacer plate [2] between the platter [1] and receiver [3] as shown in the right image.

Note: The zero point receivers come assembled. The steps below can be referenced to ensure the assembly includes all the needed components and that the receiver is compatible with the machine.

12

Turn the clamp assembly upside down.

Use dielectric grease to install the 3 O-rings onto the clamp assembly.

Install the smallest O-ring on the clamp port [1].

Install the large O-ring [2] and the medium O-ring [3] onto the clamp assembly as shown in the image.

13

Install the clamp assembly [1] onto the zero point receiver [2].

Make sure that the clamp port [3] is aligned with the port on the pallet receiver plate [4].

Note: If the clamp port is not aligned, the zero point will not clamp/unclamp properly.

14

Place the alignment keys on the pallet receiver plate [3] and the platter spacer plate [4].

Fasten the alignment key [1] to the plates using the 2 M6 x 1 x 12MM SHCS [2]

Torque the bolts to their required specs.

Note: The platter space plate [4] is only on UMC-750 and UMC-1000 machines. UMC-500 machines do not need the spacer plate shown in the image.

15

Assemble the pallet receiver that will be installed on the platter.

Important: Place the 3 O-Rings [5] in the receiver plate.

Note: The platter space plate [3] is only on UMC-750 and UMC-1000 machines. UMC-500 machines do not need the spacer plate shown in the image.

Fasten the receiver spud [1] to the pallet spacer plate [2] and the receiver plate [3] using the 3 M6 x 55mm SHCS [4].

Note: Make sure that the platter spacer and receiver plate are oriented the same direction. The alignment keys installed in the previous step will help this alignment.

Torque the bolts to their required specs.

 

16

Place 3 2-011 O-Rings into the top of the coupler through the center bore in the platter.

Then install the pallet receiver and spud assembled in the previous step to the platter. 

The receiver is held in position by 4 T-nuts that are placed in the T-slots of the platter.

Use the 4 SHCS [3] to fasten the pallet receiver [2] to the T-nuts [1]. 

Note: The spud is not shown in the image but should be located into the center bore in the platter. The spud must be assembled to the pallet receiver [2] before the receiver is fastened to the platter.

17

Rotate the B-axis 90 degrees [1].

18

Attach the anti-rotation block [3] to the gearbox using the M6 bolts [4].

If the read head is in configuration [1] you will need to clock it to position [2]  this will require you to redo the compensations on the machine.

If the read head is in configuration [2] the compensations will not need to be redone.

Torque the bolts to their required specs.

Please contact service about borrowing a swivel checker.

19

Install the manifold assembly [2] from step 1 by inserting the anti-rotation dowel pin [1] into the pneumatic manifold.

20

After installing the shaft assembly to the pneumatic manifold make sure to install the snap ring [2] to the shaft groove [1].

Note: If the groove for the snap ring is not visible on the shaft, then some bolts may not be fully tightened, or the dowel pin needs to be pressed further into the manifold.

21

Install the foot pedal cable [1] to P14 on the I/O board.

From there route the cable to the hole of the front skirt of the machine. 

Connect the foot pedal to the cable [1] coming from the front skirt of the machine. 

Note: If there is already a foot pedal cable connected to P14 make sure it is cable 32-1303. This has additional cables going to P14 for the robot load station.

Lube Panel - Installation

1

Close the air valve [1] at the bottom of the lube cabinet.

Bleed the remaining air out of the manifold by pulling on the air release [2]. Make sure the gauge on the manifold reads zero.

2

Install the elbow fitting [1] directly into the air manifold on the front face as shown in the image. 

3

Install the Air Booster on the back of the machine using the magnets to attach it.

Hose and Cable Routing

1

Route the zero point air lines through the black conduit that routes through the center bore and to the work holding manifold.

Route the opposite ends of the zero point air lines [1] to the Air Booster. 

Note: Make sure the hoses for the zero point are high pressure hoses.

2

Pull the hoses through the B-axis body and to the pneumatic manifold as shown.

Use the velcro-ties [1] and cable clamps to neatly route the cables to the pneumatic manifold.

3

The unclamp hose denoted in green  [1] goes the fittings as shown.

The clamp hose denoted in red [2] is goes to the fitting as shown.

4

Connect the green hose to the unclamp port [1] of the solenoid denoted with a green zip tie on it.

Connect the red hose to the clamp port [2] of the solenoid denoted with a red zip tie on it.

 

5

Connect the air booster to the manifold [1] using the included HOSE 1/4 OD PE RED HIGH PRESSURE.

6

This step is for non-CAN lube panel machines only: 

Connect cable 33-1532 - Air Lube Solenoid cable to P35 on the IO PCB with the connector with the pigtail for Pallet Unclamp [16].

Route the cable to the lube panel to make the following connections to all the solenoid power cables. The color for each connector is listed:

[2] PulseJet Solenoid - White and Violet

[3] Auto Door  - Gray

[4] TRP Unclamp  - Yellow and Black

[5] Spindle Air - Violet

[6] Spindle Lube - White

[7] Min Lube Grease - White and Red

[8] Open Door Interlock - White and Brown

[9] Auto Air Gun (AAG) - Red

[10] TSC Purge - White and Orange and Yellow jumper to TAB Air [15]

[11] SMTC Pocket U/D - White and Black

[12] UMC Auto Window - White and Yellow

[13] Purge Solenoid - White and Gray

[14] Pallet Air Blast - White and Green

[15] Tool Air Blast Air (TAB) Yellow jumper from TSC Purge [10]

7

Connect cable 33-1307 CBL AIR VISE PRESS SWS PP ROBOT 21FT to the pressure sensor as shown. 

Route the cable back to the I/O board and plug this into P13 using the adapter cable provided in the kit.

Note: The pressure sensor should be on the fitting where the red hose is connected. This sensor makes sure the zero point is clamped.

8

Connect cable 33-1306 to P36 [5] on the IO PCB. Connect the coolant refill to the pigtail if needed.

Route the other end directly to the Air Booster.

Connect the V-1 end [1] to the solenoid going to the zero point in the machine [4].

Connect the V-2 end [2] to the solenoid going to the load station zero point [3].

9

Re-introduce air to the manifold by turning the valve [1].

Check for leaks and tighten fittings as needed. 

10

Reinstall the new cover [2] and return the rotary [1] to 0 degrees on the B axis.

Update Configuration Files

If this is a field installation, the configuration file will need to be updated to implement the necessary parameters. 

Visit HBC.HAASCNC.COM to download the latest configuration file.

Note: Only Haas Certified Service technicians can log into this website.

Load the configuration patch file to the control. Refer to the NEXT GENERATION CONTROL - CONFIGURATION FILE - DOWNLOAD/LOAD procedure. 

 

Zero Point Receiver - MRZP

1

After installing the Zero Point Receiver, MRZP needs to be done to account for the change in pallet height compared to the platter.

Assemble the zero point MRZP pallet [1].

Press the dowel pin [2] into the MRZP pallet.

Install the zero point pull stud [3] using the M10x20 SHCS [4].

Mount the MRZP artifact [5] to the zero point MRZP pallet using the 2 SHCS [6].

2

Go to the Recovery Page. Press [F2] [1] to unclamp the zero point pallet receiver [2] inside the machine.

Place the MRZP pallet assembly [3] with the artifact in the receiver. Make sure the dowel pin is aligned in the correct position.

Clamp the zero point receiver by pressing [F2] again.

Exit recovery and continue with doing MRZP. Refer to the UMC - MRZP and Safe zones page for more information on how to do MRZP.

Note: The center bore in the zero point calibration pallet can also be used for probing. The diameter of the center bore is 2 inches.

Zero Point Ready - Testing

1

To test the clamp and unclamp of the zero point ready kit go to the Pallet Changer Recovery page.

Press [F2] [1] to unclamp the zero point pallet. 

Place a pallet [2] into the zero point receiver [3].

Note: Make sure that pallet is oriented correctly so that the dowel pin aligns with the zero point receiver.

Press [F2] again to clamp the zero point pallet.

Verify that the pallet is clamped to the receiver and that no alarms are generated.

Recently Viewed Items

You Have No Recently Viewed Items Yet

Feedback
Haas Logo

Haas Delivered Price

This price includes shipping cost, export and import duties, insurance, and any other expenses incurred during shipping to a location in France agreed with you as a buyer. No other mandatory costs can be added to the delivery of a Haas CNC Product.